MCC Melody Data Streamer Library: Using a Custom Struct | Videos
MCC Melody Data Streamer Library: Using a Custom Struct
Click on the link below to choose the API reference for AVR or PIC16F/18F: https://onlinedocs.microchip.com/v2/keyword-lookup?keyword=DATA-STREAMER-DRIVER&version=latest&redirect=true
This video covers How to Use the Data Streamer Component in MCC Melody. The custom structure for the Data Streamer can be used to change the variables. This project shows the refactoring needed to use the custom structure.
This is useful because in the initial stages of an MCC project development the changes of the various MCU peripherals are often done while having the MCC open. However, the final touches can be done without opening the MCC.