PIC® ADCC PLIB Driver: Printf of ADC Result with Variables Window and Printf | Videos
PIC® ADCC PLIB Driver: Printf of ADC Result with Variables Window and Printf
MCC Melody Data Streamer Library: How to use the ADCC PLIB Driver: https://onlinedocs.microchip.com/v2/keyword-lookup?keyword=scf-pic8-adcc-v1&version=latest&redirect=true
This video covers how to create a project in MCC Melody which takes an ADC conversion is taken every 100 ms, on the selected analog channel. After each ADC conversion a LED is toggled, and the ADC Result is sent to the PC terminal using printf. The video also shows how to verify the ADC results. First while debugging, using the Variables Window, then when running the project, sending printf strings to the MPLAB Data Visualizer terminal.