We detect you are using an unsupported browser. For the best experience, please visit the site using Chrome, Firefox, Safari, or Edge. X

The Benefits of Serial-Attached Memory with Compute Express Link™

Serial-attached memory solutions using Compute Express Link have many benefits compared to parallel interfaces and can be used to replace or augment parallel memory solutions.


Introduction

With the ever-increasing compute and memory bandwidth demands on data center servers, system implementers continuously strive to find novel techniques to provide higher performance for a wide range of application workloads while maintaining or even decreasing the cost of new infrastructure. The fundamental challenge of traditional servers results from being locked to specific memory types and having limited DRAM memory channels that prevent the flexibility needed to implement these techniques and optimize cost and performance metrics. Let’s look at how Compute Express Link’s CXL.memory sub-protocol can be used to create CXL™ memory controllers to:

● Expand memory bandwidth and/or capacity beyond what the host processor’s native DDR memory channels allow

● Enable host processors to have media-independence and support different memory types

● Decrease solutions costs by right-sizing memory capacity for targeted application workloads

To continue reading the article on computeexpresslink.org, click here

For more information on CXL technology, visit our Resource Library for white papers, presentations and webinars. 


Ahmad Danesh, Jun 24, 2020