Getting STARTed with AVR® - Ep. 5 - Adding ADC Functionality | Videos
Getting STARTed with AVR® - Ep. 5 - Adding ADC Functionality
- SKIP if you’re an advanced user
- Reconfigure the AVR START project, adding an ADC
- Choosing an analog input pin, configuring an ADC Result Ready IRQ
- Show how to use the View Diff (with WinMerge), to decide whether to override changes to generated files or not.
- Show how START ADC_init () function implements all the datasheet recommended steps, required in order to setup the ADC, all that is left is for us to start a conversion.
- Write ADC_start_conversion (), which is called in the RTC overflow IRQ, and ADC_get_result () which is called in the ADC conversion complete IRQ.
- Create a global variable adc_result, adding this to main.h, along with above function prototypes.
- Write a usart_send_data () function, in order to send ADC results.
- Demonstrate ADC results on the Data Visualizer.
http://start.atmel.com/