Microchip Technology Inc

Third-Party Tool Categories

Microchip’s third-party tools and providers offer a diverse range of embedded-design development boards and software that compliment the development tools we develop in-house. Over 200 Microchip Third-Party Recognized Providers and Premier Partners provide development tools in almost every embedded application. Premier Third-Party Partners in particular are certified by our engineers to be the best in the industry providing not only a large array of software and hardware tools, but superior support for the products as well.

Hardware Tools

Premier Third-Party Partners


http://www.ccsinfo.com
Waukesha, Wisconsin, United States of America
Phone: (262) 522-6500
Fax: (262) 522-6504

Established in 1996, CCS is a leading worldwide supplier of embedded software, and hardware development tools, that enable companies to develop premium products based on Microchip PIC® MCU and dsPIC® DSC devices. CCS C Compilers are the most advanced, highly developed and most widely used compiler in the industry. These compilers include a generous library of built-in functions, pre-processor commands, and ready-to-run example programs to quickly jump-start any project. CCS IDE C compiler products provide a unique Profiler Tool to track time and usage information for use on functions, code blocks, as well as receiving live data from running programs. Complete proven tool chains include a full line of programmers and debuggers,application specific hardware prototyping boards, and software development kits. CCS is also a leading provider of electronic engineering services for embedded software development, R&D support, hardware design, and custom electronic products that adhere to our client's high-quality standards. Download our free demo for the Microchip PIC®MCU C compiler!

For Technical Support, please visit www.ccsinfo.com/support, contact support@ccsinfo.com, or call 262-522-6500 ext 72. For FAE Support visit www.ccsinfo.com/fae.


http://www.matrixtsl.com
Halifax, United Kingdom
Phone: 01422 252380
Fax: 01422 252381

Matrix Technology Solutions provides teaching and learning services in numerous fields including mathematics, science, electronics, and PIC-micro programming. Matrix also provides a range of courses on PIC-micro programming, PIC-micro robotics systems. Flowcode is an advanced graphical programming language for microcontrollers. The great advantage of Flowcode is that it allows those with little to no programming experience to create complex electronic systems in minutes. Flowcode is available in multiple languages and supports the PIC micro, dsPIC, and PIC24 series of microcontrollers. Matrix produces a flexible PIC-micro microcontroller programmer/development board for a range of 8-, 18-, 28- and 40-pin PIC micros.

For technical support, please visit http://www.matrixtsl.com/sup_menu.php or call 01422 252380.


http://saleae.com
San Francisco, California, United States of America
Phone: 510-984-2463

Saleae makes some of the world’s best logic analyzers, now with analog!

For Technical Support, please visit support.saleae.com or contact support@saleae.com.

Products

Saleae Logic 8 - USB Logic Analyzer

$399.00

Buy Now

Logic analyzers (Saleae SAL-0015) are great for debugging embedded applications. They operate by sampling a digital input connected to a device under test (DUT) and then displaying the recording on your computer. The Saleae Logic devices connect to your PC over USB. Just download the software at www.saleae.com. Navigate your data easily and intuitively with Logic's fluid and fully animated mouse-driven interface. The Saleae products support decoding for over 20 different protocols.

Features:

  • 8 digital inputs and 8 analog inputs (shared with the digital channels)
  • Digital Max Sample Rate: 100 MSPS @ 3 channels, 50 MSPS @ 6 channels, 25 MSPS @ 8 channels
  • Analog Max Sample Rate: 10 MSPS @ 2 channels, 5 MSPS @ 5 channels, 2.5 MSPS @ 8 channels
  • Digital Bandwidth: 25 MHz square wave at 100 MSPS sample rate
  • Analog Bandwidth: 1 MHz at 10 MSPS sample rate
  • Edge or pulse-width trigger
  • Cross platform support (Windows, Mac and Linux)
  • Supports many protocols including: Serial, SPI, I2C, CAN, LIN, JTAG, USB, and much more


Saleae is a trusted Third-Party Tool provider

Saleae Logic Pro 8 - USB Logic Analyzer

$699.00

Buy Now

Logic analyzers (Saleae SAL-0016)  are great for debugging embedded applications. They operate by sampling a digital input connected to a device under test (DUT) and then displaying the recording on your computer. The Saleae Logic devices connect to your PC over USB. Just download the software at www.saleae.com. Navigate your data easily and intuitively with Logic's fluid and fully animated mouse-driven interface. The Saleae products support decoding for over 20 different protocols.

Features:

  • 8 digital inputs and 8 analog inputs (shared with the digital channels)
  • Digital Max Sample Rate: 500 MSPS @ 4 channels, 100 MSPS @ 8 channels (USB 3.0 required)
  • Analog Max Sample Rate: 50 MSPS @ 3 channels, 12.5 MSPS @ 8 channels (USB 3.0 required)
  • Digital Bandwidth: 100 MHz square wave at 500 MSPS sample rate
  • Analog Bandwidth: 5 MHz at 50 MSPS sample rate
  • Edge or pulse-width trigger
  • Cross platform support (Windows, Mac and Linux)
  • Supports many protocols including: Serial, SPI, I2C, CAN, LIN, JTAG, USB, and much more


Saleae is a trusted Third-Party Tool provider

Saleae Logic Pro 16 - USB Logic Analyzer

$999.00

Buy Now

Logic analyzers (Saleae SAL-0017) are great for debugging embedded applications. They operate by sampling a digital input connected to a device under test (DUT) and then displaying the recording on your computer. The Saleae Logic devices connect to your PC over USB. Just download the software at www.saleae.com. Navigate your data easily and intuitively with Logic's fluid and fully animated mouse-driven interface. The Saleae products support decoding for over 20 different protocols.

Features:

  • 16 digital inputs and 16 analog inputs (shared with the digital channels)
  • Digital Max Sample Rate: 500 MSPS @ 4 channels, 100 MSPS @ 16 channels (USB 3.0 required)
  • Analog Max Sample Rate: 50 MSPS @ 3 channels, 12.5 MSPS @ 13 channels, 6.25 MSPS @ 16 channels
  • Digital Bandwidth: 100 MHz square wave at 500 MSPS sample rate
  • Analog Bandwidth: 5 MHz at 50 MSPS sample rate
  • Edge or pulse-width trigger
  • Cross platform support (Windows, Mac and Linux)
  • Supports many protocols including: Serial, SPI, I2C, CAN, LIN, JTAG, USB, and much more


Saleae is a trusted Third-Party Tool provider


http://www.segger.com
Hilden, Germany
Phone: +49 2013-2878-0

SEGGER develops hardware and software development tools specifically for embedded systems.  We understand the needs and timelines of the modern embedded developer and mold our products around them with unparalleled performance and reliability. Founded in 1992, SEGGER is a privately held ISO9001:2008 company and is steadily growing. Based out of Hilden Germany, with distributors on all continents and an office in Massachusetts, SEGGER offers its full product range worldwide.

SEGGER software products include: embOS (RTOS), emWin (GUI), emFile (File System), emUSB (USB Host and Device Stack), embOS/IP (TCP/IP Stack), and emLoad (Boot Loader). These are all optimized for minimum memory usage, while achieving maximum performance.  SEGGER makes use of its own RTOS and middleware solutions to create highly integrated, cost-effective, development and programming tools known as the industry leading J-Link/J-Trace family of emulators and the Flasher (stand-alone flash programmer). SEGGER cuts software development time for embedded applications by offering affordable, high-quality, flexible, and easy-to-use tools and software components allowing developers to focus on their applications.

For Technical Support please contact support@segger.com.

Products

SEGGER J-Link Debug Probe

$378.00

Buy Now

The J-Link BASE Debug Probe is a USB-powered in-circuit debugger supporting PIC32 devices. Based on a 32-bit RISC CPU, it can communicate at high speed with supported target devices. J-Link is a great tool for flash programming and debugging in development and production environments. Note: J-Link is fully supported in MPLAB X IDE v2.15.

Features include:

  • USB-powered and plug-and-play compatible
  • Direct download into flash memory
  • Download speed up to 1 MByte/second
  • Unlimited breakpoints in flash memory
  • Remote Server included allowing use of J-Link remotely via TCP/IP
  • Supports JTAG chains with multiple devices
  • Cross-platform support Windows, Linux, Mac OS X
  • SDK available

SEGGER is a trusted third-party tool provider

 


http://tag-connect.com
Burlingame, California, United States of America
Phone: 877-244-4156

Tag-Connect specializes in Product Development, In-Circuit Plug-of-Nails™ Programming Cables, and Programming / Debugging Equipment.

For Technical Support visit www.tag-connect.com/contact or contact support@tag-connect.com.

Products

Tag-Connect Clip Board (pkg of 3)

$18.00

Buy Now

The Tag-Connect Clip Board (TC2030-CLIP-3PACK) attaches to the alignment pins of a Tag-Connect No Legs cable such as TC2030-MCP-NL. The Clip Board can be pressed onto the alignment pins from underneath the circuit board, providing a temporary connection for debugging purposes. Then you have the best of both worlds: a small PCB footprint and a reliable debugging connection. Note: Clip Boards are small and easily misplaced, so we include 3 in the package.

Tag-Connect is a trusted third-party tool provider

Tag-Connect In-Circuit Cable Legged Version

$36.00

Buy Now

Tag-Connect In-Circuit Programming and Debug Cable (TC2030-MCP) is compatible with MPLAB REAL ICE, MPLAB ICD 3 and MPLAB ICD 2. This cable uses high-reliability spring pins which connect to a tiny footprint of pads and locating holes on your PCB. It has plastic legs that snap directly into the board to hold it securely in place saving both board space and the cost of a mating header component on every PCB.

Tag-Connect is a trusted third-party tool provider

Tag-Connect In-Circuit Cable No Legs

$36.00

Buy Now

Tag-Connect In-Circuit Programming Cable (TC2030-MCP-NL) is compatible with MPLAB REAL ICE, MPLAB ICD 3 and MPLAB ICD 2. This cable uses high-reliability spring pins which connect to a tiny footprint of pads and locating holes on your PCB. It has three steel pins that ensure accurate alignment and correct orientation and is hand-held during a fast programming operation. TC2030-MCP-NL is particularly suitable for production programming operations and applications where board space is a premium.

Tag-Connect is a trusted third-party tool provider.

Tag-Connect Starter Kit

$78.00

Buy Now

This Kit includes 2 Tag-Connect cables Legged and No Legs, a sample PCB to demonstrate footprint for each type of cable, and a Tag-Connect Clip Board for debugging with a No-Legs cable. The cables use high-reliability spring pins that connect to a tiny footprint of pads and locating holes on your PCB. The Legged version has plastic legs that snap directly into the board to hold it securely in place. The No-Legs version has three steel pins that ensure accurate alignment and correct orientation and is hand-held during a fast programming operation. Tag-Connect cables save the board space and expense of a mating header component on every PCB.

  • Compatible with MPLAB REAL ICE, MPLAB ICD 2, and MPLAB ICD 3
  • Legged cable available separately: TC2030-MCP
  • No Legs cable available separately: TC2030-MCP-NL
  • Clip Board is available separately: TC2030-CLIP-3PACK

Tag-Connect is a trusted third-party tool provider.


http://www.totalphase.com/
Sunnyvale, California, United States of America
Phone: +1 (408) 850-6502
Fax: +1 (408) 850-6501

Total Phase is a leading provider of embedded systems development tools for engineers all over the world. Total Phase's mission is to create powerful, high-quality, and affordable solutions for the embedded engineer. For years, Total Phase has developed products that have become tools of choice for Fortune 500 companies, small businesses, and research institutions alike. The simplicity and ease of integration of Total Phase products have led to many unique engineering solutions. As customers build Total Phase products into their systems, Total Phase actively incorporates their feedback, building the solutions that engineers find most valuable. Customers are able to leverage these solutions to build higher-quality products for their own markets.

For technical support, please visit www.totalphase.com/support or call +1 (408) 850-6502.

Products

Total Phase Beagle USB 480 Protocol Analyzer

$1200.00

Buy Now

The Beagle™ USB 480 Protocol Analyzer (Total Phase TP320510) is a non-intrusive High-Speed USB 2.0 protocol analyzer. Developers can monitor what is happening on the USB bus as it happens with packet-level timing information at 16.67 nS resolution.

Total Phase is a trusted third-party tool provider.

Total Phase Beagle USB 12 Protocol Analyzer

$400.00

Buy Now

The Beagle™ USB 12 Protocol Analyzer (Total Phase TP320221) is a non-intrusive Full/Low-Speed protocol analyzer. Developers can monitor what is happening on the USB bus as it happens with bit-level timing information at 21nS resolution.

Total Phase is a trusted third-party tool provider.

Total Phase Beagle I2C/SPI Protocol Analyzer

$330.00

Buy Now

The versatile Beagle I2C/SPI Protocol Analyzer (Total Phase TP320121) is the ideal tool for the embedded engineer who is developing an I2C or SPI based product. The Beagle Analyzer provides a high performance monitoring solution in a small, portable package.

Total Phase is a trusted third-party tool provider

Total Phase Cheetah SPI Host Adapter

$350.00

Buy Now

The Cheetah SPI Host Adapter (Total Phase TP280121) is a high-speed SPI adapter that is capable of communicating over SPI at up to 40+MHz.

Total Phase is a trusted third-party tool provider.

Total Phase Aardvark I2C/SPI Host Adapter

$300.00

Buy Now

Connect your Windows, Linux, or Mac OS X PC to I2C and SPI bus through USB with the Aardvark I2C/SPI Host Adapter (Total Phase TP240141). Multi-master, slave, and GPIO are featured in this versatile development and testing tool.

Total Phase is a trusted third-party tool provider.

Total Phase I2C Development Kit

$605.00

Buy Now

The I2C Development Kit by Total Phase (TP120112) is a comprehensive and cost-effective kit that bundles together a complete set of Total Phases industry-leading I2C development tools and popular accessories.

With this kit, developers can exercise target devices on an I2C bus as a master device, simulate an I2C master or slave device, program and verify I2C-based devices, and passively monitor an I2C bus in real time with bit-level timing down to 20 ns. The kit includes:

  • (1) Aardvark I2C/SPI Host Adapter
  • (1) Beagle I2C/SPI Protocal Analyzer
  • (2) 10-Pin Split Cables
  • (1) I2C/SPI Activity Board
  • (2) 6 foot USB A->B cables
  • Software CD for Windows and Linux


Total Phase is a trusted third-party tool provider.

Total Phase Komodo CAN Duo Interface

$450.00

Buy Now

The Komodo™ CAN Duo Interface by Total Phase (TP360110) is a powerful two-channel USB-to-CAN adapter and analyzer. The Komodo interface is an all-in-one tool capable of active CAN data transmission as well as non-intrusive CAN bus monitoring. This portable and durable unit easily integrates into end-user systems. It provides a flexible solution for a variety of applications, including automotive, military, industrial, medical and more.

  • Dual channel: two independent customizable CAN channels
  • Transfer rate up to 1 Mbps
  • Independent galvanic isolation per CAN channel
  • 8 general purpose digital I/O lines
  • USB 2.0 full-speed; bus-powered
  • Free software and API, with bindings for C/C++, .NET, Python, Visual Basic
  • Windows, Linux and Mac OS X compatible
Total Phase is a trusted third-party tool provider.

Beagle USB 480 Power Protocol Analyzer - Standard Edition

$1800.00

Buy Now

The Beagle USB 480 Power Protocol Analyzer Standard Edition (Total Phase TP323510) enables VBUS current and voltage measurement within our industry-leading Data Center Software. The extra-large hardware buffer and one-click correlation of voltage and current measurement to protocol-level actively ensures that engineers can take advantage of our unique real-time data analysis and display, enabling them to easily debug the functionality of their embedded systems while also optimizing the power profile of their applications. Features include:

  • Current/Voltage VBUS Monitor with real-time graphing of values
  • Bi-directional correlation of VBUS values with USB data
  • 256MB Hardware Buffer
  • Real-Time Non-Intrusive Monitoring
  • Automatic bus-speed detection
  • Low/Full/High-Speed USB 2.0
  • Real-Time USB Class-Level Decoding
  • Capture traces >25GB

Total Phase is a trusted third-party tool provider.


Beagle USB 480 Power Protocol Analyzer - Ultimate Edition

$2400.00

Buy Now

The Beagle USB 480 Power Protocol Analyzer Ultimate Edition (Total Phase TP323610) enables VBUS current and voltage measurement within our industry-leading Data Center software. The enhanced USB 2.0 advanced triggering, extra-large hardware buffer, and one-click correlation of voltage and current measurement to protocol-level activity ensures that engineers can take advantage of our unique real-time data analysis and display, enabling them to easily debug the functionality of their embedded systems while also optimizing the power profile of their applications. The Ultimate Edition has all the features of the Standard Edition, plus:

  • USB 2.0 Advanced Triggers to match data patterns, packets, errors types

Total Phase is a trusted third-party tool provider.



Recognized Third-Party Tool Providers


Aristotle Enterprises Inc.

http://www.aristotle.com.tw
New Taipei City, Taiwan
Phone: +886-2-89707048

Aristotle is a leading design & manufacturing company in antenna ODM/OEM? business. Aristotle is the specialist in antenna design, mechanical design, and with automatic production ability. We serve our customers with the best quality products of Antenna, RF connector and RF cable assembly with 30 years of experience on product automation.


ASCALAB d.o.o

http://www.ascalab.com
Ljubljana, Taiwan
Phone: +386 40 649 101

Ascalab is providing state of the art R&D production of prototypes, small-scale and medium-scale high-tech products which allows us to provide solutions on demand basis. All phases of the product life-cycle are covered: starting with the design of printed circuit boards (PCB) to software development, production, assembly, testing and dispatch respective to the electronics, IoT, medical and manufacturing segments. We offer highest standards of business, project management and software engineering processes with the knowledge of innovative technologies and value added engineering on Windows, Linux, mobile platforms. We have experience in Manufacturing, Healthcare, Metrology, Telemedicine, Insurance, Security industry.The company was founded in 2012 by software experts with proven track of successfully developed and implemented projects in various industries and markets. We are based in Ljubljana, Slovenia.


Embed Inc

http://www.embedinc.com
Littleton, United States of America
Phone: (978) 742-9014

Embed Inc is primarily a consulting company performing electrical, firmware, and software engineering of embedded systems, specializing in Microchip PIC microcontrollers and the circuits around them.  We have worked on well over 100 projects containing Microchip PICs and dsPICs. Embed also makes some physical products, which are mostly aids for developing, testing, and using small embedded systems. Some of these products are available on MicrochipDirect, but for the full product line, see http://www.embedinc.com/products.

For Technical support, please call (978) 742-9014.


JTAG Technologies

http://www.jtag.com
Eindhoven, Netherlands
Phone: +31 40 295 0870

JTAG Technologies offers generic test tools for boundary-scan (IEEE 1149.x) compliant devices and Microchip-specific tools for hardware validation and device programming. CoreCommander PIC32 allows the activation of the in-circuit debugger mode to communicate at-speed with on-chip or on-board peripherals. JTAG Technologies also supports the in-system programming of several Microchip parts that use the ICSP or JTAG port via its generic JTAG hardware (PIC16, dsPIC33, PIC32MX, etc.).


openPicus

An open source family of programmable and interchangeable system on modules with connectivity for IoT/M2M. Our modules run your application and connect to the Cloud (Wi-Fi or GPRS or Ethernet) or may be directly interfaced to a smartphone. No need for a microcontroller on your carrier board. The free IDE, Tutorials and Libraries (HTTP, MQTT and others) will speed up your time to market by 6 months.


ProMik GmbH

http://www.promik.com
Nürnberg, Germany
Phone: +49 911 25 26 65 92

Since its beginning in 1995, ProMik has focused on providing state of the art support for programmable microcontrollers and provides systems for development and production, manual and automated systems, and programming services. The company has specialized in supporting applications in automotive electronics and industrial process controls. The company is fully ISO and TS certified. ProMik's solutions include flashing and testing solutions including cell margin analysis to verify the quality of device programming.


Velleman, Inc.

http://www.vellemanusa.com
Fort Worth, Texas, United States of America
Phone: 817-284-7785

Velleman is a worldwide supplier of electronic products, including, but not limited to the following:

  • DIY-Kits
  • Tools
  • Test equipment
  • Components
  • Consumer products
  • Adapters and power supplies
  • Lighting
  • 3D Printers