Microchip Technology Inc

Third-Party Tool Categories

Microchip’s third-party tools and providers offer a diverse range of embedded-design development boards and software that compliment the development tools we develop in-house. Over 200 Microchip Third-Party Recognized Providers and Premier Partners provide development tools in almost every embedded application. Premier Third-Party Partners in particular are certified by our engineers to be the best in the industry providing not only a large array of software and hardware tools, but superior support for the products as well.

Emulators / Debuggers

Premier Third-Party Partners


http://www.iar.com
Uppsala, Sweden
Phone: +46 18 16 78 00

IAR Systems supplies future-proof software tools and services for embedded development, enabling companies worldwide to create the products of today and the innovations of tomorrow. Since 1983, IAR Systems’ solutions have ensured quality, reliability and efficiency in the development of over one million embedded applications. The complete C/C++ compiler and debugger toolchain, IAR Embedded Workbench, offers full-scale support for Microchip’s 8- and 32-bit AVR MCUs as well as Microchip’s ARM-based and 8051-based MCUs families. The company is headquartered in Uppsala, Sweden and has sales and support offices all over the world. IAR Systems Group AB is listed on NASDAQ OMX Stockholm, Mid Cap.

For support information, visit https://www.iar.com/support/technical-support/.


http://www.segger.com
Hilden, Germany
Phone: +49 2013-2878-0

SEGGER develops hardware and software development tools specifically for embedded systems.  We understand the needs and timelines of the modern embedded developer and mold our products around them with unparalleled performance and reliability. Founded in 1992, SEGGER is a privately held ISO9001:2008 company and is steadily growing. Based out of Hilden Germany, with distributors on all continents and an office in Massachusetts, SEGGER offers its full product range worldwide.

SEGGER software products include: embOS (RTOS), emWin (GUI), emFile (File System), emUSB (USB Host and Device Stack), embOS/IP (TCP/IP Stack), and emLoad (Boot Loader). These are all optimized for minimum memory usage, while achieving maximum performance.  SEGGER makes use of its own RTOS and middleware solutions to create highly integrated, cost-effective, development and programming tools known as the industry leading J-Link/J-Trace family of emulators and the Flasher (stand-alone flash programmer). SEGGER cuts software development time for embedded applications by offering affordable, high-quality, flexible, and easy-to-use tools and software components allowing developers to focus on their applications.

For Technical Support please contact support@segger.com.

Products

SEGGER J-Link Debug Probe

$378.00

Buy Now

The J-Link BASE Debug Probe is a USB-powered in-circuit debugger supporting PIC32 devices. Based on a 32-bit RISC CPU, it can communicate at high speed with supported target devices. J-Link is a great tool for flash programming and debugging in development and production environments. Note: J-Link is fully supported in MPLAB X IDE v2.15.

Features include:

  • USB-powered and plug-and-play compatible
  • Direct download into flash memory
  • Download speed up to 1 MByte/second
  • Unlimited breakpoints in flash memory
  • Remote Server included allowing use of J-Link remotely via TCP/IP
  • Supports JTAG chains with multiple devices
  • Cross-platform support Windows, Linux, Mac OS X
  • SDK available

SEGGER is a trusted third-party tool provider

 Note: An adapter cable is available to connect SEGGER J-Link to RJ11 connectors, it's available from SEGGER's website:


J-Link Microchip Adapter


http://www.totalphase.com/
Sunnyvale, California, United States of America
Phone: +1 (408) 850-6502
Fax: +1 (408) 850-6501

Total Phase is a leading provider of embedded systems development tools for engineers all over the world. Total Phase's mission is to create powerful, high-quality, and affordable solutions for the embedded engineer. For years, Total Phase has developed products that have become tools of choice for Fortune 500 companies, small businesses, and research institutions alike. The simplicity and ease of integration of Total Phase products have led to many unique engineering solutions. As customers build Total Phase products into their systems, Total Phase actively incorporates their feedback, building the solutions that engineers find most valuable. Customers are able to leverage these solutions to build higher-quality products for their own markets.

For technical support, please visit www.totalphase.com/support or call +1 (408) 850-6502.



Recognized Third-Party Tool Providers


Acroview Technology Co., Ltd.

http://www.acroview.com
Shenzhen, China
Phone: +86-755-26971006
Fax: +86-755-26971258

Acroview is a company with more than 10 years experience in programmer research & development, manufacturing and service providing. Equipped with the world’s leading technology, we focus on providing our customers with more innovative programming products and solutions. Our products include universal programmers, production programmers, online programmers as well as emulators. We are convinced that with our devotion and pursuit of quality and advanced technology, more and more customers will choose and trust Acroview as a reliable partner.


ASCALAB d.o.o

http://www.ascalab.com
Ljubljana, Taiwan
Phone: +386 40 649 101

Ascalab is providing state of the art R&D production of prototypes, small-scale and medium-scale high-tech products which allows us to provide solutions on demand basis. All phases of the product life-cycle are covered: starting with the design of printed circuit boards (PCB) to software development, production, assembly, testing and dispatch respective to the electronics, IoT, medical and manufacturing segments. We offer highest standards of business, project management and software engineering processes with the knowledge of innovative technologies and value added engineering on Windows, Linux, mobile platforms. We have experience in Manufacturing, Healthcare, Metrology, Telemedicine, Insurance, Security industry.The company was founded in 2012 by software experts with proven track of successfully developed and implemented projects in various industries and markets. We are based in Ljubljana, Slovenia.


Dataman Programmers Ltd

http://www.dataman.com
Dorchester, Dorset, United Kingdom
Phone: (44) 0 1300 320719
Fax: (44) 0 1300 321012

With 30 years experience Dataman is the world’s leading provider of device programmers. We offer a comprehensive range of programming solutions suitable for every requirement from design and development to large scale production. We are committed to providing continued development, manufacturing and support and to deliver customer specific innovative solutions. All Dataman products come with comprehensive warranties, free lifetime support and free software updates via our website and telephone helpdesk. With offices in both the UK and USA plus distributors in 53 countries worldwide, you can be assured of the very best customer service and support.


DediProg Technology Co., Ltd

http://www.DediProg.com
Taipei, Taiwan
Phone: 886-2-27907932
Fax: 886-2-27907916

DediProg was founded in 2005 in Taiwan and the Shanghai base was established in 2010. Dediprog is a company aiming at the solutions of IC programming of EEPROM, SPI Flash, NOR Flash, NAND FLASH, Microcontroller, eMMC, CPLD and other programmable devices. We not only provide dedicated solutions for engineering development but also offer high efficiency equipment for production. Dediprog always treats customers' needs as our first concern. By designing overall solutions, DediProg is providing the best products which fit customers’ needs and requirements for their target applications.

Products & Services:

  • Dedicated engineering ISP programmers
  • Universal engineering ISP programmers
  • Universal production programmers
  • Semi-auto tape & reel taping machine
  • Automatic IC programming Systems
  • IC programming service
  • Customized solutions according to customer’s request


LEAP Electronic Co., Ltd.

http://www.leap.com.tw
New Tapei City, Taiwan
Phone: 886-2-2999-1860
Fax: 886-2-2999-9873

Leap Electronic was established in 1980, located in TangChen Industrial Park, Sanchung city, Taipei. To help our customers establish completed development system has always been our priority.  Our company involves in the field of IC test and programming equipments deeply because we ourselves manufacture IC programmer, emulator, IC tester and interface protector in a name of Leap. To promote Leap's products all over the world, Leap obtains ISO 9001 certification and absolutely guarantees customers the best quality.


Lynxar Technologies

http://www.lynxartech.com
Sassuolo, Italy
Phone: +39-0536-840586

Lynxar Technologies is a global, independent, high-tech company, leader in semiconductor device in-system programming for the electronic boards manufacturing industry. Lynxar is setting a new semiconductor device programming standard for the years ahead. DeviceClip, Lynxar flagship product, is currently the market's fastest, most advanced, reliable and easy-to-use ISP platform for the support of every type of Flash-based device.


Phyton, Inc. Microsystems and Development Tools

http://www.phyton.com
Brooklyn, New York, United States of America
Phone: (718) 259-3191
Fax: (718) 259-1539

Phyton produces and sells device programmers for in-system and in-socket programming of Microchip memory devices and embedded microcontrollers. This includes gang production programmers and engineering tools. Currently 9000+ Microchip device-package combinations are supported. Socket adapters for all popular packages are available. All Phyton device programmers can be driven remotely via the DLL or in the command line mode. The software is featured with the project support, simplifies user interface and other helpful features. Phyton also produces in-circuit emulators for SST89C5x series of Microchip microcontrollers.