Microchip logo
  • All
  • Products
  • Documents
  • Applications Notes

AN873

Title:
Using the MCP2515 CAN Developer?s Kit
Name:
AN873
Date:
03/14/2004
Author:
Pat Richards
Description:
The MCP2515 eases software development and shortens the learning curve for the MCP2515 providing three PC software templates with different functions that CAN node designers can use as needed. By using one of the templates, the user can read, display, and modify all of the registers in the MCP2515 down to the bit level. Another template can demonstrate basic input/output functionality allowing messages to be transmitted and received the CAN bus. Finally, the third template is demonstration template that, by using preprogrammed PICmicro® microcontroller (MCU), implements a two node CAN bus that gets the user ? the bus? in the shortest amount of time and effort.
Keywords:
mcp2515 development kit,mcp2515 developer's kit,stand-alone CAN
 
Application Notes & Source Code
 Last Updated
Size
 
  AN873
  03/14/2004
  378KB
Silicon Products