We detect you are using an unsupported browser. For the best experience, please visit the site using Chrome, Firefox, Safari, or Edge. X
Maximize Your Experience: Reap the Personalized Advantages by Completing Your Profile to Its Fullest. Update Here
Stay in the loop with the latest from Microchip. Update your profile while you are at it. Update Here
Complete your profile to access more resources. Update Here

Microchip Launches New Generation of 8-bit AVR® MCUs with Core Independent Peripherals

New Series is Supported by START to Optimize Software Support and Includes Rich Features in 4 KB and 8 KB Flash


CHANDLER, Ariz., Nov. 8 (Electronica), 2016 — Microchip Technology Inc. (NASDAQ: MCHP), a leading provider of microcontroller (MCU), mixed-signal, analog and Flash-IP solutions, today released a new generation of 8-bit tinyAVR MCUs. The four new devices range from 14 to 24 pins and 4 KB to 8 KB of Flash and are the first tinyAVR® microcontrollers to feature Core Independent Peripherals (CIPs). The new devices will be supported by Atmel START, an innovative online tool for intuitive, graphical configuration of embedded software projects.

“This announcement is very important to Microchip as it represents the coming together of the two most powerful 8-bit MCU brands under one roof,” said Steve Sanghi, CEO and Chairman of the Board of Microchip Technology Inc. “Customers love both PIC® and AVR® MCUs and Microchip is re-energizing new product development to not only continue to support, but to grow the esteemed AVR portfolio.”

The new ATtiny817/816/814/417 devices provide all the right features to help drive product innovation including small, low pin count and feature-rich packaging in 4 KB or 8 KB of Flash memory. Other integrated features include: a CIP called Peripheral Touch Controller (PTC); Event System for peripheral co-operation; custom programmable logic blocks; self-programming for firmware upgrades; non-volatile data storage; 20 MHz internal oscillator; high-speed serial communication with USART; operating voltages ranging from 1.8V to 5.5V; 10-bit ADC with internal voltage references; and sleep currents at less than 100 nA in power down mode with SRAM retention.

“As the number one provider of 8-bit MCUs with our broad portfolio of PIC, AVR and 8051 MCU cores, we are committed to providing our customers with more products that can help differentiate their designs,” said Steve Drehobl, vice president of Microchip’s MCU8 division. “By adding innovative capabilities like Core Independent Peripherals, interconnected analog and intuitive graphic design support that have been available on PIC MCUs for some time, we are continuing to provide our AVR MCU customers with the right tools to innovate and get to market fast.”

CIPs allow the peripherals to operate independently of the core, including serial communication and analog peripherals. Together with the Event System, that allows peripherals to communicate without using the CPU, applications can be optimized at a system level. This lowers power consumption and increases throughput and system reliability.

Accompanying the release of the four new devices, Microchip is adding support for the new AVR family in Atmel START, the online tool to configure software components and tailor embedded applications. This tool is free of charge and offers an optimized framework that allows the user to focus on adding differentiating features to their application.

 For more information about Microchip’s new AVR microcontrollers and supporting tools visit AVR MCUs.

 Development and Support

To help accelerate evaluation and development, a new Xplained Mini Kit is available for $8.88 USD. The Xplained Mini Kit is also compatible with the Arduino® kit ecosystem. The kit can be used for standalone development and is fully supported by the Atmel START and Atmel Studio 7 software development tools.

Pricing and Availability

The new generation of 8-bit tinyAVR MCUs is available in mass production today in QFN and SOIC packaging. Devices are available in 4 KB and 8 KB Flash variants, with volume pricing starting at $0.43 for 10K units. For additional information, contact any Microchip sales representative or authorized worldwide distributor.

Note: The Microchip name and logo, the Microchip logo, PIC, AVR and the Atmel name and logo are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries.  All other trademarks mentioned herein are the property of their respective companies.

About Microchip Technology
Microchip Technology Inc. (NASDAQ: MCHP) is a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at www.microchip.com.

About Atmel
Atmel is a wholly-owned subsidiary of Microchip Technology Inc.

Editorial Contact:
Cathy Gedvilas
(480) 792-4386

Chelsey Kruger
(480) 792-5047
 
Brian Thorsen
(480) 792-7182
Reader Inquiries:
1-888-624-7435

Live Chat

Need Help?

Privacy Policy