We detect you are using an unsupported browser. For the best experience, please visit the site using Chrome, Firefox, Safari, or Edge. X
Maximize Your Experience: Reap the Personalized Advantages by Completing Your Profile to Its Fullest. Update Here
Stay in the loop with the latest from Microchip. Update your profile while you are at it. Update Here
Complete your profile to access more resources. Update Here

From GEO to LEO: How Mission Profiles Affect High-Reliability Power Requirements

Not every space mission has the same level of risk tolerances. As satellite architectures expand from long-life GEO platforms into cost-sensitive LEO constellations, engineers need a smarter way to align power component selection with mission requirements.

Imagine preparing for a long road trip. The vehicle you would choose for a daily city commute is very different from one designed to cross a desert or navigate remote mountain roads. While both need to be reliable, the environment, duration and level of risk ultimately determine what is required.

Space missions are no different.

A satellite operating in Low Earth Orbit (LEO) for three years faces a very different operating environment than a communications platform expected to remain in Geostationary Orbit (GEO) for more than fifteen years. Environmental stressors like ionizing radiation, heavy-ion impacts and high temperature operation will more significantly degrade long-duration operating systems in GEO orbits than short-term counterparts in LEO. Yet for many years, space programs often approached high-reliability component selection with a "highest available protection" mindset.

Today, with the rapid growth of commercial space, Earth observation constellations and New Space missions is challenging that approach. As a result, engineers are increasingly asking a different question: What level of component reliability contributing to satellite system longevity does this mission actually require?

Understanding the answer can help optimize system performance, manage costs and reduce unnecessary design complexity.

Mission Profiles Are Changing

The traditional space industry was largely built around a small number of high-value, long-duration missions where maximizing reliability was the primary objective. In many cases, selecting the highest available reliability assurance level was the natural choice.

Today's space ecosystem looks very different.

The growth of commercial satellite constellations, Earth observation platforms, scientific missions and technology demonstrators has created a much broader range of mission profiles. Some spacecrafts are designed to operate in LEO for only a few years, while others must withstand decades of exposure in GEO. By developing a power electronics portfolio that spans a wide range of mission profiles, system designers gain the flexibility to optimize component selection based on mission needs, performance requirements and cost constraints.

The Risks of Over- and Under-Engineering

Historically, selecting power electronics with the highest available reliability was often viewed as the safest approach. However, this can lead to unnecessary costs, reduced sourcing flexibility and system-level over-engineering.

Conversely, selecting a device with insufficient reliability can lead to degraded performance, shortened mission life or even mission failure.

The objective is not simply maximizing component reliability. The objective is matching component capability to mission requirements.

This shift toward mission-based design is becoming increasingly important as commercial and government space programs seek to optimize performance while managing cost and schedule pressures.

M6 Technology: Built for Modern Space Missions

Meeting the needs of today's diverse space missions requires more than simply designing electronics to be radiation tolerant. Designers also need power devices that deliver high power density, efficient performance and predictable operation throughout the mission lifecycle.

Microchip's high-reliability power MOSFET portfolio is built on its mature M6 radiation-hardened vertical double-diffused MOSFET (VDMOS) technology platform. Developed specifically for demanding aerospace and space applications, M6 technology combines robust radiation hardness with reliable performance across a temperature range of -55°C to 150°C, while stringent manufacturing and testing flows help provide long-term device reliability.

M6 devices are engineered to withstand both Total Ionizing Dose (TID) exposure and Single Event Effects (SEE), helping designers address the key radiation challenges encountered across LEO, MEO and GEO environments. Depending on mission requirements, devices are available with Radiation Hardness Assurance (RHA) levels of up to 100 krad(Si) under JANSR qualification and up to 300 krad(Si) under JANSF qualification. In addition, Single Event Effects (SEE) performance is qualified to LET levels of up to 90 MeV·cm²/mg.

Beyond radiation performance, our M6 technology is optimized for low RDS(on), reduced gate charge and efficient switching performance while maintaining stable electrical characteristics throughout temperature and radiation exposure extremes.

This combination allows engineers to focus on selecting the appropriate radiation assurance level for their mission without sacrificing power-conversion performance.

Using the RH MOSFET Brochure as a Mission-Mapping Tool

Rather than beginning with a specific part number, designers can start by evaluating the mission itself.

Key questions include:

  • What orbit will the spacecraft operate in?
  • How long is the planned mission duration?
  • What radiation environment is expected?
  • What reliability margin is required?
  • What screening and qualification level best aligns with program objectives?

Our M6 MOSFET portfolio supports this mission-based approach through flexible component screening and qualification options, including JANSR devices qualified up to 100 krad(Si), JANSF devices qualified up to 300 krad(Si) and Microchip New Space (MNS) screening flows designed specifically for commercial LEO and New Space applications.

Rather than viewing the brochure as simply a product catalogue, engineers can use it as a mission-mapping tool—aligning orbit, mission duration and radiation requirements with the most appropriate RH MOSFET solution.

Want More?

For more information, please visit our RH MOSFET web page.

Tags/Keywords: Aero-Defense

Live Chat

Need Help?

Privacy Policy