We detect you are using an unsupported browser. For the best experience, please visit the site using Chrome, Firefox, Safari, or Edge. X
Maximize Your Experience: Reap the Personalized Advantages by Completing Your Profile to Its Fullest. Update Here
Stay in the loop with the latest from Microchip. Update your profile while you are at it. Update Here
Complete your profile to access more resources. Update Here

Trusted and Secure Authentication with ATECC608A for AWS IoT

Why Would You Harden Your IoT Security with the ATECC608A for AWS IoT?


This solution is archived and will no longer be updated. We recommend that you use the TrustFLEX ATECC608B-TFLXTLS for AWS IoT Core instead.

Securing communication with a Cloud service and manipulating keys comes with many challenges: storing and using keys in the microcontroller exposes them, operating systems and software have bugs, the Heartbleed bug for OpenSSL was notable by easily exposing keys. Consequently, governments and corporations across the globe are working to protect individual identities and privacy. Strong authentication is the start of robust security. This leads cloud providers to push towards hardware-based security to obtain strong device identity protection, prevent identity spoofing, but also to protect against unauthorized firmware updates and prevent proliferation.

An easy way to hack an IoT device today is to physically attack the embedded system and spoof the private key which is likely located in the clear of a microcontroller memory. But hacking a single device or transaction is typically not of value to an attacker. Hackers are looking for weaknesses that will enable them to exploit a large number of connected devices. Once the keys are spoofed, the devices are accessed, a scalable remote attack can be launched leveraging the corrupted IoT devices as entry points

AWS IoT Authentication Use Case

Microchip explains how hardware root of trust work using the ATECC608A secure element and AWS IoT. The Just In Time Registration and Use Your Own certificates functions from AWS IoT allow large scale authentication of automated system, yet secure by protecting private keys from users, software and manufacturing backdoors.

Update the Zero Touch Provisioning Kit Version B Using the ATECC608A


Simply use the new CryptoAuth XPRO-B board.

What about the ATECC608A for AWS IoT? Based on the  Zero Touch Provisioning Kit (version B) for AWS IoT hardware, you can simply swap the red CryptoAuth-XPRO board to the CryptoAuth-XPRO-B board that includes now the ATECC608A or use one of the socketed AT88CKSCKTUDFN-XPRO add-on boards with your device package of choice.

What remains identical compared to the ATECC508A for AWS IoT? The overall hardware is still using the ATWINC1500 Wi-Fi® module, the SAM G55 Arm® Cortex®-M4 based MCU running FreeRTOS™ and the OLED display board. The TLS is still leveraging the integrated one from the ATWINC1500 provided by Microchip. The AWS IoT setup is also identical.

What is different from the ATECC508A then? The ATECC608A doesn't come preconfigured on the CryptoAuth-XPRO-B board. During the  "getting started" procedure, the firmware update necessary to upgrade to the ATECC608A will configure the secure element as part of the process. One of the main added values of the ATECC608A is its ability to enable secure boot capabilities for light embedded systems (illustrated separately). The RNG has been upgraded and an AES hardware accelerator is integrated.

The AT88CKECC-AWS-XSTK-B kit for AWS IoT has been designed to help you start to prototype and learn the basics of secure provisioning. The secure element is pre-configured but not provisioned with keys out of the box. The Python-based scripts will guide you through the steps of provisioning and illustrate the process your company will go through when implementing certificate-based authentication in a production environment. Once the kit is provisioned, it provides a unique, trusted and protected identity.

20 Years of Experience in Secure Provisioning


Microchip is here the all way through.

Trust cannot rely only on the device but also on the manufacturing process. Exploiting third-party weaknesses is one of the top targets for hackers. Isolating keys and secrets from manufacturing is equally vital. Customers can leave this burden to Microchip's secure factories and leverage our trusted provisioning service already used by thousands of companies. It's zero touch; the private keys are never exposed.

Prototype

  • Educate yourself about the AWS IoT Security model
  • Understand why private key isolation is vital to your design
  • Learn how to code with CryptoAuthLib library
  • Learn how to configure the ATECC608A memory zone and set your expected policies
  • Learn the basics of provisioning a secure element

Personalize

  • Memory configuration is defined and locked
  • Your Certificate Authority is decided
  • AWS IoT production account is configured with AWS
  • Secret exchange with Microchip completed
  • The ATECC608A is set up with your customized part number

Mass Production

  • All the provisioning—keys/certificates generation and manipulation—is done within Microchip's secure factories
  • Keys are internally generated and never exposed to the outside world
  • Elimination of any software or manufacturing backdoors
  • The device ships pre-provisioned with the secrets

AWS IoT Authentication Products


Tools and Software


Getting Started


Getting Started - http://microchipdeveloper.com/iot:ztpk

AWS IoT Core Secure Authentication with JITR Tutorial Video: Guides you through the complete onboarding process -
https://www.youtube.com/watch?v=kvjYcPNSmoo