Features dashboard control and monitoring at Municipality local level and beyond, enabling a runway for future smart city applications.
Microchip collaboration with a distribution partner and a leading street lighting innovator results in a connected streetlight solution that also powers a new generation of connected nodes for smart city applications.
Microchip collaboration with a distribution partner and a leading street lighting innovator results in a connected streetlight solution that also powers a new generation of connected nodes for smart city applications.
Features dashboard control and monitoring at Municipality local level and beyond, enabling a runway for future smart city applications.
Features dashboard control and monitoring at Municipality local level and beyond, enabling a runway for future smart city applications.
Real-time cloud connectivity with leading-edge Microchip LoRa® and Bluetooth® solutions.
Real-time cloud connectivity with leading-edge Microchip LoRa® and Bluetooth® solutions.
Microchip CryptoAuthentication™ solution set featuring advanced confidentiality, data integrity, and authentication to systems with MCU or MPUs running encryption/decryption algorithms.
Microchip CryptoAuthentication™ solution set featuring advanced confidentiality, data integrity, and authentication to systems with MCU or MPUs running encryption/decryption algorithms.
From the earliest attempts to harness volcanic gas or burning oil, humans have been lured by the prospects of squeezing more useful hours from each day by lighting up the night. Municipal streetlights have been illuminating the paths of travelers for hundreds of years now, with many urban cores operating 24/7 as cities that never, or rarely, sleep.
As public utility organizations work with their trusted vendors to address the migration to LED-based lighting, all manner of related technology advancements have been introduced into the mix. The height, location and elevation of a municipality’s streetlights (or more importantly, their poles) offer a promising locale for smart traffic sensors, security cameras, public Wi-Fi hotspots, environmental sensors, small cell wireless antennas, solar panels, electric vehicle charging stations, and IoT nodes for applications that have yet to be developed.
A leading lighting systems vendor approached Microchip to discuss their vision for interconnected streetlights as a prerequisite for future Smart City initiatives. They described the landscape of LED streetlights as lacking widescale connectivity and an operating environment without universal standards. Urban leaders often faced expensive operational costs and maintenance burdens, along with less-than-stellar energy efficiency outcomes. Their experts felt that a strong response to increasing municipal demands for Smart City IoT solutions and the opportunity to introduce smarter streetlight solutions would give them a competitive edge in their regional markets and enhance their position globally.
Smart City schemes promise cost-effective solutions for managing public assets and interconnection among neighboring communities. In both state-run utility agencies and in highly-regulated public/private agencies, the concept of streetlights as catalysts for Smart City projects has a great deal of momentum. IoT-enabled streetlights of the future are projected to decrease the cost of municipal lighting, and offer advanced capabilities that were unthinkable a generation ago. City managers will be able to manipulate the illumination levels throughout the day, increasing them gradually as sunset approaches. Spikes in vehicle traffic, dynamic changes in weather conditions, antisocial behaviors and public gatherings at major events could all be supplemented with increased lighting from smart city platforms (SCPs). Secondary services including air quality measurement and noise pollution monitoring could be supported by the smart lighting networks.
The initial meeting led to more detailed discussions between the Microchip sales team and the vendor’s design and executive teams. With a long history of success in the development of microcontrollers, embedded wireless connectivity solutions and security applications, Microchip proposed an innovative LoRaWAN™-based approach for the company’s next-gen connected streetlights in collaboration with a trusted distribution partner.
This project mandated a solution that could produce a low total cost of ownership and simply the design process so the solution could be launched in a short time frame. Interoperability for future expansion and wide scale deployment were also critical to the success of the project.
Microchip’s new 433/868 MHz LoRaWAN module turned out to be ideal. It addresses increasing demands on end-devices for long range connectivity, low-power for battery operation, and low infrastructure cost for volume deployment. The Microchip module comes with the LoRaWAN protocol stack, so it can easily connect with established and rapidly expanding LoRa Alliance infrastructure— including both privately managed Local Area Networks (LANs) and telecom-operated public networks—to create Low Power Wide Area Networks (LPWANs) with nationwide coverage.
Enhanced security features were paramount for a first-of-its-kind solution leveraging an open long-range wireless network. Microchip was able to serve this mandate as well, with its ATECC608B CryptoAuthentication™ device. The ATECC608B part of Microchip’s family of high-security cryptographic devices which combine world-class hardware-based key storage with hardware cryptographic accelerators to implement various authentication and encryption protocols.
For short-range wireless connectivity, the connected streetlight solution would rely on a trusted module from Microchip’s Bluetooth portfolio. With a small form factor, the surface mount module has the complete Bluetooth stack on-board and is controlled via simple ASCII commands over the UART interface. The device also includes all Bluetooth SIG profiles, as well as MLDP (Microchip Low-energy Data Profile) for custom data.
High performance and reliability characteristics made the Microchip SST26VF016B Serial Quad I/O (SQI) flash device a perfect choice. Utilizing a 4-bit multiplexed I/O serial interface to boost performance while maintaining the compact form factor of standard serial flash devices, the SST26VF016B also supports full command-set compatibility to traditional Serial Peripheral Interface (SPI) protocol.