Microchip Technology Inc

Third-Party Tool Categories

Microchip’s third-party tools and providers offer a diverse range of embedded-design development boards and software that compliment the development tools we develop in-house. Over 200 Microchip Third-Party Recognized Providers and Premier Partners provide development tools in almost every embedded application. Premier Third-Party Partners in particular are certified by our engineers to be the best in the industry providing not only a large array of software and hardware tools, but superior support for the products as well.

Programmers

Premier Third-Party Partners


http://www.ccsinfo.com
Waukesha, Wisconsin, United States of America
Phone: (262) 522-6500
Fax: (262) 522-6504

Established in 1996, CCS is a leading worldwide supplier of embedded software, and hardware development tools, that enable companies to develop premium products based on Microchip PIC® MCU and dsPIC® DSC devices. CCS C Compilers are the most advanced, highly developed and most widely used compiler in the industry. These compilers include a generous library of built-in functions, pre-processor commands, and ready-to-run example programs to quickly jump-start any project. CCS IDE C compiler products provide a unique Profiler Tool to track time and usage information for use on functions, code blocks, as well as receiving live data from running programs. Complete proven tool chains include a full line of programmers and debuggers,application specific hardware prototyping boards, and software development kits. CCS is also a leading provider of electronic engineering services for embedded software development, R&D support, hardware design, and custom electronic products that adhere to our client's high-quality standards. Download our free demo for the Microchip PIC®MCU C compiler!

For Technical Support, please visit www.ccsinfo.com/support, contact support@ccsinfo.com, or call 262-522-6500 ext 72. For FAE Support visit www.ccsinfo.com/fae.

Products

CCS Load-n-Go Handheld In-Circuit Programmer

$199.00

Buy Now

Load-n-Go (CCS 53503-814) is a low-cost handheld in-circuit programmer that supports PIC10, PIC12, PIC14, PIC16, PIC18, PIC24 and dsPIC families. Running on four AA batteries this mobile programmer can go where no PC or laptop could go before. The simple user interface seamlessly allows for quick field programming of targets with up to four firmware images. Load-n-Go can also be powered via USB or with a 9V AC adapter and used as a regular ICD/ICSP with the CCS IDE compilers.

CCS is a trusted Third-Party Tool Provider More Info

CCS PRIME8 Production Programmer (Touch Screen)

$899.00

Buy Now

The latest version of CCS's Prime8 Production Programmer (SKU# 53504-830) is a low-cost way to program up to eight (8) devices concurrently. Prime8 operates in stand-alone mode or when connected to a PC. The unit will supply up to 200ma at 2-5V to power target devices. It can program all devices in the PIC10, PIC12, PIC14, PIC16, PIC17, PIC18, PIC24, dsPIC and PIC32 families. The newest features include flash-drive readability, faster programming speed, and a graphics display touchscreen menu with easy-to-read icons.

CCS is a trusted Third-Party Tool Provider.


http://digilentinc.com
Pullman, Washington, United States of America
Phone: (509) 334-6306

Digilent Inc. is a leading electrical engineering products company serving students, universities, and OEM's worldwide with technology-based educational design tools. Based in Pullman Washington USA, Digilent designs, manufactures, and distributes its electronic design tools on a worldwide basis. Since its founding in 2000, Digilent products can now be found in over 2000 universities in more than 70 countries throughout the world. As a multinational company with offices in the US, Taiwan, China and Romania, Digilent is able to provide low-cost, expert quality solutions for a variety of customer needs.


Digilent Inc. is a leading electrical engineering products company serving students, universities, and OEM's worldwide with technology-based educational design tools. Based in Pullman Washington USA, Digilent designs, manufactures, and distributes its electronic design tools on a worldwide basis. Since its founding in 2000, Digilent products can now be found in over 2000 universities in more than 70 countries throughout the world. As a multinational company with offices in the US, Taiwan, China and Romania, Digilent is able to provide low-cost, expert quality solutions for a variety of customer needs

Digilent Inc. is a leading electrical engineering products company serving students, universities, and OEM's worldwide with technology-based educational design tools. Based in Pullman Washington USA, Digilent designs, manufactures, and distributes its electronic design tools on a worldwide basis. Since its founding in 2000, Digilent products can now be found in over 2000 universities in more than 70 countries throughout the world. As a multinational company with offices in the US, Taiwan, China and Romania, Digilent is able to provide low-cost, expert quality solutions for a variety of customer needs

Digilent Inc. is a leading electrical engineering products company serving students, universities, and OEM's worldwide with technology-based educational design tools. Based in Pullman Washington USA, Digilent designs, manufactures, and distributes its electronic design tools on a worldwide basis. Since its founding in 2000, Digilent products can now be found in over 2000 universities in more than 70 countries throughout the world. As a multinational company with offices in the US, Taiwan, China and Romania, Digilent is able to provide low-cost, expert quality solutions for a variety of customer needs

Digilent Inc. is a leading electrical engineering products company serving students, universities, and OEM's worldwide with technology-based educational design tools. Based in Pullman Washington USA, Digilent designs, manufactures, and distributes its electronic design tools on a worldwide basis. Since its founding in 2000, Digilent products can now be found in over 2000 universities in more than 70 countries throughout the world. As a multinational company with offices in the US, Taiwan, China and Romania, Digilent is able to provide low-cost, expert quality solutions for a variety of customer needs

Digilent Inc. is a leading electrical engineering products company serving students, universities, and OEM's worldwide with technology-based educational design tools. Based in Pullman Washington USA, Digilent designs, manufactures, and distributes its electronic design tools on a worldwide basis. Since its founding in 2000, Digilent products can now be found in over 2000 universities in more than 70 countries throughout the world. As a multinational company with offices in the US, Taiwan, China and Romania, Digilent is able to provide low-cost, expert quality solutions for a variety of customer needs

For technical support contact support@digilentinc.com.

Products

chipKIT PGM Programmer/Debugger

$26.99

Buy Now

The chipKIT™ PGM by Digilent (410-242) is a simple, low-cost module that supports in-system programming and debugging of applications written for PIC® MCU-based microcontroller boards such as the chipKIT™ and Cerebot boards.

The chipKIT PGM is designed to work with the MPLAB® v8 and MPLAB® X IDE. This allows the chipKIT boards, for example, to be used as a more traditional microcontroller development platform.

  • Supports Microchip`s 3.3V devices only
  • Intended for use with the chipKIT Max32™, Uno32™, uC32™, and the Cerebot MX3cK
  • Includes USB A-Mini B cable and a right-angle 6 pin header

Digilent is a trusted third-party tool provider.




Digilent JTAG-USB Programming Cable

$52.59

Buy Now

The JTAG-USB (Digilent 250-003) cable allows you to use your PC to connect to a JTAG scan chain or to access an SPI interface on a board equipped with the appropriate 6-pin header. In this way, you can program devices on Digilent programmable logic boards using the Digilent Adept Suite and MCHP Serial Flash Programming Utility (SFPU) for CPG products.

Note: This is a special-order cable for use with the Synopsys Metaware IDE debugger and MCHP Serial Flash Programming Utility for CPG products.


Digilent is a trusted third-party tool provider.


http://www.matrixtsl.com
Halifax, United Kingdom
Phone: 01422 252380
Fax: 01422 252381

Matrix Technology Solutions provides teaching and learning services in numerous fields including mathematics, science, electronics, and PIC-micro programming. Matrix also provides a range of courses on PIC-micro programming, PIC-micro robotics systems. Flowcode is an advanced graphical programming language for microcontrollers. The great advantage of Flowcode is that it allows those with little to no programming experience to create complex electronic systems in minutes. Flowcode is available in multiple languages and supports the PIC micro, dsPIC, and PIC24 series of microcontrollers. Matrix produces a flexible PIC-micro microcontroller programmer/development board for a range of 8-, 18-, 28- and 40-pin PIC micros.

For technical support, please visit http://www.matrixtsl.com/sup_menu.php or call 01422 252380.


http://www.segger.com
Hilden, Germany
Phone: +49 2013-2878-0

SEGGER develops hardware and software development tools specifically for embedded systems.  We understand the needs and timelines of the modern embedded developer and mold our products around them with unparalleled performance and reliability. Founded in 1992, SEGGER is a privately held ISO9001:2008 company and is steadily growing. Based out of Hilden Germany, with distributors on all continents and an office in Massachusetts, SEGGER offers its full product range worldwide.

SEGGER software products include: embOS (RTOS), emWin (GUI), emFile (File System), emUSB (USB Host and Device Stack), embOS/IP (TCP/IP Stack), and emLoad (Boot Loader). These are all optimized for minimum memory usage, while achieving maximum performance.  SEGGER makes use of its own RTOS and middleware solutions to create highly integrated, cost-effective, development and programming tools known as the industry leading J-Link/J-Trace family of emulators and the Flasher (stand-alone flash programmer). SEGGER cuts software development time for embedded applications by offering affordable, high-quality, flexible, and easy-to-use tools and software components allowing developers to focus on their applications.

For Technical Support please contact support@segger.com.

Products

SEGGER J-Link Debug Probe

$378.00

Buy Now

The J-Link BASE Debug Probe is a USB-powered in-circuit debugger supporting PIC32 devices. Based on a 32-bit RISC CPU, it can communicate at high speed with supported target devices. J-Link is a great tool for flash programming and debugging in development and production environments. Note: J-Link is fully supported in MPLAB X IDE v2.15.

Features include:

  • USB-powered and plug-and-play compatible
  • Direct download into flash memory
  • Download speed up to 1 MByte/second
  • Unlimited breakpoints in flash memory
  • Remote Server included allowing use of J-Link remotely via TCP/IP
  • Supports JTAG chains with multiple devices
  • Cross-platform support Windows, Linux, Mac OS X
  • SDK available

SEGGER is a trusted third-party tool provider

 Note: An adapter cable is available to connect SEGGER J-Link to RJ11 connectors, it's available from SEGGER's website:


J-Link Microchip Adapter


http://www.softlog.com
Or-Yehuda, Israel
Phone: +972-544744939
Fax: +972-39527520

Softlog Systems specializes in In-Circuit Serial Programming (ICSP™) for Microchip microcontrollers. With over 12 years experience in delivering high-performance, cost-effective ICSP solutions used in the manufacturing of millions of products worldwide, Softlog is the vendor of choice for companies interested in reducing manufacturing costs and accelerating time-to-market. Softlog Systems ICP product line comprises several high -speed, production-grade in-circuit programmers, each of which offers a set of robust features and flexible options that can be adapted to each customer´s specific production requirements. Whether you need high-performance single-channel programming or 4-channel gang programming, a portable programmer for field upgrades, or cutting-edge security software to protect your intellectual property, Softlog has the right solution at the right price.

For Technical Support, please email support@softlog.com or call +972-39527316

Products

Softlog SEC-DS Secure Programming Upgrade for ICP2 Programmers

$499.00

Buy Now

The SEC-DS Secure Programming Upgrade can be applied to any Softlog ICP2 programmer. It dramatically reduces the risk of unauthorized reconstruction of hex files, and also limits how many times the hex file can be programmed. The secure programming upgrade must be installed by a user with administrative (ADMIN) privileges, and internet access is required. Once installed, the programmer can be delivered to a contract manufacturer or other un-privileged user. Programming is then controlled by environment files created by the ADMIN with strong encryption.

Softlog is a trusted Third-Party Tool provider.

Softlog SEC4CH-DS Secure Programming Upgrade for ICP2GANG Programmers

$799.00

Buy Now

The SEC4CH-DS Secure Programming Upgrade can be applied to any Softlog ICP2GANG programmer. It dramatically reduces the risk of unauthorized reconstruction of hex files, and also limits how many times the hex file can be programmed. The secure programming upgrade must be installed by a user with administrative (ADMIN) privileges, and internet access is required. Once installed, the programmer can be delivered to a contract manufacturer or other un-privileged user. Programming is then controlled by environment files created by the ADMIN with strong encryption.

Softlog is a trusted Third Party Tool provider

Softlog ICP2 ICSP Production Programmer

$399.00

Buy Now

The ICP2 Production Quality In-Circuit (ICSP) Programmer is a cost-effective programmer that operates with a PC or as a standalone unit, and programs 8-bit PIC® MCUs and serial EEPROMs. It features fast programming, 250mA Vdd drive current, programmable Vdd (2.0 to 5.5V) and Vpp (2.0 to 13.5V), programmable delay between Vdd and Vpp (0.1 to 250ms), programmable clock/data speed (500KHz to 2.5MHz) and on-board 1MByte flash memory.

Softlog is a trusted Third Party Tool provider

Softlog ICP2(G3) ICSP Production Programmer

$449.00

Buy Now

The ICP2(G3) Production Quality In-Circuit Programmer is a cost-effective programmer that operates with a PC or as a standalone unit. It programs 8-bit PIC® MCUs and Serial EEPROMs. ICP2(G3) hardware is designed to support popular programming interfaces (ICSP™, JTAG, SWD, UPDI, SPI, QSPI, etc.).

Features:

  •  Very-fast programming
  • 250mA Vdd drive current (per channel)
  • Programmable Vdd (1.8 to 5.5V) and Vpp (1.8 to 13.5V)
  • Programmable clock/data speed (500KHz to 10MHz)
  • On-board 32MByte flash memory per channel for non-volatile storage of the HEX

 Softlog is a trusted third-party tool provider.

 

Softlog ICP2-DP ICSP Production Programmer

$649.00

Buy Now

The ICP2-DP Production Quality In-Circuit (ICSP) Programmer is a cost-effective programmer that operates with a PC or as a standalone unit. It programs 8-bit PIC® MCUs, 16-bit PIC MCUs & dsPIC® DSCs, and Serial EEPROMs. It features fast programming, 250mA Vdd drive current, programmable Vdd (2.0 to 5.5V) and Vpp (2.0 to 13.5V), programmable delay between Vdd and Vpp (0.1 to 250ms), programmable clock/data speed (500KHz to 2.5MHz), on-board 1MByte flash memory and Windows® DLL functions and command-line interface for automatic programming.

Softlog is a trusted Third Party Tool provider

Softlog ICP2(G3)-DP ICSP Production Programmer

$699.00

Buy Now

The ICP2(G3)-DP Production Quality In-Circuit Programmer is a cost-effective programmer that operates with a PC or as a standalone unit. It programs 8-bit PIC® MCUs, 16-bit PIC MCUs & dsPIC® DSCs and Serial EEPROMs. ICP2(G3)-DP hardware is designed to support popular programming interfaces (ICSP™, JTAG, SWD, UPDI, SPI, QSPI, etc.)

Features:

  • Very fast programming
  • 250mA Vdd drive current
  • Programmable Vdd (1.8 to 5.5V) and Vpp (1.8 to 13.5V)
  • Programmable clock/data speed (500KHz to 10MHz)
  • On-board 32MByte flash memory for non-volatile storage of the HEX (2 environments)
  • Windows® DLL functions and command-line interface for high-volume automatic programming

Softlog is a trusted third-party tool provider.

 

Softlog ICP2GANG-DP 4-Channel ICSP Production Gang Programmer

$1459.00

Buy Now

The ICP2GANG-DP Production Quality In-Circuit (ICSP) 4-Channel (expandable up to 64 channels) GANG Programmer is a cost-effective programmer that operates with a PC or as a standalone unit and simultaneously programs 8-bit PIC® MCUs, 16-bit PIC MCUs & dsPIC® DSCs, and serial EEPROMs. It features ultra fast programming, 250mA Vdd drive current (per channel), programmable Vdd (2.0 to 5.5V) and Vpp (2.0 to 13.5V), programmable delay between Vdd and Vpp (0.1 to 250ms), programmable clock/data speed (500KHz to 2.5MHz), on-board 1MByte flash memory (per channel) and Windows® DLL functions and command-line interface for high volume automatic programming.

Softlog is a trusted Third Party Tool provider

Softlog ICP2GANG(G3)-DP 4-Channel ICSP Production Gang Programmer

$1499.00

Buy Now

The ICP2GANG(G3)-DP Production Quality In-Circuit 4-channel (expandable to 64 channels) GANG programmer is a cost-effective programmer that operates with a PC or as a standalone unit and simultaneously programs 8-bit PIC® MCUs, 16-bit PIC MCUs & dsPIC® DSCs, and serial EEPROMs. ICP2GANG(G3)-DP hardware is designed to support popular programming interfaces (ICSP™, JTAG, SWD, UPDI, SPI, QSPI, etc.)

Features:

  • Very fast programming
  • 250mA Vdd drive current (per channel)
  • Programmable Vdd (1.8 to 5.5V) and Vpp (1.8 to 13.5V)
  • Programmable clock/data speed (500KHz to 10MHz)
  • On-board 32MByte flash memory per channel for non-volatile storage of the HEX (2 environments)
  • Windows® DLL functions and command-line interface for high-volume automatic programming

Softlog is a trusted third-party tool provider.

 

Softlog ICP2GANG 4-channel ICSP Production Gang Programmer

$799.00

Buy Now

The ICP2GANG Production Quality In-Circuit (ICSP) 4-Channel (expandable to 64 channels) GANG programmer is a cost-effective programmer that operates with a PC or as a standalone unit and simultaneously programs 8-bit PIC® MCUs and serial EEPROMS. It features ultra fast programming, 250mA Vdd drive current (per channel), programmable Vdd (2.0 to 5.5V) and Vpp (2.0 to 13.5V), programmable delay between Vdd and Vpp (0.1 to 250 ms), programmable clock/data speed (500KHz to 2.5MHz), on-board 1MByte flash memory (per channel).

Softlog is a trusted Third Party Tool provider

Softlog ICP2GANG(G3) 4-Channel ICSP Production Gang Programmer

$849.00

Buy Now

The ICP2GANG(G3) Production Quality In-Circuit 4-Channel (expandable to 64 channels) GANG programmer is a cost-effective programmer that operates with a PC or as a standalone unit and simultaneously programs 8-bit PIC® MCUs and serial EEPROMs. ICP2GANG(G3) hardware is designed to support popular programming interfaces (ICSP™, JTAG, SWD, UPDI, SPI, QSPI, etc.)

Features:

  • Very-fast programming
  • 250mA Vdd drive current (per channel)
  • Programmable Vdd (1.8 to 5.5V) and Vpp (1.8 to 13.5V)
  • Programmable clock/data speed (500KHz to 10MHz)
  • On-board 32MByte flash memory per channel for non-volatile storage of the HEX (2 environments)


Softlog is a trusted third-party tool provider.

 

Softlog ICP2GANG-DS ICSP Secure Production Gang Programmer

$1599.00

Buy Now

The ICP2GANG-DS Production Quality ICSP Secure GANG Programmer is a 4-channel in-circuit programmer (expandable up to 64 channels) that operates with a PC or as a standalone unit and simultaneously programs 8-bit PIC® MCUs and serial EEPROMs. The secure programming feature dramatically reduces the risk of unauthorized reconstruction of hex files, and also limits how many times the hex file can be programmed. It features ultra fast programming, 250mA Vdd drive current (per channel), programmable Vdd (2.0 to 5.5V) and Vpp (2.0 to 13.5V), programmable delay between Vdd and Vpp (0.1 to 250 ms), programmable clock/data speed (500KHz to 2.5 MHz), on-board 1MByte flash memory (per channel) and Windows® DLL functions and command-line interface for high volume automatic programming.

Softlog is a trusted Third Party Tool provider

Softlog ICP2GANG(G3)-DS ICSP Secure Production Gang Programmer

$1649.00

Buy Now

The ICP2GANG(G3)-DS Production Quality ICSP Secure GANG Programmer is a 4-channel in-circuit programmer (expandable up to 64 channels) that operates with a PC or as a standalone unit and simultaneously programs 8-bit PIC® MCUs and serial EEPROMs. The secure programming feature dramatically reduces the risk of unauthorized reconstruction of hex files, and also limits how many times the hex file can be programmed. ICP2GANG(G3)-DS hardware is designed to support popular programming interfaces (ICSP™, JTAG, SWD, UPDI, SPI, QSPI, etc.)

Features:

  • Very fast programming
  • 250mA Vdd drive current (per channel)
  • Programmable Vdd (1.8 to 5.5V) and Vpp (1.8 to 13.5V)
  • Programmable clock/data speed (500KHz to 10MHz)
  • On-board 32MByte flash memory per channel for non-volatile storage of the HEX (2 environments)
  • Windows® DLL functions and command-line interface for high-volume automatic programming

Softlog is a trusted third-party tool provider. 

 

Softlog ICP2-DS ICSP Secure Production Programmer

$899.00

Buy Now

The ICP2-DS Production Quality ICSP Secure Programmer is an in-circuit programmer that operates with a PC or as a standalone unit, and programs 8-bit PIC® MCUs and serial EEPROMs. The secure programming feature dramatically reduces the risk of unauthorized reconstruction of hex files, and also limits how many times the hex file can be programmed. It features fast programming, 250 mA Vdd drive current, programmable Vdd (2.0 to 5.5V) and Vpp (2.0 to 13.5V), programmable delay between Vdd and Vpp (0.1 to 240ms), programmable clock/data speed (500KHz to 2.5MHz), 1MByte flash memory, Windows® DLL functions and command-line interface for high volume automatic programming.

Softlog is a trusted Third Party Tool provider

Softlog ICP2(G3)-DS ICSP Secure Production Programmer

$919.00

Buy Now

The ICP2(G3)-DS Production Quality Secure Programmer is an in-circuit programmer that operates with a PC or as a standalone unit, and programs 8-bit PIC® MCUs and serial EEPROMs. The secure programming feature dramatically reduces the risk of unauthorized reconstruction of hex files, and also limits how many times the hex file can be programmed.
ICP2(G3)-DS hardware is designed to support popular programming interfaces (ICSP™, JTAG, SWD, UPDI, SPI, QSPI, etc.)

Features:

  • Very fast programming
  • 250mA Vdd drive current
  • Programmable Vdd (1.8 to 5.5V) and Vpp (1.8 to 13.5V)
  • Programmable clock/data speed (500KHz to 10MHz)
  • On-board 32MByte flash memory for non-volatile storage of the HEX (2 environments)
  • Windows® DLL functions and command-line interface for high-volume automatic programming

Softlog is a trusted third-party tool provider.

 

Softlog ICP2(HC) ICSP High-Current Production Programmer

$599.00

Buy Now

The ICP2(HC) Production Quality ICSP High Current Programmer is a cost-effective in-cicuit programmer that operates with a PC or as a standalone unit, and programs 8-bit PIC® MCUs and serial EEPROMs. The unit includes a universal power adapter (100-240 VAC to 12 VDC) and is designed to program target boards with high current requirements. It features fast programming, 1000mA Vdd drive current, 100mA Vpp clock/data current, programmable Vdd (2.0 to 5.5V) and Vpp (2.0 to 13.5V), programmable delay between Vdd and Vpp (0.1 to 250ms), programmable clock/data speed (500KHz to 2.5 MHz), and on-board 1MByte flash memory. Softlog is a trusted Third Party Tool provider

Softlog ICP2PORT Portable In-Circuit Production Programmer

$199.00

Buy Now

A member of the ICP family of high-speed, production-grade in-circuit programmers. This compact, battery-powered device supports up to six different programming environments, making it an ideal, low-cost solution for field upgrades.

Programs Microchip 8-bit MCUs and serial EEPROMs. It features fast programming, 50mA Vdd drive current, programmable Vdd (2.0 to 5.5V) and Vpp (2.0 to 13.5V), programmable Vdd source (programmer or target), programmable clock/data speed (500 KHz to 10 MHz) and 4 MB on-board flash memory. Includes a counter to limit the number of devices programmed. Powered by 3 AAA batteries, USB, or Adapter.

Softlog is a trusted 3rd Party Tool provider

Softlog ICP2PORT(G3) Portable In-Circuit Production Programmer

$299.00

Buy Now

A member of the ICP(G3) family of high-speed, production-grade in-circuit programmers. This compact, battery-powered device supports up to six different programming environments, making it an ideal, low-cost solution for field upgrades.

ICP2PORT(G3) programs Microchip 8-bit MCUs and serial EEPROMs. ICP2PORT(G3) hardware is designed to support popular programming interfaces (ICSP™, JTAG, SWD, UPDI, SPI, QSPI, etc.)

Softlog ICP2PORT-P Portable In-Circuit Production Programmer

$249.00

Buy Now

A member of the ICP family of high-speed, production-grade in-circuit programmers. This compact, battery-powered device supports up to six different programming environments, making it an ideal, low-cost solution for field upgrades.

Programs Microchip 8-bit PIC® MCUs, 16-bit PIC MCUs & dsPIC® DSCs, and serial EEPROMs. It features fast programming, 50 mA Vdd drive current, programmable Vdd (2.0 to 5.5V) and Vpp (2.0 to 13.5V), programmable Vdd source (programmer or target), programmable clock/data speed (500 KHz to 10MHz), 4 MB on-board flash memory, and a counter to limit the number of devices programmed. Powered by 3 AAA batteries, USB, or Adapter.

Softlog is a trusted 3rd Party Tool provider

Softlog ICP2PORT(G3)-P Portable In-Circuit Production Programmer

$359.00

Buy Now

A member of the ICP(G3) family of high-speed, production-grade in-circuit programmers. This compact, battery-powered device supports up to six different programming environments, making it an ideal, low-cost solution for field upgrades.

ICP2PORT(G3)-P programs Microchip 8-bit PIC® MCUs, 16-bit PIC MCUs & dsPIC® DSCs, and serial EEPROMs. ICP2PORT(G3)-P hardware is designed to support popular programming interfaces (ICSP™, JTAG, SWD, UPDI, SPI, QSPI, etc.)

Softlog ICP2PORT-PX Portable In-Circuit Production Programmer

$299.00

Buy Now

A member of the ICP family of high-speed, production-grade in-circuit programmers. This compact, battery-powered device supports up to six different programming environments, making it an ideal, low-cost solution for field upgrades.

ICP2PORT-PX programs Microchip 8-bit PIC® MCUs, 16-bit PIC MCUs & dsPIC® DSCs, 32-bit PIC MCUs, and serial EEPROMs. It features fast programming, 50 mA Vdd drive current, programmable Vdd (2.0 to 5.5V) and Vpp ( 2.0 to 13.5V), programmable Vdd source (programmer or target), programmable clock/data speed (500 KHz to 10MHz), 4 MB on-board flash memory, and a counter to limit the number of devices programmed. Powered by 3 AAA batteries, USB, or Adapter.

Softlog is a trusted 3rd Party Tool provider

Softlog ICP2PORT(G3)-PX Portable In-Circuit Production Programmer

$399.00

Buy Now

A member of the ICP(G3) family of high-speed, production-grade in-circuit programmers. This compact, battery-powered device supports up to six different programming environments, making it an ideal, low-cost solution for field upgrades.

ICP2PORT(G3)-PX programs Microchip 8-bit PIC® MCUs, 16-bit PIC MCUs & dsPIC® DSCs, 32-bit PIC MCUs and serial EEPROMs. ICP2PORT(G3)-PX hardware is designed to support popular programming interfaces (ICSP™, JTAG, SWD, UPDI, SPI, QSPI, etc.)

Softlog ICP2-DPX ICSP Production Programmer

$749.00

Buy Now

The ICP2-DPX Production Quality In-Circuit (ICSP) Programmer is a cost-effective programmer that operates with a PC or as a standalone unit. It programs 8-bit PIC® MCUs, 16-bit PIC MCUs & dsPIC® DSCs, 32-bit PIC MCUs, and Serial EEPROMs.

ICP2-DPX features fast programming, 250mA Vdd drive current, programmable Vdd (2.0 to 5.5V) and Vpp (2.0 to 13.5V), programmable delay between Vdd and Vpp ( 0.1 to 250ms), programmable clock/data speed (500KHz to 2.5MHz), on-board 1MByte flash memory and Windows® DLL functions and command-line interface for automatic programming.

Softlog is a trusted 3rd Party Tool provider

Softlog ICP2(G3)-DPX ICSP Production Programmer

$749.00

Buy Now

The ICP2(G3)-DPX Production Quality In-Circuit Programmer is a cost-effective programmer that operates with a PC or as a standalone unit. It programs 8-bit PIC® MCUs, 16-bit PIC MCUs & dsPIC® DSCs, 32-bit PIC MCUs and Serial EEPROMs. ICP2(G3)-DPX hardware is designed to support popular programming interfaces (ICSP™, JTAG, SWD, UPDI, SPI, QSPI, etc.)

Features: 

  • Very-fast programming
  • 250mA Vdd drive current (per channel)
  • Programmable Vdd (1.8 to 5.5V) and Vpp (1.8 to 13.5V)
  • Programmable clock/data speed (500KHz to 10MHz)
  • On-board 32MByte flash memory per channel for non-volatile storage of the HEX (2 environments)
  • Windows® DLL functions and command-line interface for high-volume automatic programming

 Softlog is a trusted third-party tool provider.

 

Softlog ICP2GANG-DPX 4-Channel ICSP Gang Programmer

$1599.00

Buy Now

The ICP2GANG-DPX Production Quality In-Circuit (ICSP) 4-Channel (expandable up to 64 channels) GANG Programmer is a cost-effective programmer that operates with a PC or as a standalone unit and simultaneously programs 8-bit PIC® MCUs, 16-bit PIC MCUs & dsPIC® DSCs, 32-bit PIC MCUs, and serial EEPROMs.

ICP2GANG-DPX features ultra fast programming, 250mA Vdd drive current (per channel), programmable Vdd (2.0 to 5.5V) and Vpp (2.0 to 13.5V), programmable delay between Vdd and Vpp (0.1 to 250ms), programmable clock/data speed (500KHz to 2.5MHz), on-board 1MByte flash memory per channel and Windows® DLL functions and command-line interface for high volume automatic programming.

Softlog is a trusted 3rd Party Tool provider

Softlog ICP2GANG(G3)-DPX ICSP 4-Channel Gang Programmer

$1599.00

Buy Now

The ICP2GANG(G3)-DPX Production Quality In-Circuit 4-Channel (expandable to 64 channels) GANG programmer is a cost-effective programmer that operates with a PC or as a standalone unit and simultaneously programs 8-bit PIC® MCUs, 16-bit PIC MCUs & dsPIC® DSCs, 32-bit PIC MCUs and serial EEPROMs. ICP2GANG(G3)-DPX hardware is designed to support popular programming interfaces (ICSP™, JTAG, SWD, UPDI, SPI, QSPI, etc.)

Features:

  • Very-fast programming
  • 250mA Vdd drive current (per channel)
  • Programmable Vdd (1.8 to 5.5V) and Vpp (1.8 to 13.5V)
  • Programmable clock/data speed (500KHz to 10MHz)
  • On-board 32MByte flash memory per channel for non-volatile storage of the HEX (2 environments)
  • Windows® DLL functions and command-line interface for high-volume automatic programming


Softlog is a trusted third-party tool provider.

 

Softlog ICP2COMBO-DPX 12-Channel Gang Programmer

$5499.00

Buy Now

The ICP2COMBO-DPX-12 Production Quality In-Circuit (ICSP) 12-Channel (expandable up to 60 channels) GANG Programmer is a cost-effective programmer that operates with a PC or as a standalone unit and simultaneously programs 8-bit PIC® MCUs, 16-bit PIC MCUs & dsPIC® DSCs, 32-bit PIC MCUs, and serial EEPROMs.

Features:

  • Ultra fast programming
  • Built-in opto-relay barrier for target lines
  • Galvanic isolation of control lines
  • 250mA Vdd drive current (per channel)
  • Programmable Vdd (2.0 to 5.5V) and Vpp (2.0 to 13.5V)
  • Programmable delay between Vdd and Vpp (0.1 to 250ms)
  • Programmable clock/data speed (500KHz to 2.5MHz)
  • On-board 4MByte flash memory per channel for non-volatile storage of the HEX  (6 environments)
  • Windows® DLL functions and command-line interface for high-volume automatic programming
Softlog is a trusted Third-Party Tool Provider

Softlog ICP2COMBO-DPX-8 8-Channel Gang Programmer

$3669.00

Buy Now

The ICP2COMBO-DPX-8 Production Quality In-Circuit (ICSP) 8-Channel (expandable up to 64 channels) GANG Programmer is a cost-effective programmer that operates with a PC or as a standalone unit and simultaneously programs 8-bit PIC® MCUs, 16-bit PIC MCUs & dsPIC® DSCs, 32-bit PIC MCUs, and serial EEPROMs.

Features:

  • Ultra fast programming
  • Built-in opto-relay barrier for target lines
  • Galvanic isolation of control lines
  • 250mA Vdd drive current (per channel)
  • Programmable Vdd (2.0 to 5.5V) and Vpp (2.0 to 13.5V)
  • Programmable delay between Vdd and Vpp (0.1 to 250ms)
  • Programmable clock/data speed (500KHz to 2.5MHz)
  • On-board 4MByte flash memory per channel for non-volatile storage of the HEX  (6 environments)
  • Windows® DLL functions and command-line interface for high-volume automatic programming
Softlog is a trusted Third-Party Tool Provider

Softlog ICP2COMBO(G3)-DPX-8 8-Channel Gang Programmer

$3669.00

Buy Now

The ICP2COMBO(G3)-DPX-8 Production Quality In-Circuit (ICSP) 8-channel (expandable up to 64 channels) GANG Programmer is a cost-effective programmer that operates with a PC or as a standalone unit and simultaneously programs 8-bit PIC® MCUs, 16-bit PIC MCUs & dsPIC® DSCs, 32-bit PIC MCUs, and serial EEPROMs. ICP2COMBO(G3)-DPX-8 hardware is designed to support popular programming interfaces (ICSP™, JTAG, SWD, UPDI, SPI, QSPI, etc.)

Features:

  • Ultra-fast programming
  • Built-in opto-relay barrier for target lines
  • Galvanic isolation of control lines
  • 250mA Vdd drive current (per channel)
  • Programmable Vdd (1.8 to 5.5V) and Vpp (1.8 to 13.5V)
  • Programmable clock/data speed (500KHz to 10MHz)
  • On-board 32MByte flash memory per channel for non-volatile storage of the HEX (6 environments)
  • Windows® DLL functions and command-line interface for high-volume automatic programming

Softlog is a trusted third-party tool provider.

 

Softlog ICP2COMBO-12 12-Channel Gang Programmer

$2999.00

Buy Now

The ICP2COMBO-12 Production Quality In-Circuit (ICSP) 12-Channel (expandable up to 60 channels) GANG Programmer is a cost-effective programmer that operates with a PC or as a standalone unit and simultaneously programs 8-bit PIC® MCUs and serial EEPROMs.

Features:

  • Ultra-fast programming
  • Built-in opto-relay barrier for target lines
  • Galvanic isolation of control lines
  • 250mA Vdd drive current (per channel)
  • Programmable Vdd (2.0 to 5.5V) and Vpp (2.0 to 13.5V)
  • Programmable delay between Vdd and Vpp (0.1 to 250ms)
  • Programmable clock/data speed (500KHz to 2.5MHz)
  • On-board 4MByte flash memory per channel for non-volatile storage of the HEX  (6 environments)
Softlog is a trusted Third-Party Tool Provider

Softlog ICP2COMBO(G3)-12 12-Channel Gang Programmer

$2999.00

Buy Now

The ICP2COMBO(G3)-12 Production Quality In-Circuit (ICSP) 12-channel (expandable up to 60 channels) GANG Programmer is a cost-effective programmer that operates with a PC or as a standalone unit and simultaneously programs 8-bit PIC® MCUs and serial EEPROMs. ICP2COMBO(G3)-12 hardware is designed to support popular programming interfaces (ICSP™, JTAG, SWD, UPDI, SPI, QSPI, etc.)

Features:

  • Ultra-fast programming
  • Built-in opto-relay barrier for target lines
  • Galvanic isolation of control lines
  • 250mA Vdd drive current (per channel)
  • Programmable Vdd (1.8 to 5.5V) and Vpp (1.8 to 13.5V)
  • Programmable clock/data speed (500KHz to 10MHz)
  • On-board 32MByte flash memory per channel for non-volatile storage of the HEX (6 environments)


Softlog is a trusted third-party tool provider.

 

Softlog ICP2COMBO-8 8-Channel Gang Programmer

$1999.00

Buy Now

The ICP2COMBO-8 Production Quality In-Circuit (ICSP) 8-Channel (expandable up to 64 channels) GANG Programmer is a cost-effective programmer that operates with a PC or as a standalone unit and simultaneously programs 8-bit PIC® MCUs and serial EEPROMs.

Features:

  • Ultra-fast programming
  • Built-in opto-relay barrier for target lines
  • Galvanic isolation of control lines
  • 250mA Vdd drive current (per channel)
  • Programmable Vdd (2.0 to 5.5V) and Vpp (2.0 to 13.5V)
  • Programmable delay between Vdd and Vpp (0.1 to 250ms)
  • Programmable clock/data speed (500KHz to 2.5MHz)
  • On-board 4MByte flash memory per channel for non-volatile storage of the HEX  (6 environments)
Softlog is a trusted Third-Party Tool Provider

Softlog ICP2COMBO(G3)-8 8-Channel Gang Programmer

$1999.00

Buy Now

The ICP2COMBO(G3)-8 Production Quality In-Circuit (ICSP) 8-channel (expandable up to 64 channels) GANG Programmer is a cost-effective programmer that operates with a PC or as a standalone unit and simultaneously programs 8-bit PIC® MCUs and serial EEPROMs. ICP2COMBO(G3)-8 hardware is designed to support popular programming interfaces (ICSP™, JTAG, SWD, UPDI, SPI, QSPI, etc.)

Features:

  • Ultra-fast programming
  • Built-in opto-relay barrier for target lines
  • Galvanic isolation of control lines
  • 250mA Vdd drive current (per channel)
  • Programmable Vdd (1.8 to 5.5V) and Vpp (1.8 to 13.5V)
  • Programmable clock/data speed (500KHz to 10MHz)
  • On-board 32MByte flash memory per channel for non-volatile storage of the HEX (6 environments)

Softlog is a trusted third-party tool provider. 

 


http://www.totalphase.com/
Sunnyvale, California, United States of America
Phone: +1 (408) 850-6502
Fax: +1 (408) 850-6501

Total Phase is a leading provider of embedded systems development tools for engineers all over the world. Total Phase's mission is to create powerful, high-quality, and affordable solutions for the embedded engineer. For years, Total Phase has developed products that have become tools of choice for Fortune 500 companies, small businesses, and research institutions alike. The simplicity and ease of integration of Total Phase products have led to many unique engineering solutions. As customers build Total Phase products into their systems, Total Phase actively incorporates their feedback, building the solutions that engineers find most valuable. Customers are able to leverage these solutions to build higher-quality products for their own markets.

For technical support, please visit www.totalphase.com/support or call +1 (408) 850-6502.



Recognized Third-Party Tool Providers


Acroview Technology Co., Ltd.

http://www.acroview.com
Shenzhen, China
Phone: +86-755-26971006
Fax: +86-755-26971258

Acroview is a company with more than 10 years experience in programmer research & development, manufacturing and service providing. Equipped with the world’s leading technology, we focus on providing our customers with more innovative programming products and solutions. Our products include universal programmers, production programmers, online programmers as well as emulators. We are convinced that with our devotion and pursuit of quality and advanced technology, more and more customers will choose and trust Acroview as a reliable partner.


Advin Systems Inc.

http://www.advin.com
Sunnyvale, California, United States of America
Phone: 408-243-7000
Fax: 1-877-727-9610

Device programmers and gang programmers.


Algocraft Srl

http://www.algocraft.com
Villotta di Chions, Italy
Phone: +39 0434 630415

Algocraft is a high-tech company whose core business is to design, develop and market a wide range of professional systems dedicated to the manufacturing and testing of electronic boards. Our main series of products is the WriteNow! Series of In-System Programmers. The WriteNow! technology is targeted to on-board (in-system) programming and has been designed to achieve high-speed programming, while maintaining reliability and flexibility. The WriteNow! technology has been created with speed and reliability as key features, and employs state-of-the art components and techniques to give birth to the WriteNow! Series of In-System Programmers. We also produce a second brand, called Write!BEFORE, a socket programmer specialized in MCUs, able to program up to 8 devices at once and based on WriteNow! Technology.


Amfeltec Corporation

http://www.amfeltec.com
Markham, Ontario, Canada
Phone: 905-604-6438

Amfeltec Corporation is a leading provider of complex and innovative solutions for the world’s diverse electronics markets. One of our products, the In-Circuit Programmer/Loader (EasyLoader) is  a standalone device that provides a flexible and cost-effective solution for electronics device production and electronics device development. It saves your company huge chunks of production employee working time, making lengthy pre-programming tasks many times quicker. Upgrade your code on Microchip microcontrollers (such as dsPIC30/dsPIC33/PIC24) at any time during development, testing or production. User-friendliness is maximized: anyone can use it, no matter their qualifications or experience. Program your latest firmware just prior to shipping (customers will always get latest version of your firmware). It can also be sent to customers in the field for firmware updates.


ASCALAB d.o.o

http://www.ascalab.com
Ljubljana, Slovenia
Phone: +386 40 649 101

Ascalab is providing state of the art R&D production of prototypes, small-scale and medium-scale high-tech products which allows us to provide solutions on demand basis. All phases of the product life-cycle are covered: starting with the design of printed circuit boards (PCB) to software development, production, assembly, testing and dispatch respective to the electronics, IoT, medical and manufacturing segments. We offer highest standards of business, project management and software engineering processes with the knowledge of innovative technologies and value added engineering on Windows, Linux, mobile platforms. We have experience in Manufacturing, Healthcare, Metrology, Telemedicine, Insurance, Security industry.The company was founded in 2012 by software experts with proven track of successfully developed and implemented projects in various industries and markets. We are based in Ljubljana, Slovenia.


BPM Microsystems, Inc.

http://www.bpmmicro.com
Houston, Texas, United States of America
Phone: (800) 225-2102
Fax: (713) 688-0920

BPM Microsystems provides both low-volume and high-volume innovative programming solutions used by the leading electronic distributors, contract manufacturers, OEMs, programming centers and semiconductor manufacturers around the world. Our products exhibit the highest up time & reliability, with the most throughput at a lower cost per device. So if you need to program ten devices or ten million, BPM Microsystems offers a full range of programmers that will get the job done faster and improve your bottom line.


Conitec Datensysteme GmbH

http://www.conitec.com
Dieburg, Germany
Phone: +49 6071 92520
Fax: +49 6071 925233

We manufacture device programmers for the 21st Century. Due to its pocket format and power supply independence, our GALEP-5 is the perfect programmer for development and service. It supports 62,000+ devices with the lowest per-device cost in the industry. Its big brother GALEP-5D is a heavy duty production device programmer with up to 240 pin drivers, socket module system, remote control, and dual USB2/LAN port. The new GALEP-5P semi-automatic programming station is a lean solution for after-placement programming and series production. It can process up to 1000 boards/hour at a fraction of the price of a programming robot.


Data I/O Corporation

http://www.data-io.com
Redmond, United States of America
Phone: 800-332-8246
Fax: 425-869-7423

Celebrating 30 years of innovative leadership in the device programming industry, Data I/O Corporation provides manual and automated device programming systems that specifically address the requirements of engineering and manufacturing customers. The Company, which is publicly traded (NASDAQ: DAIO), is headquartered in Redmond, Wash., and has sales and service offices worldwide.


Dataman Programmers Ltd

http://www.dataman.com
Dorchester, Dorset, United Kingdom
Phone: (44) 0 1300 320719
Fax: (44) 0 1300 321012

With 30 years experience Dataman is the world’s leading provider of device programmers. We offer a comprehensive range of programming solutions suitable for every requirement from design and development to large scale production. We are committed to providing continued development, manufacturing and support and to deliver customer specific innovative solutions. All Dataman products come with comprehensive warranties, free lifetime support and free software updates via our website and telephone helpdesk. With offices in both the UK and USA plus distributors in 53 countries worldwide, you can be assured of the very best customer service and support.


DediProg Technology Co., Ltd

http://www.DediProg.com
Taipei, Taiwan
Phone: 886-2-27907932
Fax: 886-2-27907916

DediProg was founded in 2005 in Taiwan and the Shanghai base was established in 2010. Dediprog is a company aiming at the solutions of IC programming of EEPROM, SPI Flash, NOR Flash, NAND FLASH, Microcontroller, eMMC, CPLD and other programmable devices. We not only provide dedicated solutions for engineering development but also offer high efficiency equipment for production. Dediprog always treats customers' needs as our first concern. By designing overall solutions, DediProg is providing the best products which fit customers’ needs and requirements for their target applications.

Products & Services:

  • Dedicated engineering ISP programmers
  • Universal engineering ISP programmers
  • Universal production programmers
  • Semi-auto tape & reel taping machine
  • Automatic IC programming Systems
  • IC programming service
  • Customized solutions according to customer’s request


EETools

http://www.eetools.com
San Jose, California, United States of America
Phone: (408) 263-2221
Fax: (408) 263-2230

EETools is in the center of Silicon Valley. EETools is a solution provider for cost effective universal programmers for PC driven or stand-alone. TopMaxII and ChipMax2 support most of the PIC Microcontrollers. For production programming, ProMax-4G has 4 gang solutions for PC USB interface. We also provide all possible programming adapters for non-standard devices in stock. All of our products are manufactured, supported in the U.S.A. to guarantee product reliability.

For technical support, please click here.


ELNEC s.r.o.

http://www.elnec.com
Presov, Slovakia
Phone: (421) 51 7734328
Fax: (421) 51 7732797

Elnec offers wide range of production and universal programmers, which meet requirements of engineering or manufacturing customers. Our programmers provide programming in single or multiprogramming mode. All programmers are controlled by single control program, which supports over 110,000 programmable devices. PIC-micro devices can be programmed in ZIF socket or through ISP connector (depends on the programmer model). Free technical support (hot-line) and free life-time software update via Internet are available for our customers. All Elnec programmers carry 3-years warranty and are approved by CE laboratory to meet CE requirements.


Elprotronic Inc

http://www.elprotronic.com/
King City, ON, Canada
Phone: +9055390424

Elprotronic Inc. offers flash programming solutions for a wide variety of embedded MCUs. Production programmers for both low and high volume production. Programmers with up to 1MB/s data transfer and built-in galvanic isolation, programmable communication clock up to 20 MHz, real-time current measurement, and both USB and Ethernet connectivity. Supports both Linux and Windows(TM)  ME, 2000, XP, 7, 8, 10.  In addition, Offer customers customized solutions for more challenging production and programming requirements, dependent on the requirements of the hardware.


Embed Inc

http://www.embedinc.com
Littleton, United States of America
Phone: (978) 742-9014

Embed Inc is primarily a consulting company performing electrical, firmware, and software engineering of embedded systems, specializing in Microchip PIC microcontrollers and the circuits around them.  We have worked on well over 100 projects containing Microchip PICs and dsPICs. Embed also makes some physical products, which are mostly aids for developing, testing, and using small embedded systems. Some of these products are available on MicrochipDirect, but for the full product line, see http://www.embedinc.com/products.

For Technical support, please call (978) 742-9014.


HI-LO SYSTEM RESEARCH CO. LTD.

http://www.hilosystems.com.tw
Taipei, Taiwan
Phone: 886-2-8792-3301
Fax: 886-2-8792-3285

HI-LO has been devoted to providing device programmers and programming / testing solutions with reliable quality at reasonable prices for over 30 years. Our product range covers Engineering, Production Programmers, a variety of Automated Device Programming Systems and 3D Lead / Marking Inspection Systems. HI-LO is one of the market leaders with regards to Device Programming Equipment and Programming services in Pan Asia (Hong Kong, Taiwan, China, Japan, etc.).


JTAG Technologies

http://www.jtag.com
Eindhoven, Netherlands
Phone: +31 40 295 0870

JTAG Technologies offers generic test tools for boundary-scan (IEEE 1149.x) compliant devices and Microchip-specific tools for hardware validation and device programming. CoreCommander PIC32 allows the activation of the in-circuit debugger mode to communicate at-speed with on-chip or on-board peripherals. JTAG Technologies also supports the in-system programming of several Microchip parts that use the ICSP or JTAG port via its generic JTAG hardware (PIC16, dsPIC33, PIC32MX, etc.).


LEAP Electronic Co., Ltd.

http://www.leap.com.tw
New Tapei City, Taiwan
Phone: 886-2-2999-1860
Fax: 886-2-2999-9873

Leap Electronic was established in 1980, located in TangChen Industrial Park, Sanchung city, Taipei. To help our customers establish completed development system has always been our priority.  Our company involves in the field of IC test and programming equipments deeply because we ourselves manufacture IC programmer, emulator, IC tester and interface protector in a name of Leap. To promote Leap's products all over the world, Leap obtains ISO 9001 certification and absolutely guarantees customers the best quality.


Lynxar Technologies

http://www.lynxartech.com
Sassuolo, Italy
Phone: +39-0536-840586

Lynxar Technologies is a global, independent, high-tech company, leader in semiconductor device in-system programming for the electronic boards manufacturing industry. Lynxar is setting a new semiconductor device programming standard for the years ahead. DeviceClip, Lynxar flagship product, is currently the market's fastest, most advanced, reliable and easy-to-use ISP platform for the support of every type of Flash-based device.


mcelectronics

http://www.mcelectronics.com.ar
Buenos Aires, Argentina
Phone: +541148225220

mcelectronics produces development kits for PIC microcontrollers. We have products for beginners (Starter Kit Student), tools for USB (Starter Kit USB) and Ethernet (MCE Web Server). We have programmers and debuggers and a universal adapter for programmers. SMD to thru-hole is made easy with our MCE PIM for PIC and dsPIC. We also offer on-line DVD classes from PIC12 to PIC32, connectivity lessons, and ongoing support through the web with on-line technical resources and training books in Spanish.

For technical support, please visit www.mcelectronics.com.ar/soporte or contact soporte@mcelectronics.com.ar.


microEngineering Labs, Inc.

http://www.melabs.com
Colorado Springs, Colorado, United States of America
Phone: (719) 520-5323
Fax: (719) 520-1867

Development tools for PICmicro MCUs including PICBASIC Pro Compiler and Field Programmer for 8-bit PIC microcontrollers.

For Technical Support, please visit http://support.melabs.com/forum.php or contact support@melabs.com.


Phyton, Inc. Microsystems and Development Tools

http://www.phyton.com
Brooklyn, New York, United States of America
Phone: (718) 259-3191
Fax: (718) 259-1539

Phyton produces and sells device programmers for in-system and in-socket programming of Microchip memory devices and embedded microcontrollers. This includes gang production programmers and engineering tools. Currently 9000+ Microchip device-package combinations are supported. Socket adapters for all popular packages are available. All Phyton device programmers can be driven remotely via the DLL or in the command line mode. The software is featured with the project support, simplifies user interface and other helpful features. Phyton also produces in-circuit emulators for SST89C5x series of Microchip microcontrollers.


ProMik GmbH

http://www.promik.com
Nürnberg, Germany
Phone: +49 911 25 26 65 92

Since its beginning in 1995, ProMik has focused on providing state of the art support for programmable microcontrollers and provides systems for development and production, manual and automated systems, and programming services. The company has specialized in supporting applications in automotive electronics and industrial process controls. The company is fully ISO and TS certified. ProMik's solutions include flashing and testing solutions including cell margin analysis to verify the quality of device programming.


SMH Technologies

http://www.smh-tech.com/
Villotta di Chions, Pordenone, Italy
Phone: +39 0434 421 111
Fax: +39 0434 421 111

SMH Technologies is a global, independent, high-tech leader in Silicon Device In-System Programming and related services for the electronic boards manufacturing industry. The FlashRunner series, the company's professional Silicon Device In-System Programming platform, is the result of the decennial experience in micro-code encoding for 8-, 16- and 32-bit processors. FlashRunner helps our customers enhance quality, save time, and optimize manufacturing cycles. SMH Technologies continuously improves their products by releasing new programming algorithms weekly. Thanks to FlashRunner's flexible and modular design, the same algorithms can be used on all of the models.


System General Corp.

http://www.sg.com.tw
Shin-Dian, Taipei, Taiwan
Phone: +886-2-2917-3005 105
Fax: +886-2-2911-1283

Single-site and gang type high-speed universal USB programmers for both labaratory and the production floor. Extremely fast data download and programming speed are features available across all product platforms. Fully automated programming handler is also available for high throughput and mass production.


TOA ELECTRONICS, Inc. Flash Support Group Company

http://www.j-fsg.co.jp/en/index.html
Takanawa, Minatoku, Japan
Phone: +81-3-3444-9316
Fax: +81-3-3444-9312

Flash Support Group Company (FSG) is Leading company in the semiconductor programming tool market, by providing the high quality products and services to satisfy the advanced customer’s needs. Our vision is that improvement of customer satisfaction with Quick and Flexible service and utilization. We provide programmers, automation programming system, serial programmers and device programming service, we can do all proposals about device programming.


Xeltek Inc.

http://www.xeltek.com
Sunnyvale, California, United States of America
Phone: (408) 530-8080
Fax: (408) 530-0096

Xeltek develops and manufactures universal Parallel, ISP, Production and Automated Programmers since 1991. Located in Silicon Valley, Xeltek works closely with neighboring semiconductor companies to build up the largest device library in the industry and provide support for the latest IC chips (i.e. PICs, EEPROM, FLASH, microcontrollers, high density eMMC).  Universal programmers and adapters from the SuperPro® line cover programming demands from engineering development to automated volume production at competitive prices; universal socket adapters support various package types such as PLCC, SOIC, SOP, TSOP, QFP, SDIP and uBGA. As of August 2013, Xeltek supports over 90,000 devices from over 300 IC manufacturers and will continue to release faster programmers to meet new performance expectation for both parallel and in-system (LabVIEW interface) programming technology.