What is the MCP1501 Voltage Reference Building Block Solutions (BBS) kit?
The BB89X25A MCP1501 Voltage Reference BBS Kit is a modular evaluation platform containing several analog and mixed signal devices configured in separate BBS boards. It provides 10 different high-precision voltage reference devices, allowing users to evaluate and implement solutions in system-level applications. Each board can be used independently or in combination with other boards.
What voltage reference variants are included in the kit?
The kit includes 10 MCP1501 High Precision Voltage Reference BBS boards with the following output voltages:
What do I need to use the board?
The boards come fully populated with Surface-Mount Device (SMD) components. For evaluation, you will need:
Depending on the specific application, some or all these components may be required in combination.
What applications or use cases is this kit designed for?
The MCP1501 BBS Kit is designed for the following applications and use cases, including but not limited to:
Why is this kit useful for rapid prototyping?
The BB89X25A MCP1501 BBS Kit speeds up prototyping because it provides a pre-configured set of 10 diverse, precision voltage reference boards that you can test, compare and integrate immediately—no additional design or assembly required. The modular format allows users to seamlessly integrate individual boards into existing systems or configure multiple boards for diverse application requirements.
How do I decide which voltage reference sub-board to use?
Select the board whose output voltage matches the reference voltage required by your system:
How do I power up the MCP1501 Voltage Reference BBS board?
The power-up procedure for each MCP1501 BBS board is:
IMPORTANT: Each variant requires a different minimum VDD. Applying insufficient supply voltage will prevent correct output. Refer to the table below (from MCP1501 datasheet Table 2-1):
Variant | VDD Minimum | VDD Maximum |
MCP1501-10 | 1.65V | 5.5V |
MCP1501-12 | 1.65V | 5.5V |
MCP1501-18 | 2.0V | 5.5V |
MCP1501-20 | 2.25V | 5.5V |
MCP1501-25 | 2.70V | 5.5V |
MCP1501-30 | 3.2V | 5.5V |
MCP1501-33 | 3.5V | 5.5V |
MCP1501-40 | 4.3V | 5.5V |
MCP1501-45 | 4.7V | 5.5V |
MCP1501-50 | 5.2V | 5.5V |
What are the output current capabilities of each board?
Each MCP1501 BBS board outputs a high-precision, buffered reference voltage capable of sinking and sourcing 20 mA of current (±20 mA, TA = +25°C, per datasheet Table 2-1). The absolute maximum output current rating is 30 mA, however sustained operation at ±20 mA is the specified operating limit. This makes the boards suitable not only as references but also as low-current supply rails for other components in a system.
How can I generate a negative voltage reference using this kit?
A negative voltage reference can be generated using any device in the MCP1501 family. The voltage inversion is implemented externally using an MCP6061 op-amp and two equal resistors (10 kΩ, 0.1%). The output of the MCP1501 drives R1, which connects to the inverting input of the MCP6061 amplifier. Since the non-inverting input is biased to ground, the current through R1 also flows through the feedback resistor R2, producing a negative output equal in magnitude to the selected reference voltage. For example, using the MCP1501-25 produces a 2.5V output; using the MCP1501-40 produces a
4.096V output. A
5V supply is required for the MCP6061 in this configuration.
How do I use the MCP1501 as an ADC voltage reference?
The MCP1501 product family was designed to provide a precise, low-noise voltage reference for our ADC families. Connect the OUT pin of the selected MCP1501 BBS board to the VREF pin of your ADC. A typical configuration pairs the MCP1501-25 with the MCP3201 12-bit ADC using a 50Ω series resistor between the reference output and the ADC VREF pin, with a 1 nF and a 2.2 µF capacitor at the MCP1501 output and a 10 µF reservoir capacitor at the ADC VREF pin. The 10 µF capacitor is particularly important for SAR ADCs which draw charge-kick currents during conversion. See Figure 2-6 of the user guide and Figure 5-4 of the MCP1501 datasheet (DS20005474) for the complete recommended circuit.
Live Chat