Microchip Advances Space-Grade Timing with Enhanced Radiation Tolerance and Extended Temperature Performance
The Space CSAC-SA65 combines atomic-clock accuracy with built-in 1 PPS disciplining and low-power consumption
CHANDLER, Ariz., August 13, 2026 — The growing New Space market is fueling demand for smaller, less expensive space hardware to support short-duration missions for applications such as satellite-to-cellular communications, alternative navigation and Earth imaging. Microchip Technology (Nasdaq: MCHP) today announces it expanded its atomic clock portfolio with the radiation-tolerant Space CSAC-SA65, a Chip Scale Atomic Clock designed to deliver precise timing for space systems. The device provides a compact, low-power alternative to traditional radiation-hardened timing solutions, helping developers reduce size, weight, power and cost while maintaining accuracy.
Building on the heritage of Microchip's Space CSAC-SA45, the Space CSAC-SA65 extends radiation tolerance to at least 30 kRad and operates in extended temperature ranges from –40°C to +80°C. Consuming less than 120 mW and occupying less than 17 cc of volume, the device is optimized for size-, weight- and power-constrained satellite designs. Its built-in 1 PPS input and output capabilities support synchronization for satellite systems, while its atomic stability enables extended operation without continuous reliance on external timing references such as Global Navigation Satellite System (GNSS) signals.
“By enabling one of the lowest power atomic clocks to thrive in extreme conditions, even the smallest CubeSat can now fly with atomic accuracy,” said Randy Brudzinski, corporate vice president of Microchip’s frequency and time systems business unit. “The Space CSAC-SA65 brings atomic-clock performance to applications where size, weight, power and cost are tightly constrained, helping developers maintain synchronization and timing accuracy even when external timing references are unavailable.”
Manufactured as a Commercial Off-The-Shelf (COTS) product using radiation-tolerant commercial electronic components, the device can offer shorter lead times and lower overall costs compared to traditional space-grade oscillators. Designed for Low Earth Orbit (LEO) missions, the CSAC-SA65 is well suited for applications including satellite timing and frequency control, satellite clock reference, assured positioning, navigation and timing (PNT), and satellite cross-linking.
Microchip offers an extensive portfolio of clock and timing systems, ranging from miniature component oscillators, to small plug-in timing server cards, to multi-rack time scale systems. As a primary contributor to the world's time, Microchip's timing solutions are trusted, reliable and resilient. For more information, visit Microchip's Clock and Timing Systems web page.
Development Tools
The CSAC-SA65 is supported by Microchip’s Clockstudio™ software for control and analysis of atomic clocks, as well as a CSAC Developer Kit.
Pricing and Availability
The CSAC-SA65 (part number 090-02789-007) is available for purchase. For additional information and to purchase, contact a Microchip sales representative or authorized worldwide distributor.
Resources
High-res images available through Flickr or editorial contact (feel free to publish):
- Application image: www.flickr.com/photos/microchiptechnology/55415868006/sizes/l
About Microchip
Microchip Technology Inc. is a broadline supplier of semiconductors committed to making innovative design easier through total system solutions that address critical challenges at the intersection of emerging technologies and durable end markets. Its easy-to-use development tools and comprehensive product portfolio support customers throughout the design process, from concept to completion. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support and delivers solutions across the industrial, automotive, consumer, aerospace and defense, communications and computing markets. For more information, visit the Microchip website at www.microchip.com.
###
Note: The Microchip name and logo and the Microchip logo are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. Clockstudio is a trademark of Microchip Technology Inc. in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.
Kim Dutton
kim.dutton@microchip.com