| Title |
Title
AN2000- USB to UART Bridging with Microchip USB 3.1 Gen 1 Hubs
|
|---|---|
| Name |
Name
AN2000
|
| Date |
Date
09/22/2015
|
| Description |
Description
The USB to UART bridging feature of Microchip?s USB 3.1 Gen 1 hubs provides system designers expanded system control and potential BOM reductions. When using this feature, a separate USB to UART device is no longer required and a downstream USB port is not lost, as occurs when a standalone USB to UART device is implemented. This feature is available on the Microchip USB5734 USB3.1 Gen 1 Hub, which contains the internal Hub Feature Controller. Commands may be sent from the USB Host to the internal Hub Feature Controller device in the Microchip hub to perform the following functions: ? Enable/Disable UART Interface ? Set UART Interface Baud Rate ? UART Write ? UART Read
|
Live Chat