We detect you are using an unsupported browser. For the best experience, please visit the site using Chrome, Firefox, Safari, or Edge. X
Maximize Your Experience: Reap the Personalized Advantages by Completing Your Profile to Its Fullest. Update Here
Stay in the loop with the latest from Microchip. Update your profile while you are at it. Update Here
Complete your profile to access more resources. Update Here

Run Firmware TPM 2.0 on Microchip PolarFire® SoC With wolfTPM

Embedded Linux developers who need TPM 2.0 services without a discrete security chip or third-party trusted execution environment can now evaluate wolfTPM’s firmware TPM example on Microchip PolarFire® SoC, running on a dedicated RISC-V® core isolated from Linux.

We just opened a pull request (PR) adding a wolfTPM Firmware TPM (fTPM) example for the PolarFire SoC, validated end-to-end on the MPFS250T Video Kit. It runs a full TPM 2.0 service on a dedicated RISC-V hart, isolated from Linux, with no discrete TPM chip and no third-party TEE.

Learn how wolfTPM’s firmware TPM example runs on a dedicated RISC-V core on PolarFire SoC, how Linux communicates with it through shared memory and how the supplied scripts verify the connection. The article also covers the default hardware entropy source and planned work on persistent storage, post-quantum cryptography and a Mi-V soft-core implementation.

Why This Matters

Most TPM integrations need either a discrete SPI/I2C chip or a firmware TPM buried in someone else’s TEE. This is a different option: a TPM 2.0 service you own end-to-end, on a hard RISC-V core, isolated by AMP partitioning, small enough to live in M-mode. The result is ~200 KB of code giving Linux TPM-grade key storage, sealing and attestation with no security chip and no vendor blob owning the boundary.

Why wolfTPM’s fTPM

It is the same ftpm library across every target. The TPM 2.0 command dispatch, TIS protocol, NV journal and the FWTPM_NV_HAL / FWTPM_CLOCK_HAL / FWTPM_TIS_HAL interfaces remain consistent across supported platforms, demonstrating the portability of the wolfTPM firmware TPM library.

wolfTPM supports a range of embedded architectures, including RISC-V hart in AMP (this port). It also supports SPDM-protected sessions (v1.84) and post-quantum ML-DSA / ML-KEM (v1.85), bringing these capabilities together in a single vendor with auditable source.

PolarFire SoC has four U54 application cores plus an E51 monitor core. Microchip’s HSS launches an AMP payload:

  • E51: HSS monitor.
  • U54 harts 1-3: Linux (S-mode under OpenSBI), Yocto rootfs.
  • U54 hart 4: the fwTPM server – M-mode, bare-metal, loaded at 0x91C00000.

Linux reaches hart 4 through a shared-memory mailbox, console ring and TIS register block in L2 LIM at 0x08000000:

0x08000000  mailbox      (64 B   - cmd/rsp + boot/trap debug)
0x08000040  console ring (4 KB   - server stdout via /dev/mem)
0x08001040  TIS regs     (~8 KB  - regs + cmd/rsp FIFOs)

Because LIM is not in Linux’s System RAM map, the mailbox is readable from /dev/mem even under a stock CONFIG_STRICT_DEVMEM=y kernel—no kernel rebuild. The one device-tree change is a small overlay releasing hart 4.

The transport is build-selectable (FWTPM_XPORT): the default cacheable L2-LIM mailbox is coherent under HSS AMP and just works, and a fully-uncached DDR-alias path ships as a verified alternative for designs that want the mailbox outside cache entirely.

Smoke Test

Two root scripts ship with the example. fwtpm_mbox_dump.py decodes the mailbox, boot-progress marker, M-mode trap fields (mcause/mepc/mtval) and the captured console ring—so you can see exactly where the server is even with no routed UART. fwtpm_smoke.py confirms the server is alive (Phase 1), then drives a TIS transaction through the mailbox (Phase 2) with a rolling nonce the server echoes back, proving hart 4 saw the new write, not a stale cache line.

It Works End-to-End

The full Linux <-> hart 4 round-trip works on real hardware: both phases pass reproducibly on the default build, no special configuration.

Entropy is secure by default: a plain make seeds the DRBG from the System Controller hardware TRNG (FWTPM_RNG=SCB_NONCE) as the sole entropy source, validated on the Video Kit. A development-only MTIME-jitter seed exists for early bring-up but is gated behind an explicit opt-in, so it can never ship silently and a default build is never weakly seeded.

Where This Is Going

Today the fTPM runs on a hard U54 application core. The headline next step makes it a true fabric root of trust: instantiate a Microchip Mi-V RISC-V soft core in the MPFS250T’s FPGA fabric and host the fTPM there. The hard U54 cluster keeps running Linux untouched; the Mi-V core becomes a dedicated security processor in programmable logic, with its own bus mastering and no application code sharing its silicon.

Because the ftpm library is portable, that move is mostly a new transport HAL and startup file—the TPM 2.0 core is unchanged. The payoff is the tie-in to the PolarFire device’s hardware security blocks: seed entropy from the System Controller TRNG (already wired), bind a device-unique root key to the SRAM-PUF, offload crypto to the User Crypto (Athena TeraFire) processor and persist NV state in sNVM secure storage. That turns the soft-core fTPM into a self-contained, tamper-resistant root of trust living in fabric—not borrowed from the application complex.

Also on the roadmap:

  • Persistent NV behind FWTPM_NV_HAL (sNVM integrity key + QSPI bulk) so keys survive a power cycle
  • PQC: enable ML-KEM / ML-DSA and benchmark on the target
  • An interrupt-driven doorbell so the TPM core sleeps between requests
  • A wolfBoot-hosted variant (wolfBoot replaces HSS and owns the SBI on E51), opening an SBI doorbell and measured boot

Want More?

If you have a design that wants TPM 2.0 key storage, sealing or attestation but no room for a discrete chip or closed TEE, this is the shape of the answer—and it runs end-to-end on a shipping RISC-V SoC today, with a soft-core fabric root of trust next. The full example is on GitHub; reach out if you want a hand bringing it up on your part.

Reference

If you have questions about any of the above, please contact us at facts@wolfssl.com or call us at +1 425 245 8247.

David Garske, wolfSSL, Nov 19, 2026
Tags/Keywords: Security

Live Chat

Need Help?

Privacy Policy