We detect you are using an unsupported browser. For the best experience, please visit the site using Chrome, Firefox, Safari, or Edge. X
Maximize Your Experience: Reap the Personalized Advantages by Completing Your Profile to Its Fullest. Update Here
Stay in the loop with the latest from Microchip. Update your profile while you are at it. Update Here
Complete your profile to access more resources. Update Here

Thermal (IR) Imaging Pipeline (ISP) Core on PolarFire® SoC FPGA SoM

Digital Core Technologies (DCT) has developed a thermal Imaging Pipeline on PolarFire® SoC FPGA. The thermal Image Signal Processor (ISP) is an extremely low power yet powerful alternative for the thermal imaging available in other architectures. This can be tuned for various applications like security/surveillance, medical imaging, industrial monitoring, gas detections and others.


Powerful Alternative for the Thermal Imaging

Digital Core Technologies (DCT) has developed a thermal imaging pipeline on PolarFire® SoC FPGA. The thermal Image Signal Processor (ISP) is an extremely low power yet powerful alternative for the thermal imaging available in other architectures. This can be tuned for various applications like security/surveillance, medical imaging, industrial monitoring, gas detections and others. The pipeline is built to run on DCT’s SoM, CMSV_A1_PF254_AX. This SoM carries the PolarFire® SoC FPGA, MPFS250T, a 64-bit multicore RISC-V® CPU subsystem processor with FPGA fabric, DRAM, EMMC Flash and Wi-Fi® systems on board and runs on the Linux® Operating System (OS).

Digital Core Technologies Thermal Image

Thermography Cameras IR Sensor

Thermography cameras usually detect radiation in the Longwave-Infrared (LW-IR) range of the electromagnetic spectrum (roughly 9–14 µm) and produce visual images of the thermal radiation. Since IR radiation is emitted by all objects with a temperature above absolute zero, these cameras make it possible to see one’s environment with or without visible illumination. Thermal imaging cameras makes warm objects stand out well against cooler backgrounds; all warm-blooded animals become easily visible against the environment, day or night.

Thermal Camera IR Sensor.

Thermography Electronic Core

Thermal cameras are widely used in defense and civilian applications. In the defense sector, they are mainly used for night vision applications such as gun-site and as surveillance cameras. Civilian applications include industrial inspection applications, driving assistance and medical diagnostics. Firefighters use thermography to see through smoke. Maintenance technicians use thermography to locate overheating joints and sections of power lines and machines. Building construction technicians can see thermal signatures that indicate heat leaks in faulty thermal insulation and can use the results to improve the efficiency of heating and air conditioning.

The most important part of a thermography camera is an IR sensor. Focal plane array sensors with “uncooled microbolometers” are the most popular technology used now for the thermal imaging. The sensor with its front-end electronics circuit is called camera core, which literally forms the core of a thermal camera.  

In a thermography camera the important parts are a thermal (IR) sensor and electronic core with imaging ISP. The core captures and conditions the pixel data from the sensor and converts it into a digital stream representing an image frame. An image processing pipeline transform the stream of frames suitable for human vision.

Extremely Low-Power Image Signal Processor

Image processing is normally a very computation-intensive task because digital images include large amount of information. Most of the architectures currently available use high power for doing these computationally intensive digital image processing. The RISC-V-based PolarFire® SoC FPGA utilizes extreme low power for the image processing. In many applications, thermal cameras need to run on battery-powered products so it is important to perform image processing operations as efficiently as possible to reduce the power consumption. That makes the PolarFire® SoC FPGA-based ISP a powerful alternative for the other architecture-based ISPs available for thermal imaging systems.

In this case, we used a 640 × 480 VGA image sensor from Lynred as an IR sensor, which includes a proxy circuit that converts the analog signal to a digital bus. From there, we take it through a PolarFire SoC SoM developed by DCT. The imaging pipeline (ISP) is implemented on the PolarFire SoC FPGA. The processor manages the pipeline.

Lynred IR Image Sensor PolarFire FPGA SoC

From the raw frames received from the sensor, we will not be able to distinguish anything. The thermal ISP pipeline takes this frame through a series of processes to generate a visual frame from which we can distinguish the thermal profile of the objects in the frame. The first level processes we do in the raw image are tone mapping, bad pixel correction, non-uniformity correction and image enhancement, such as digital filters. After that, ISP normally apply image overlay and color palette to differentiate different temperature areas and regions. The output of the ISP is a human understandable thermal image similar to that shown in the below image.

Thermal ISP Image Pipeline PolarFire SoC FPGA Fabric

Advantages of Developing Thermal ISP core in the PolarFire FPGA SoC

  • Low power consumption of the SoC
  • Low power means less heat is generated in the product, which is crucial for the performance and stability of thermal cameras
  • Flexibility in tuning and customizing the ISP as it is implemented in FPGA
  • Ample CPU resources for embedded camera application
  • Compact design and low cost

Please visit the Digital Core Technologies or core modules page for more info regarding thermal ISP development or email them at info@dicortech.com for detailed information about the PolarFire-/RISC-V-based developments like the thermal ISP.

S Thomas, May 31, 2022
Tags/Keywords: Industrial and IoT, Development Tools

Live Chat

Need Help?

Privacy Policy