We detect you are using an unsupported browser. For the best experience, please visit the site using Chrome, Firefox, Safari, or Edge. X
Maximize Your Experience: Reap the Personalized Advantages by Completing Your Profile to Its Fullest. Update Here
Stay in the loop with the latest from Microchip. Update your profile while you are at it. Update Here
Complete your profile to access more resources. Update Here

Effective Prototyping De-Risks Product Innovation

Adopting the proper design thinking approach, along with a culture that embraces prototyping and rapid iteration, can improve time to market while reducing the capital and human costs of product development.

Product and user experience (UX) design are fraught with tremendous amounts of risk because of the time, energy and money that these types of projects demand. Organizations are looking for ways to innovate faster, while mitigating the inherent risk of new products and design. The balance between speed of innovation and risk isn’t new. What is new is the number (and size) of organizations embracing design thinking and prototyping as THE solution to de-risk product design. 

 

Adopting the proper design thinking approach, along with a culture that embraces prototyping and rapid iteration, can improve time to market while reducing the capital and human costs of product development. 

 

The Innovation Trap 

 

Product teams are pressured to produce tools, software and products at a rapid pace, and are measured by how quickly they bring product iterations to market, or how well a new product is executed. The trap is focusing energy and attention on the execution, without creating the infrastructure to test for a market fit, or to ensure that a new product is accomplishing the business outcomes it’s meant to.  

 

Oftentimes, an organization may target and measure for usability, or ease of use, or thoroughness of the style and the experience of a new idea, without validating that the new idea is the correct one. A concept may test well for usability, brand experience and functionality, but it might not serve a need that the market desires. Simply put, a company can execute an idea well, but can fail to validate the need for the new product or innovation.  

 

How Do You Avoid the Trap? 

 

1. Business outcomes should drive your prototyping hypotheses, just as much as usability and experience. 

The best UX designers are trained to identify usability and experience gaps within their prototypes. But they aren’t always adept at recognizing the market forces and business outcomes that a new product is solving for. A great product solves problems for its users but should also provide a tangible return for the business. When defining your prototyping process, be sure to include the ultimate business outcome as part of your testing design.  

 

2. Don’t forget the other tools in your design thinking toolbox.  

Great product leaders and great innovation designers have hundreds of different methodologies in their toolbox to draw from. The real art or skill is knowing when to use what tool. Some will take longer but reduce more risk. Other approaches may be quicker and given certain business contexts, may reduce a similar amount of risk. Prototyping is becoming easier and more popular but knowing when to use which forms of prototyping is more important than simply knowing how to create any single prototype. 

 

Consider the case of a popular consumer goods company. When developing a new household cleaning product, it skipped many of the design thinking phases and jumped straight into the development of new soaps that would improve their customer’s floor cleaning experience. The company assumed that users wanted new soaps, without stepping through a proper design thinking approach. After a series of failures, it brought in a design thinking firm, who leveraged direct interaction with customers to recognize that consumers didn’t want new soap, but actually wanted a new mop. It began testing different versions of disposable mops, eventually settling on the design of one of today’s most popular household cleaning products. A design thinking approach, backed with user research and eventually prototyping, created a new billion-dollar market where one didn’t exist before. 

 

3. Recognize that your organization’s UX maturity and culture may need to change.  

Every organization possesses a certain level of UX maturity and testing infrastructure, and this will affect the risk involved with product innovation. Knowing where your organization fits could provide clues as to the steps needed to adopt a prototyping culture. The most mature companies are building a prototyping and testing infrastructure, including employee facing interfaces and testing and reporting tools —all in the interest of de-risking the process of innovation. 

 

Consider the social media giant whose famous motto “Go Fast and Break Things” is rooted in the prototype-and-test methodology. The company’s co-founder and CEO recently explained that its speed in the early days injected risk into its systems because it didn’t have the proper structure in place to execute. He recognized early on that the company’s innovation would be a function of its ability to test new UX design and features in a stable environment. He said, “We thought, ‘OK, we need a new strategy to enable us to move fast.’ And what we came up with was: we’re going to do this by building the best infrastructure.” Today, “going fast” at this company is the result of a calculated approach to build a stable testing infrastructure, helping engineers speed up their prototyping. As the platform grew, “breaking things” became much riskier and more costly for the company. The company slowed its new feature builds for two years so it could get the proper structure in place. It’s a more mature organization, with less risk involved in its testing processes. Today, at any given time, there are more than 10,000 different live versions of its site being prototyped and tested by their engineers. Each version is testing user experience, levels of engagement, etc., and the company is able to ship the best performing UX instantly. 

 

When in Doubt, Rely On An Expert

 

Most innovation leaders can recognize their need for additional UX prototyping assistance, but don’t have the time to change the entire culture of the organization. Hiring an outside expert can be a cost-effective endeavor, especially if it helps jump-start your design thinking DNA. Because the real risk in product development and improvement is simply never getting started.  

 

Whether you need help with hardware, software or UX prototype design, Microchip offers an entire ecosystem of support, including partners like Drawbackwards. Want to validate a UX prototype concept, get buy-in, or take the first step toward making your idea come to life? Drawbackwards will help you navigate the UX process and uncover the insights you need to move forward. Learn more at www.drawbackwards.com


Tags/Keywords: Development Tools

Live Chat

Need Help?

Privacy Policy