We detect you are using an unsupported browser. For the best experience, please visit the site using Chrome, Firefox, Safari, or Edge. X

The MPLAB Harmony Configurator (MHC) is a time-saving hardware configuration utility for MPLAB Harmony, Microchip's award winning software framework. Developers use MHC to get visual understanding and control of the configuration of their target device and application. MHC is a fully integrated tool within MPLAB X IDE.

  • Generates all hardware configuration code
  • Generates all middleware framework related code
  • Automatically updates the active MPLAB X IDE project with all required files.

MHC is available as a plug-in within MPLAB X IDE. Click here for details on how to install.

MPLAB Harmony Features


Feature Description
The Framework MPLAB Harmony is a framework of system services, device drivers, and other libraries that are built upon a base of portable peripheral libraries to provide flexible, portable, and consistent software "building blocks" that you can use to develop your embedded PIC32 applications.
TCP/IP Stack and Wi-Fi support

The MPLAB Harmony TCP/IP Stack provides a foundation for embedded network applications by handling most of the interaction required between the physical network port and your application. It includes modules for several commonly used application layers, including HTTP for serving web pages, SMTP for sending e-mails, SNMP for providing status and control, Telnet, TFTP, Serial-to-Ethernet, and much more. In addition, the stack includes lightweight and high-performance implementations of the TCP and UDP transport layers, as well as other supporting modules such as IP, ICMP, DHCP, ARP, and DNS.

  • Multiple interfaces - Ethernet and/or Wi-Fi interfaces are supported
  • Dual stack with IPv4 and/or IPv6 support
  • Fully dynamic
  • Improved modularity and stack layout
  • Run-time configuration through the TCP/IP console
  • Interrupt driven operation
  • RTOS friendly, with easy RTOS integration
  • The BSD layer compatibility has been greatly improved, new dynamic socket options have been added as well as IPv6 support.
  • Run time benchmarking support using standard industry tools - Iperf
  • The MPLAB Harmony file system (SYS FS) is used by the HTTP, FTP, SNMP, modules, among others. This makes the stack independent of the specific file structure of a particular media and allows web page storage on a multitude of storage media.
  • The stack uses the high-performance MPLAB Harmony Cryptographic Library, which is a very efficient and modern implementation supporting the latest encryption and key exchanges algorithms
  • The stack security has been greatly improved by adding support of the modern wolfSSL TLS libraries
  • TCP/IP Stack and Wi-Fi support
  • IGMPv3 support
Wi-Fi

The Wi-Fi software library, in conjunction with the MRF24WG0MA and MRF24WN0MA module, allows an application to:

  • Join an existing 802.11 Wi-Fi network
  • Create a 802.11 Wi-Fi network
USB Device Stack

The MPLAB Harmony USB Device Library (referred to as the USB Device Library) provides embedded application developers with a framework to design and develop a wide variety of USB Devices. A choice of Full Speed only or Full Speed and Hi-Speed USB operations are available, depending on the selected PIC32 microcontroller. The USB Device Library facilitates development of standard USB devices through function drivers that implement standard USB Device class specification. Custom USB devices can also be implemented via a USB Generic Device Driver. The USB Device Library is modular, thus allowing application developers to readily design composite USB devices. The USB Device Library is a part of the MPLAB Harmony installation and is accompanied by demonstration applications that highlight library usage. These demonstrations can also be modified or updated to build custom applications. The USB Device Library also features the following:

  • Support for different USB device classes (CDC, Audio, HID, MSD, and Generic)
  • Supports multiple instances of the same class in a composite device
  • Supports multiple configurations at different speeds
  • Supports full speed and high speed operation
  • Supports multiple USB peripherals (allows multiple device stacks)
  • Modular and Layered architecture
  • Supports deferred control transfer responses
  • Completely non-blocking
  • Supports both polled and interrupt operation
  • Works readily in an RTOS environment
USB Host Stack

The USB Host Layer in the MPLAB Harmony USB Host Stack performs the tasks of enumerating an attached device and interfacing the HCD. The following are the key features of the MPLAB Harmony USB Host Layer:

Host Layer:

  • Supports multi-configuration and composite USB Devices
  • Supports VID PID and class, subclass, and protocol devices
  • Can manage multiple USB devices through the Root Hub
  • Concise API simplifies application development
  • Modular architecture allows support for multiple (and different) USB controller in one application. Can operate multiple USB segments
  • Supports Low-Speed, Full-Speed, and High-Speed USB devices
Fixed-Point DSPk Math Libraries

The DSP Fixed-Point Library contains building block functions for developing digital signal processing algorithms. The library supports the Q15 and Q31 fractional data formats. The functions are implemented in efficient assembly specifically targeted at the DSP extensions in this core family. The library makes these functions available in a simple C-callable structure.

  • complex math
  • vector math
  • matrix math
  • digital filters
  • transforms
Graphics Library
  • Completely overhauled library improves drawing performance to enable faster updates and reduced need for screen painting
  • Updates to MPLAB Harmony Graphics Suite (MHGS) includes the ability to undock all windows within the tool, the ability to zoom and copy/paste in composer window, and the addition of new resource utilities.
  • New MPLAB Harmony Event Manager to provide simplified coordination of graphics activity to external events
  • Support for GPU-enabled MCUs (PIC32MZ DA family)
  • New Image and Font Asset Manager gives fine-grained understanding of memory footprint and enables resizing to meet specific application needs and target MCU memory sizes.
  • New MPLAB Harmony Display Manager to quickly enable the use of displays with non-standard formats.
Cryptographic Library

This library provides a software Cryptographic Library that is available on the Microchip family of microcontrollers with a convenient C language interface. The Cryptographic Library includes functions to perform encryption, decryption, hashing, authentication, and compression within the embedded application. Random number generation (RNG) functions are also provided.

Block Ciphers - The library provides DES, 3DES, and AES for block cipher needs. Depending on the algorithm in use, CBC and CTR modes are supported.

Public Key Cryptography - The library provides RSA and Elliptic Curve Cryptography (ECC) for Public Key Cryptography, and Diffie-Hellman (DH) for key agreement arrangements.

Hash Functions - The library provides MD5, SHA, SHA-256, SHA-384, and SHA-512 for hashing. These functions do not require keys or initialization vectors (IV).

Random Number Generation Functions - The library provides functions to generate either a single pseudo-random number, or a block of such numbers.

File System

The File System service is a framework designed to support multiple file systems (native file system) and multiple media in the same application. Supported file systems are FAT12, FAT32, MPFS, and JFS. Each of these native file systems have a common set of APIs that can be used to access the files of that particular native file system.

  • Support for multiple file system (FAT, MPFS)
  • Supports multiple physical media (NVM, SD card)
  • More physical media can be interfaced with the FS once the driver is available for the media
  • Modular and Layered architecture
Peripheral Library
  • Compliance with all MISRA-C: 2012 Mandatory Standards
  • Re-implemented to more directly access physical registers
  • More efficient and easier to read and understand
  • No changes to interface APIs
  • Support for all PIC32 Devices and peripherals, including:
    • PIC32MX320_340_360_420_440_460
    • PIC32MX575/675/695/775
    • PIC32MX534/564/664/764
    • PIC32MX1XX/2XX
    • PIC32MX1XX/2XX (256 KB/64 KB)
    • PIC32MX330_350_370_430_450_470
    • PIC32MX320_340_360_420_440_460
    • PIC32MX1XX/2XX/5XX
    • PIC32MX1XX/2XX (256 KB/16 KB)
    • PIC32MZEC
    • PIC32MZEF
    • PIC32MK
    • PIC32MZ DA
Device Drivers Static and/or Dynamic drivers for the following peripherals: ADC, CMP, I2C, I2S, IC, NVM, OC, PMP, RTCC, SD, SPI, External Flash (SST25VF016B, SST25VF020B), Timer, UART.
System Services

MPLAB Harmony system services are responsible for managing shared resources so that other modules, such as drivers, middleware, and applications, do not conflict on shared resources.

Clock - This library provides an interface to manage the Oscillator module on the Microchip family of microcontrollers during different modes of operation.

Console - This service routes data or message traffic between a console device and a middleware layer or application. The most common use of the Console Service is to route debug or error messages from a PIC32-based device to a terminal program on a host development system.

Debug - This service provides a set of functions that allow the developer to output debug and/or error messages based on a global error level. The messages are sent to the System Console Service, where they are routed to a console device.

Device Control - This service provides the developer with simple APIs to configure and control device-specific functions.

DMA - This library provides an interface to interact with the DMA subsystem to control and manage the data transfer between different peripherals and/or memory without intervention from the CPU.

Interrupt - This service provides support for initializing the processor's interrupt controller, registering Interrupt Service Routines (ISRs) and managing interrupts. These features enable making efficient and dynamic applications, drivers, and middleware that respond to external events as they occur in real time.

Messaging - This library provides intra-process and inter-process communication by the sending and receiving of simple messages.

Ports - This library provides an interface to manage and control general purpose input or output ports controlled by the Ports modules

Random Number Generator - This System Service provides a simple C-language interface for generating random numbers at both pseudo-random and cryptographic strengths.

Reset – This service can be used to identify the reason for the most recent processor reset, manage the system's reset reason status flags, and even cause a reset under software control if the processor in use supports that functionality.

Timer - This library provides interfaces to manage alarms and/or delays.

WDT - This library provides a low-level abstraction of the Watchdog Timer peripheral.

Operating System Abstraction Layer (OSAL)

The OSAL provides the interface to commonly available Real-Time Operating Systems (RTOS) such that drivers and middleware (and optionally, applications) may be written using a single interface to a minimal set of OS-specific features needed to provide thread safety. The OSAL interface can be implemented appropriately to support almost any desired RTOS. For applications where no RTOS is available, or desired, a bare version of the OSAL supports either polled or interrupt-driven environments running directly on the hardware. This allows applications designed with the MPLAB Harmony stack to be executed in all three common embedded environments: polled (shared multi-tasking), interrupt-driven, or RTOS-based.

Support for the following RTOS:

  • FreeRTOS
  • OpenRTOS
  • µC/OS-III, µC/OS-II
  • ThreadX
  • embOS
MPLAB Harmony Configurator (MHC) Tool

MPLAB Harmony provides a MPLAB Harmony Configurator (MHC) MPLAB-X IDE plug-in that can be installed in MPLAB X IDE to help you create your own MPLAB Harmony applications. It supports configuration and code generation for all MPLAB Harmony components and 3rd-party software (coming soon). Additional features:

  • Graphical clock configuration
  • Graphical Pin management
  • MPLAB Harmony® Graphics Composer and GRC integration

The Display Manager plug-in for MHC was added which includes the following features:

  • Automatically configures display drivers
  • 8-bit pallet support
  • WVGA double-buffer support
3rd-Party Software

wolfSSL - A lightweight C-language-based SSL/TLS library targeted for embedded, RTOS, or resource-constrained environments primarily because of its small size, speed, and portability. wolfSSL supports industry standards up to the current TLS 1.2 and DTLS 1.2 levels, is up to 20 times smaller than OpenSSL, offers a simple API, an OpenSSL compatibility layer, OCSP and CRL, and offers several progressive ciphers. wolfSSL is under active development, and should be chosen over yaSSL when possible.

  • Segger emWin Pro Library: emWin from SEGGER Microcontroller GmbH & Co. KG, is a software graphics library that provides an efficient, processor and LCD controller-independent Graphical User Interface (GUI) for applications that operate with a graphical LCD. emWin provides a graphical user interface for a graphics application, that is independent of the LCD controller and CPU.

MPLAB Harmony v2.0x Downloads


Windows (x86/x64)


Title Download
MPLAB Harmony Integrated Software Framework v2.06 Windows Download
MPLAB Harmony Release Notes and Contents (v2.06) Download
MPLAB Harmony Release Brief v2.06 Download

Linux 32-Bit and Linux 64-Bit


Title Download
MPLAB Harmony Integrated Software Framework v2.06 Linux Download
MPLAB Harmony Release Notes and Contents (v2.06) Download
MPLAB Harmony Release Brief v2.06 Download

Mac (10.X)


Title Download
MPLAB Harmony Integrated Software Framework v2.06 OSX Download
MPLAB Harmony Release Notes and Contents (v2.06) Download
MPLAB Harmony Release Brief v2.06 Download

Before using MPLAB Harmony, ensure that the following development tools and plug-ins are installed:

Development Tools:

MPLAB X IDE plug-ins:

  • MPLAB Harmony Configurator (MHC) v2.0.6.0

MPLAB Harmony v2.0x Downloads


v2.05

Windows (x86/x64)


Title Download
MPLAB Harmony Integrated Software Framework v2.05.01 Windows Download
MPLAB Harmony Release Notes and Contents (v2.05.01) Download
MPLAB Harmony Release Brief v2.05.01 Download

Linux 32-Bit and Linux 64-Bit


Title Download
MPLAB Harmony Integrated Software Framework v2.05.01 Linux Download
MPLAB Harmony Release Notes and Contents (v2.05.01) Download
MPLAB Harmony Release Brief v2.05.01 Download

Mac (10.X)


Title Download
MPLAB Harmony Integrated Software Framework v2.05.01 OSX Download
MPLAB Harmony Release Notes and Contents (v2.05.01) Download
MPLAB Harmony Release Brief v2.05.01 Download

v2.04

Windows (x86/x64)


Title Download
MPLAB Harmony Integrated Software Framework v2.04 Windows Download
MPLAB Harmony Release Notes and Contents (v2.04) Download
MPLAB Harmony Release Brief v2.04 Download

Linux 32-Bit and Linux 64-Bit


Title Download
MPLAB Harmony Integrated Software Framework v2.04 Linux Download
MPLAB Harmony Release Notes and Contents (v2.04) Download
MPLAB Harmony Release Brief v2.04 Download

Mac (10.X)


Title Download
MPLAB Harmony Integrated Software Framework v2.04 OSX Download
MPLAB Harmony Release Notes and Contents (v2.04) Download
MPLAB Harmony Release Brief v2.04 Download

v2.03b

Windows (x86/x64)


Title Download
MPLAB Harmony Integrated Software Framework v2.03b Windows Download
MPLAB Harmony Help Files/Release Notes (v2.03b) Download
MPLAB Harmony Release Brief v2.03b Download

Linux 32-Bit and Linux 64-Bit


Title Download
MPLAB Harmony Integrated Software Framework v2.03b Linux Download
MPLAB Harmony Help Files/Release Notes (v2.03b) Download
MPLAB Harmony Release Brief v2.03b Download

Mac (10.X)


Title Download
MPLAB Harmony Integrated Software Framework v2.03b OSX Download
MPLAB Harmony Help Files/Release Notes (v2.03b) Download
MPLAB Harmony Release Brief v2.03b Download

v2.02b

Windows (x86/x64)


Title Download
MPLAB Harmony Integrated Software Framework v2.02b Windows Download
MPLAB Harmony Help File/Release Notes (v2.02b) Download
MPLAB Harmony Release Brief v2.02b Download

Linux 32-Bit and Linux 64-Bit


Title Download
MPLAB Harmony Integrated Software Framework v2.02b Linux Download
MPLAB Harmony Help File/Release Notes (v2.02b) Download
MPLAB Harmony Release Brief v2.02b Download

Mac (10.X)


Title Download
MPLAB Harmony Integrated Software Framework v2.02b OSX Download
MPLAB Harmony Help File/Release Notes (v2.02b) Download
MPLAB Harmony Release Brief v2.02b Download

v2.01b

Windows (x86/x64)


Title Download
MPLAB Harmony Integrated Software Framework v2.01b Windows Download
MPLAB Harmony Release Brief v2.01b Download

Linux 32-Bit and Linux 64-Bit


Title Download
MPLAB Harmony Integrated Software Framework v2.01b Linux Download
MPLAB Harmony Release Brief v2.01b Download

Mac (10.X)


Title Download
MPLAB Harmony Integrated Software Framework v2.01b OSX Download
MPLAB Harmony Release Brief v2.01b Download

v2.00b

Windows (x86/x64)


Title Download
MPLAB Harmony Integrated Software Framework v2.00 Windows Download
MPLAB Harmony Help Files/Release Notes (v2.00b) Download
MPLAB Harmony Release Brief v2.00b Download

Linux 32-Bit and Linux 64-Bit


Title Download
MPLAB Harmony Integrated Software Framework v2.00b Linux Download
MPLAB Harmony Help Files/Release Notes (v2.00b) Download
MPLAB Harmony Release Brief v2.00b Download

Mac (10.X)


Title Download
MPLAB Harmony Integrated Software Framework v2.00b OSX Download
MPLAB Harmony Help Files/Release Notes (v2.00b) Download
MPLAB Harmony Release Brief v2.00b Download

Before using MPLAB Harmony, ensure that the following development tools and plug-ins are installed:

Development Tools:

MPLAB X IDE plug-ins:

  • MPLAB Harmony Configurator v2.xx

Tutorials


User Guides


 

Title
Volume V MPLAB Harmony Framework Reference Part II
Volume VII Utilities
Volume VI Third Party Products
Volume V MPLAB Harmony Framework Reference Part I
Volume IV MPLAB Harmony Development
Volume II Supported Hardware
Volume III MPLAB Harmony Configurator (MHC)
Volume I Getting Started With MPLAB Harmony
Using MPLAB Harmony Help
USB Libraries
Understanding MPLAB Harmony
Third-Party Products
Test Harness Library
TCP/IP Stack Libraries
System Service Libraries
Sample Library
Segger emWin User guide
Prebuilt Libraries
PIC32 Bluetooth Stack Library
Peripheral Libraries
OSAL Library
Networking Presentation Layer Library
MPLAB Harmony Tutorial - Creating an Application
MPLAB Harmony Test Harness Users Guide
MPLAB Harmony Release Notes and Contents (v2.05)
MPLAB Harmony Release Notes (v2.04) Archive
MPLAB Harmony Release Brief v2.05
MPLAB Harmony Release Brief v2.04
MPLAB Harmony Release Brief v2.03b
MPLAB Harmony Release Brief v2.02b
MPLAB Harmony Release Brief v2.01b
MPLAB Harmony Release Brief v2.00
MPLAB Harmony Overview
MPLAB Harmony Help File and Release Notes (v2.03b)
MPLAB Harmony Graphics Composer (MHGC)
MPLAB Harmony Configurator User's Guide
MPLAB Harmony Configurator Developer's Guide
MPLAB Harmony Configurator (MHC) and MPLAB Harmony Graphics Composer
MPLAB Harmony Configurator (MHC)
MPLAB Harmony Compatibility Worksheet
MPLAB Harmony Compatibility Guide
MPFS2 Utility
Microchip MIB Compiler
Microchip Compact MP3 Decoder Library User's Guide
Math Libraries
Graphics Libraries
embTelnet User's Guide for PIC32
embTCP User's Guide for PIC32
embHTTP User's Guide for PIC32
embFTP User's Guide for PIC32
embDUAL User's Guide for PIC32
Driver Libraries
Demo Applications
Decoder Libraries
Crypto Library
Bootloader Library
Board Support Packages (BSPs)

 

Interested in getting to know more about Harmony?


For Developers


If you have a great idea for embedded software that will enhance the MPLAB® Harmony engineer's experience or fill a technological need, then Microchip has everything you need to get started. This is your opportunity to open new avenues of business for you and your company by becoming an MPLAB Harmony third-party software provider, just like just like other leading software and operating system providers. This page contains the tools you need to build a set of solutions that other MPLAB Harmony developers worldwide can use to make the next generation of embedded products.

Getting Started


Are you ready to start developing with MPLAB Harmony? These guides will help you design your own software offering for MPLAB® Harmony:

Other Things to Check Out


  • For more information on MPLAB X IDE, including where to download the tools, check out the MPLAB Design Center.
  • Find out more about PIC32, Microchip's industry-leading 32-bit architecture, by going to here.
  • Microchip partners with select software providers as part of our MPLAB® Harmony Premium Third-Party Solutions program. Go here to find out more.

Tell Us About Your Project


Do you have an MPLAB® Harmony project that you want other developers to hear about? Are you interested in becoming a featured MPLAB® Harmony Software Provider? We want to hear from you! Tell us more about you and what you're working on. We can't wait to hear about the great software that you are developing for PIC32 devices. We may even feature you in one of the many ways that we connect with our developer audience.

Contact Information

Please fill out your contact information below.
Name*
 
 

Porting from v1.XX


All MPLAB Harmony applications have already been ported to the MPLAB Harmony v2.0x framework and BSP. These should work without any other user changes. Considerations below may be needed for user code created in previous versions, depending on custom driver or other middleware usage.

BSPs have changed, and with them specifics about the pin and GPIO management, which may:

  • Impact custom drivers, and need refinement of the driver to correspond with pin names
  • Impact custom pin manager settings
  • Impact some applications, particularly that directly call GPIO (button, LED, external interrupt and enables)

Drivers have been changed

  • The APIs have not changed, so there should not be a direct reflection on applications that use them
  • Drivers provided in MPLAB Harmony will be updated by MHC configuration, and you will need to use the latest MHC version and reconfigure your project

PLIBs have changed

  • APIs for the PLIBs have not changed; however, implementation checking is more rigid
  • May cause some driver rewrite if they did not follow strict API convention

Compiler version has changed

  • MPLAB Harmony v1.08 and previous versions use MPLAB X IDE v1.40 (and parts support)
  • MPLAB Harmony v2.00 and later uses MPLAB X IDE v1.42 and later
  • More strict checking of some structures in later compilers make cross compilation problematic (e.g., Zero to pointer instead of null)

Graphics tools have changed (future release)

  • A one-way export from MPLAB Harmony v1.0x is possible
  • An import of the previous export will be possible in the new version
  • Some new elements like multi-layer and resource management will require additional data
  • You can continue to develop basic graphics in MPLAB Harmony v1.xx and port that to MPLAB Harmony v2.0 at any time; however, the reverse is not possible

In Graphics 2.0, all resources are by default stored in SRAM. If you what to use flash memory instead due to size constraints, please download and add the below file to your framework (framework\gfx\gac\gac_source.c.ftl) and provide flash memory access to MHGC.