We detect you are using an unsupported browser. For the best experience, please visit the site using Chrome, Firefox, Safari, or Edge. X
Maximize Your Experience: Reap the Personalized Advantages by Completing Your Profile to Its Fullest. Update Here
Stay in the loop with the latest from Microchip. Update your profile while you are at it. Update Here
Complete your profile to access more resources. Update Here

Trust&GO LoRa® Secure Authentication with the ATECC608B Secure Element

Security with LoRaWAN™ Join Servers


When it comes to LoRa security, provisioning and storing network server and application server keys are as important as they are complex due to the nature of the shared key authentication model. Because of this, you will face three main challenges when implementing secure authentication on a LoRaWAN network:

  • Protecting the symmetric keys both in the network backend and at the edge node
  • Overcoming the manufacturing logistics of securely shipping and distributing the physical keys into millions of edge nodes
  • Preventing attackers who will be taking advantage of this known security weakness from accessing keys and exploiting your system

To overcome these challenges, you can strengthen the authentication process by implementing a secure hardened key storage both at the node and in the LoRaWAN backend. This prevents the exposure of authentication keys to software, firmware, manufacturing sites, end users and other third parties. Our secure elements—ATECC608B-TNGLORA for The Things Industries (TTI) and ATECC608B-TNGACT for Actility—are pre-provisioned with the corresponding authentication keys and provide a JIL “high” rated secure key storage to isolate keys in the nodes. This is especially valuable in LoRa systems that are based on a shared key security model and leverage a wide variety of traditional low-power microcontrollers.

To make adding secure elements to your design easier, the devices are paired with the join server services of either The Things Industries (TTI) or Actility for turnkey secure authentication. The corresponding AES128 authentication keys are also hosted and protected in their managed join servers. Through a claim procedure available via TTI’s or Actility’s web portal, the protected keys in the secure element are claimed and then owned by the company. This process simplifies the cumbersome and unsecure provisioning practice used without secure key storage. The join server is completely agnostic to the network server and/or application server providers to preserve business scalability, offering you freedom of choice in your architecture. Flexibility doesn’t stop here though. The secure element is a microcontroller-agnostic solution that adds hardware secure key storage to any LoRa-connected products.

Benefits of Using the Trust&GO ATECC608B for LoRa-Based Designs:


  • Pre-provisioned secure elements with authentication AES128 keys
  • Leverages Microchip’s secure provisioning service
  • Offers network- and application server-agnostic join servers
  • Works with both TTI and Actility
  • Simplifies logistics of shipping shared keys and reduces manufacturing costs
  • Provides a unique, trusted, protected and managed device identity
  • Is supported by Microchip and Arm® LoRaWAN stacks
  • Supports rekeying between join servers and the secure element
  • Provides JIL rated “high” secure key storage
  • Includes protection against anti-tampering, side-channel attacks
  • Provides microcontroller-agnostic implementation

Start Developing Your LoRa Solution with Four Hardware Options


To quickly begin developing your next LoRa-connected design with secure authentication, choose one of the following options and the steps for each will guide you through the process of selecting the hardware and setting up your join server account.

Develop with the SAM R34 LoRa SiP and Microchip LoRaWAN Stack on TTI Join Servers

Develop with the SAM R34 LoRa SiP and Semtech LoRaWAN Stack on TTI Join Servers

Develop with the SAM L21 MCU and Discrete Semtech Radio and Arm mBed™ OS LoRaWAN Stack on TTI Join Servers

Develop with the SAM R34 LoRa SiP and Microchip LoRaWAN Stack on Actility Join Servers

Trust Platform Products


Development Tools


Development Tool Description
CryptoAuthentication UDFN Socket Kit
(AT88CKSCKTUDFN-XPRO)
This board provides a uDFN8 socket to accommodate an ATECC608B or ATSHA204A secure element and an Xplained Pro (XPro) interface to develop solutions using the microcontrollers featured on our Xplained Pro boards.
SAM R34 Xplained Pro Evaluation Kit
(DM320111)
The SAM R34 Xplained Pro is a hardware platform designed to evaluate the SAM R34 family of LoRa® devices. This FCC, ISED and RED certified board is also an excellent reference design for developing SAM R34-based LoRa end-node applications.

Definitions


Credentials: Identity verification tools or methods that include X.509 certificates, generic certificates for thumbprint authentication, keys and data packets

Customization: The action of creating a unique device/system through its configuration and set of secrets

Firmware Verification: When a key and cryptographic operation are used to verify a signed image on a device at boot up or during run time

IP Protection: When a key and a cryptographic operation are used to verify signed (or hashed) firmware that is considered Intellectual Property (IP) of a product

Key(s): A set of binary numbers that is used to trigger a cryptographic algorithm that implements asymmetric or symmetric encryption

Over-the-Air (OTA) Verification: When a key and a cryptographic operation are used to verify a signed image that has been loaded into a connected device by a push notification from a cloud service

PKI: Public Key Infrastructure

Provisioning: The action of generating a credential into an embedded storage area

Thumbprint Certificate: An X.509 certificate not issued by a certificate authority that is used for authentication to the cloud

FAQS


How Does the Join Server Service Work?

The architecture of TTI’s or Actility’s join server services makes securing LoRaWAN connections both easy and portable. Their services are network server agnostic and application server agnostic, enabling you to protect your connection from anywhere at any time. Once a device identifies itself to join a LoRaWAN network, the network contacts the join server to verify that the identity comes from a trusted device and not a fraudulent one. The derived session keys are then sent securely to your network server and application server of choice. The join server supports any LoRaWAN network, from commercially operated networks to private networks built on open-source components.

We have also partnered with TTI and Actility to make the onboarding process of LoRaWAN devices seamless and secure. LoRaWAN device identities protected in the secure element are claimed by the join server provider with minimal intervention, eliminating the need for you to have expertise in security or add unnecessary supply chain costs. You can choose any LoRaWAN network and migrate to any other LoRaWAN join server by rekeying the device. This means that there is no vendor lock-in and you have full control over where and how the device keys are stored.

What Is the Value of a Configured and Provisioned Secure Element for LoRa-Based Systems?

Without a simplified onboarding process, such as the one provided by Microchip and TTI or Actility, the procedure to provision the authentication keys is not only complex but also unsecure. The handling of AES keys is particularly sensitive. You will need to be aware of the security risks associated with the deployment and management of a shared key model, not only in your hardware, but across all the stacks of the LoRa network. This includes the cloud backend architecture and all the steps involved in going from prototyping to production at a global scale.

During your prototyping and development phases, the first complexity will be selecting a technology provider in the segmented LoRa industry. Security, a well-known gap, needs to be added, significantly increasing the complexity of your design. Here are some questions you will need to answer:

  • How will you get started with securely provisioning authentication keys in secured storage?
  • How will you to develop, deploy and manage a join server on the LoRaWAN network?
  • How will you make sure the keys of the join server and the ones in the edge node match?
  • How will you avoid the keys leaking throughout the whole process?
  • How will you distribute shared keys securely?
  • How will you manufacture thousands of devices with a different key in each system?

Assuming these questions have been answered and you have designed in the necessary requirements, as you move onto production you will face the next question:

  • How will you implement a secure environment to handle millions of your shared keys between your join server provider, the site where keys are provisioned and across your complete supply chain—including your semiconductor vendor, distribution partner, design house and ODM—to finally arrive at the OEM?

To simplify the onboarding and logistics process, our bundled solution provides simple-to-use yet robust security foundations for developing LoRa products. Here are the basic steps you need to follow:

  1. Purchase the secure elements
  2. Open a join server account and activate it
  3. Claim the batch of secure elements to your join server account
  4. Start coding your application without the design burden of securing your authentication

Why Is Secure Hardware Key Storage So Important?

Security is often mistaken to mean just encryption. While encryption is an important aspect of security, encryption alone doesn’t solve all security needs. Encrypting and storing a key in a standard memory does not mean that a system is secure since firmware and software bugs are a natural part of coding and will always exist. There is another considerable attack surface to consider too. During the manufacturing process, keys and other cryptographic assets can be exposed to employees and equipment. All these backdoors can be exploited to spoof a key and inflict malicious actions on a device or system.

When you use an ATECC608B secure element combined with our provisioning service, you can isolate your keys from software, firmware, manufacturing, third-party companies and users. This solution also simplifies and reduces the cost and complexity of your supply chain by leveraging Microchip’s provisioning service.

The secure element is equipped with active anti-tampering protections as well as side-attack channel protections. All of the cryptographic functions involved with the key are in the same secure boundary as the secure element. This architecture can be used with any microprocessor or microcontroller to reduce backdoors to keys, providing a very affordable means of implementing a high grade of security. The ATECC608B secure element has been rated JIL “high” demonstrating its high robustness in protecting keys.

What Do You Really Get with This Configured and Provisioned ATECC608B for LoRaWAN-Connected Applications?

All ATECC608B-TNGLORA or ATECC608B-TNGACT secure elements provide:

  • An already defined and configured memory zone within the secure element with all the agreed policies necessary to work with the TTI (ATECC608B-TNGLORA) or Actility (ATECC608B-TNGACT) join server and the LoRaWAN authentication protocol. More precisely, these secure elements are configured for authentication, rekeying and secure boot use cases.
  • Already-provisioned keys for network servers and application servers. Both authentication keys are used to connect to the network and application LoRa server of your choice. TTI and Actility offer both network and application server services, but their join servers are agnostic of the network server and application server.

Trust&GO LoRa® Secure Authentication with Join Servers