Production-Ready, Full-Stack Edge AI Solutions Turn Microchip’s MCUs and MPUs Into Catalysts for Intelligent Real-Time Decision-Making
Company simplifies and accelerates edge AI system development with silicon, software, tools, production-ready applications and support from a growing partner ecosystem
Chandler, Ariz., February 10, 2026 — A major next step for artificial intelligence (AI) and machine learning (ML) innovation is moving ML models from the cloud to the edge for real-time inferencing and decision-making applications in today’s industrial, automotive, data center and consumer Internet of Things (IoT) networks. Microchip Technology (Nasdaq: MCHP) has extended its edge AI offering with full-stack solutions that streamline development of production-ready applications using its microcontrollers (MCUs) and microprocessors (MPUs) – the devices that are located closest to the many sensors at the edge that gather sensor data, control motors, trigger alarms and actuators, and more.
Microchip’s products are long-time embedded-design workhorses, and the new solutions turn its MCUs and MPUs into complete platforms for bringing secure, efficient and scalable intelligence to the edge. The company has rapidly built and expanded its growing, full-stack portfolio of silicon, software and tools that solve edge AI performance, power consumption and security challenges while simplifying implementation.
“AI at the edge is no longer experimental—it’s expected, because of its many advantages over cloud implementations,” said Mark Reiten, corporate vice president of Microchip’s Edge AI business unit. “We created our Edge AI business unit to combine our MCUs, MPUs and FPGAs with optimized ML models plus model acceleration and robust development tools. Now, the addition of the first in our planned family of application solutions accelerates the design of secure and efficient intelligent systems that are ready to deploy in demanding markets.”
Microchip’s new full-stack application solutions for its MCUs and MPUs encompass pre-trained and deployable models as well as application code that can be modified, enhanced and applied to different environments. This can be done either through Microchip’s embedded software and ML development tools or those from Microchip partners. The new solutions include:
- Detection and classification of dangerous electrical arc faults using AI-based signal analysis
- Condition monitoring and equipment health assessment for predictive maintenance
- Facial recognition with liveness detection supporting secure, on-device identity verification
- Keyword spotting for consumer, industrial and automotive command-and-control interfaces
Development Tools for AI at the Edge
Engineers can leverage familiar Microchip development platforms to rapidly prototype and deploy AI models, reducing complexity and accelerating design cycles. The company’s MPLAB® X Integrated Development Environment (IDE) with its MPLAB Harmony software framework and MPLAB ML Development Suite plug-in provides a unified and scalable approach for supporting embedded AI model integration through optimized libraries. Developers can, for example, start with simple proof-of-concept tasks on 8-bit MCUs and move them to production-ready high-performance applications on Microchip’s 16- or 32-bit MCUs.
For its FPGAs, Microchip’s VectorBlox™ Accelerator SDK 2.0 AI/ML inference platform accelerates vision, Human-Machine Interface (HMI), sensor analytics and other computationally intensive workloads at the edge while also enabling training, simulation and model optimization within a consistent workflow.
Other support includes training and enablement tools like the company’s motor control reference design featuring its dsPIC® DSCs for data extraction in a real-time edge AI data pipeline, and others for load disaggregation in smart e-metering, object detection and counting, and motion surveillance. Microchip also helps solve edge AI challenges through complementary components that are required for product design and development. These include PCIe® devices that connect embedded compute at the edge and high-density power modules that enable edge AI in industrial automation and data center applications.
The analyst firm IoT Analytics stated in its October 2025 market report that embedding edge AI capabilities directly into MCUs is among the top four industry trends, enabling AI-driven applications “...that reduce latency, enhance data privacy, and lower dependency on cloud infrastructure.” Microchip’s AI initiative reinforces this trend with its MCU and MPU platform, as well as its FPGAs. Edge AI ecosystems increasingly require support for both software AI accelerators and integrated hardware acceleration on multiple devices across a range of memory configurations.
Availability
Microchip is actively working with customers of its full-stack application solutions, providing a variety of model training and other workflow support. The company is also working with multiple partners whose software provides developers with additional deployment-ready options. To learn more about Microchip’s edge AI offering and new full-stack solutions, visit www.microchip.com/EdgeAI. Additional information on each solution can be found at Microchip’s on-demand Edge AI Webinar Series, starting February 17.
Resources
High-res images available through Flickr or editorial contact (feel free to publish):
- Application image: www.flickr.com/photos/microchiptechnology/55062918660/sizes/o/
About Microchip
Microchip Technology Inc. is a broadline supplier of semiconductors committed to making innovative design easier through total system solutions that address critical challenges at the intersection of emerging technologies and durable end markets. Its easy-to-use development tools and comprehensive product portfolio support customers throughout the design process, from concept to completion. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support and delivers solutions across the industrial, automotive, consumer, aerospace and defense, communications and computing markets. For more information, visit the Microchip website at www.microchip.com.
###
Note: The Microchip name and logo, the Microchip logo, dsPIC and MPLAB are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. VectorBlox is a trademark of Microchip Technology Inc. in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.
Brian Thorsen
480-792-7182
brian.thorsen@microchip.com