Microchip logo
Microchip logo
  • All
  • Products
  • Documents
  • Applications Notes

Press Release


Industry’s First ‘zigbee PRO with Green Power Certified Platform’ Unveiled by Microchip

BitCloud 4.0 Complete zigbee Software Development Kit is Available Now

CHANDLER, Ariz., Feb. 13, 2017 — The industry’s first zigbee alliance certified zigbee®platform with zigbee PRO and Green Power features (formerly known as zigbee 3.0) from a semiconductor company is now available from Microchip Technology Inc. (NASDAQ: MCHP), a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions. With greater interoperability and lower latency than ever before, this software stack and corresponding BitCloud 4.0 software development kit are ideal for the design of home automation, commercial lighting, smart energy and Internet of Things (IoT) applications. For more information about the complete software development kit, visit: www.microchip.com/bitcloud.

The zigbee certified solution enables cross-functional device support and will be backward-compatible with existing zigbee certified products for seamless interoperability. Along with the zigbee PRO (2015) feature set, developers can expect to find features such as low latency suitable for RF remote applications, mesh networking for large networks such as lighting applications, and the Green Power benefits of an energy harvesting switch.

The zigbee PRO Green Power feature, making its debut on the new certified software stack, enables battery-less devices to securely join a network while leveraging eco-friendly energy sources such as light, vibration or motion. Additionally, zigbee Light Link and zigbee Home Automation device types are now fully supported.

“We’re proud to be the first silicon manufacturer to offer a zigbee certified platform with zigbee PRO and Green Power features,” said Steve Caldwell, vice president of Microchip’s Wireless Solutions Group. “With both our hardware and SDK, we’re able to provide best-in-class functionality for a wide range of applications from large-scale commercial lighting to ultra-low power battery-less devices.” 

“Having a long-standing member company like Microchip continue to invest in the creation and commercialization of new platforms based on our latest standards shows the strength of the zigbee market,” said Victor Berrios, Vice President of Technology, zigbee alliance. “This zigbee platform enables developers to create new, ground-breaking and interoperable designs for connected applications.”

Development Support
To bring zigbee designs to market faster, Microchip offers the BitCloud 4.0 Software Development Kit (SDK). The SDK enables application development on the SAM R21 Xplained Pro Evaluation Kit, a Cortex® M0+-based 32-bit microcontroller with an integrated 2.4GHz 802.15.4 compliant radio. When used with the newly certified software stack, the SDK provides a complete zigbee certified development platform.

Pricing and Availability
Microchip currently offers two platforms to begin zigbee development. The SAM R21 Xplained Pro Evaluation Kit (ATSAMR21-XPRO) is available for $58 and the SAM R21 zigbee Light Link Evaluation Kit (ATSAMR21ZLL-EK) can be purchased for $92.

For additional information, contact any Microchip sales representative or authorized worldwide distributor. To purchase products mentioned in this press release, go to microchipDIRECT (https://www.microchipdirect.com/productsearch.aspx?Keywords=sam%20r21) or contact one of Microchip’s authorized distribution partners.

Resources
High-res images available through Flickr or editorial contact (feel free to publish):

About Microchip Technology
Microchip Technology Inc. (NASDAQ:  MCHP) is a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide.  Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality.  For more information, visit the Microchip website at www.microchip.com.

 
Images

About Microchip Technology
Microchip Technology Inc. (NASDAQ: MCHP) is a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at http://www.microchip.com/Homepage-041715a

###

Note:
Tags / Keywords:

Editorial Contact:
Kimberly Kulesh
480-792-4531
kimberly.kulesh@microchip.com

Reader Inquiries:
1-888-624-7435
www.microchip.com