• AVR Freaks

CDC PC Examples in the Windows Vista/7 64-bit operating system

Author
xiaofan
Super Member
  • Total Posts : 6247
  • Reward points : 0
  • Joined: 2005/04/14 07:05:25
  • Location: Singapore
  • Status: offline
2010/03/21 07:40:11 (permalink)
0

CDC PC Examples in the Windows Vista/7 64-bit operating system

The release notes of USB Stack V2.6a mentions this.

3. CDC PC Examples in the Windows Vista 64-bit operating system

The CDC PC example code does not run as implemented on the 64-bit version of the Windows Vista operating system. The .NET SerialPort object does not appear to receive data as implemented in these examples.



What about Windows 7 64bit? I guess it is still the same. I do not have any 64bit Windows but maybe I will get one with Windows 7 64bit in the future.


Is this related to the bug in .Net serial components (2.0 -- 3.5). It seems to me Microsoft kind of really gave up on the component (similar to usbser.sys).

http://connect.microsoft.com/VisualStudio/feedback/details/426766/net-serialport-and-ftdi-usb-driver-unauthorizedaccessexception#
https://connect.microsoft.com/VisualStudio/feedback/details/140018/serialport-crashes-after-disconnect-of-usb-com-port


  USB_Links and libusb
#1

0 Replies Related Threads

    Jump to:
    © 2020 APG vNext Commercial Version 4.5