• AVR Freaks

MCHPFSUSB v2.6a Released

Author
USBApplicationsTeam
Moderator
  • Total Posts : 7
  • Reward points : 0
  • Joined: 2009/05/28 08:40:17
  • Location: 0
  • Status: offline
2010/03/01 09:11:18 (permalink)
0

MCHPFSUSB v2.6a Released

New to v2.6a
  • Device
    • Bug fixes
    • Changed how the PIC24F HID bootloader works to simplify interrupt usage

  • Host
    • Bug fixes

 
MCHPFSUSB v2.6a is distributed with Microchip Applications Libraries v2009-02-09 and can be downloaded from the Software link on the USB design center (www.microchip.com/usb).
 
Please note that there are two download sections on the software page.  The first link has the MCHPFSUSB v2.6a stack.  The second has the PIC32 legacy stack.

For more information about Microchip's USB offerings please refer to www.microchip.com/usb

For support, please contact http://support.microchip.com
#1

3 Replies Related Threads

    xiaofan
    Super Member
    • Total Posts : 6247
    • Reward points : 0
    • Joined: 2005/04/14 07:05:25
    • Location: Singapore
    • Status: offline
    RE: MCHPFSUSB v2.6a Released 2010/03/21 07:50:07 (permalink)
    0

    5. HID Examples on Macintosh and Linux machines
    Devices that implement the HID demos will enumerate successfully on both Linux and Macintosh based operating systems. Currently there is not an example program to interface these devices on Macintosh and Linux machines.


    Under Mac, maybe it is a bit of work to use the native HID API.

    But under Linux, it is not that difficult to modify the libusb example (change the VID/PID) to work with the HID examples. The HID bootloader may require more efforts.

      USB_Links and libusb
    #2
    xiaofan
    Super Member
    • Total Posts : 6247
    • Reward points : 0
    • Joined: 2005/04/14 07:05:25
    • Location: Singapore
    • Status: offline
    RE: MCHPFSUSB v2.6a Released 2010/03/21 07:53:34 (permalink)
    0

    6. LibUSB example on Macintosh
    Devices that implement the Simple HID demo will enumerate successfully on Macintosh based operating systems (provided the correct drivers are installed). Currently there is not an example program to communicate to these devices on these operating systems in this installation.


    Hmm, Mac OS X has the libusb port. So it should not be too difficult to build the example under Mac OS X.

      USB_Links and libusb
    #3
    xiaofan
    Super Member
    • Total Posts : 6247
    • Reward points : 0
    • Joined: 2005/04/14 07:05:25
    • Location: Singapore
    • Status: offline
    RE: MCHPFSUSB v2.6a Released 2010/03/28 06:57:38 (permalink)
    0

    3. CDC PC Examples in the Windows Vista 64-bit operating system

    The CDC PC example code does not run as implemented on the 64-bit version of the Windows Vista operating system. The .NET SerialPort object does not appear to receive data as implemented in these examples.


    http://www.microchip.com/forums/tm.aspx?m=487021

    My guess is that it will not work under Windows 7 64bit either. Maybe this is due to problems with the dotnet serial component.

      USB_Links and libusb
    #4
    Jump to:
    © 2020 APG vNext Commercial Version 4.5