• AVR Freaks

Code 1 through Code 10 USB Enumeration Problem

Author
xiaofan
Super Member
  • Total Posts : 6247
  • Reward points : 0
  • Joined: 2005/04/14 07:05:25
  • Location: Singapore
  • Status: offline
2009/05/11 03:33:05 (permalink)
0

Code 1 through Code 10 USB Enumeration Problem

Code 1 through Code 10 from Microsoft
http://support.microsoft.com/kb/310123

Code 10: what is the reason
http://support.microsoft.com/kb/943104/

  USB_Links and libusb
#1

4 Replies Related Threads

    fajardiary
    Super Member
    • Total Posts : 245
    • Reward points : 0
    • Joined: 2009/02/19 03:51:17
    • Location: Indonesia
    • Status: offline
    RE: Code 1 through Code 10 USB Enumeration Problem 2009/05/11 04:49:34 (permalink)
    0
    Dear Xiaofan,

    I am having this problem. I am using PIC18F14K50 from Microchip. This is the LAB 1. HID Enumeration demo.

    This device cannot start. (Code 10)

    Click 'Check for solutions' to send data about this device to Microsoft and to see if there is a solution available.

    I have read the link you gave, but still..not working..

    this happens on vista and xp computers..

    Kindest Regards,




    Fajar
    #2
    xiaofan
    Super Member
    • Total Posts : 6247
    • Reward points : 0
    • Joined: 2005/04/14 07:05:25
    • Location: Singapore
    • Status: offline
    RE: Code 1 through Code 10 USB Enumeration Problem 2009/05/11 06:37:48 (permalink)
    0
    Are you using the official demo board and the official firmware? 

      USB_Links and libusb
    #3
    fajardiary
    Super Member
    • Total Posts : 245
    • Reward points : 0
    • Joined: 2009/02/19 03:51:17
    • Location: Indonesia
    • Status: offline
    RE: Code 1 through Code 10 USB Enumeration Problem 2009/05/11 06:43:31 (permalink)
    0
    I am using microchip Low Pin count USB. When I used the sample program, it works correctly, so I guest the problem is from the software configuration.
     
    Kindest Regards,
     
     
    Fajar
    #4
    xiaofan
    Super Member
    • Total Posts : 6247
    • Reward points : 0
    • Joined: 2005/04/14 07:05:25
    • Location: Singapore
    • Status: offline
    RE: Code 1 through Code 10 USB Enumeration Problem 2009/05/11 07:33:32 (permalink)
    0
    So you are using your own program. Then you need to post your program for more help.

      USB_Links and libusb
    #5
    Jump to:
    © 2020 APG vNext Commercial Version 4.5