• AVR Freaks

Have you? SPI in Slave Mode Frame Slave Mode

Author
bellhop
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2009/05/06 06:22:31
  • Location: 0
  • Status: offline
2009/05/06 06:34:08 (permalink)
0

Have you? SPI in Slave Mode Frame Slave Mode

Have you used the SPI port in 16 bit Slave Mode Frame Slave Mode with Enhanced Buffers? Do you know what happens after 16 clocks? I would like the port to continue loading data to the shift register and generating flags/interrupts. The Frame Sync will arrive once every 32 clocks. If you know the answer to this question, then you can save me having to order parts, build a circuit, and write code only to scrap it all if the SPI port cannot do this thing. I would be most grateful.


#1

0 Replies Related Threads

    Jump to:
    © 2021 APG vNext Commercial Version 4.5