• AVR Freaks

SSD1906 with External TFT

Author
mm_rnd
New Member
  • Total Posts : 15
  • Reward points : 0
  • Joined: 2009/02/10 06:57:59
  • Location: 0
  • Status: offline
2009/04/16 06:39:18 (permalink)
0

SSD1906 with External TFT

Dear All

I have connected an External TFT with SSD1906 on Graphic Pictail board.
The display is working fine but the refresh rate of the screen is very slow.
I have made some corrections in "void DelayMs(WORD time)" but not sure how to fix it.

I have removed the 25MHz crystal and attached a 48MHz crystal to the SSD1906.
I have also changed the resistor and the capacitors next to Y1,

R7 = 127ohms
C6 and C7 = 26pF

Any ideas how I can improve the refresh rate of this TFT screen?

Thank You
#1

0 Replies Related Threads

    Jump to:
    © 2021 APG vNext Commercial Version 4.5