• AVR Freaks

rs-232 and ds33fj128mc804

Author
berkandincay
New Member
  • Total Posts : 4
  • Reward points : 0
  • Joined: 2009/02/26 09:15:45
  • Location: 0
  • Status: offline
2009/03/01 06:29:10 (permalink)
0

rs-232 and ds33fj128mc804

I got explorer 16 and ds33fj128mc804 i am trying to make rs232 connection to pc but my problem is ds33fj128mc804 uart pins are not connected to the inputs of the development board?I am looking for a way to connect my uart2 RX and TX to the pins 49 and 50 in the development board to use rs-232.
#1

6 Replies Related Threads

    MBedder
    Circuit breaker
    • Total Posts : 6973
    • Reward points : 0
    • Joined: 2008/05/30 11:24:01
    • Location: Zelenograd, Russia
    • Status: offline
    RE: rs-232 and ds33fj128mc804 2009/03/01 07:03:58 (permalink)
    0
    The ds33fj128mc804 has a Peripheral Pin Select function which allows you to remap the peripheral i/o to virtually any of the package pins in software. It is a good idea to read a device datasheet and reference manual prior to starting a development.
    #2
    p.erasmus
    Super Member
    • Total Posts : 1799
    • Reward points : 0
    • Joined: 2004/11/25 03:18:34
    • Location: Saratov Russia
    • Status: offline
    RE: rs-232 and ds33fj128mc804 2009/03/01 08:12:02 (permalink)
    0
    I agree with this one
     

    Automotive Engineering

    #3
    Neiwiertz
    Super Member
    • Total Posts : 2131
    • Reward points : 0
    • Joined: 2004/09/01 02:58:52
    • Status: offline
    RE: rs-232 and ds33fj128mc804 2009/03/01 08:42:03 (permalink)
    0
    Yeah, certain read the  section 17 uart reference manual, and datasheet part peripheral pin select as mentioned above. Additonal you might have a look at those collection(s) of members helpfull reply's

    E16 MA330018  - dsPIC33FJ128MC804 PIM

    E16 Peripheral Pin Select Map Input/Ouput Functions Of PIM

    Flying With --|Explorer 16|HardWare|SoftWare|-- Fav(s) Gallery Lists
    #4
    berkandincay
    New Member
    • Total Posts : 4
    • Reward points : 0
    • Joined: 2009/02/26 09:15:45
    • Location: 0
    • Status: offline
    RE: rs-232 and ds33fj128mc804 2009/03/01 12:40:14 (permalink)
    0
    i solved my problem finally soldering two empty pins to correspond pin 49 and pin 50 on the board because max232 is connected to pin49 and pin 50(uart2 RX-TX)
    #5
    MBedder
    Circuit breaker
    • Total Posts : 6973
    • Reward points : 0
    • Joined: 2008/05/30 11:24:01
    • Location: Zelenograd, Russia
    • Status: offline
    RE: rs-232 and ds33fj128mc804 2009/03/01 12:55:50 (permalink)
    0
    Hmm, looks like the PIM developers failed to route these important pins at all. Sorry for misunderstanding your problem and for mentor tone[:@]
    #6
    Neiwiertz
    Super Member
    • Total Posts : 2131
    • Reward points : 0
    • Joined: 2004/09/01 02:58:52
    • Status: offline
    RE: rs-232 and ds33fj128mc804 2009/03/01 15:09:11 (permalink)
    0
    Good catch see if we can make a picture of the PIM itself which shows this issue to put this at the E16 list

    Flying With --|Explorer 16|HardWare|SoftWare|-- Fav(s) Gallery Lists
    #7
    Jump to:
    © 2021 APG vNext Commercial Version 4.5