• AVR Freaks

Problem of Configuration Word Editor dialog in PICkit2v2.60

Author
air_variable
New Member
  • Total Posts : 17
  • Reward points : 0
  • Joined: 2007/02/22 02:50:26
  • Location: Japan
  • Status: offline
2009/02/01 09:44:11 (permalink)
0

Problem of Configuration Word Editor dialog in PICkit2v2.60

I installed a new PICkit2 Programmer Software v2.60.
It is convenience that I can operate bit of Coufiguration word.
 
By the way, it is the function, but one part of the indication lacks.
(see attach the screen shot,please) 




However, this does not have any problem functionally.
I wish it is improved by the next version update.
I report it.
 
Operation environment:
 Windows XP SP2 Japanese version
 
Thanking you in advance.
 

post edited by air_variable - 2011/12/24 03:17:46
#1

3 Replies Related Threads

    PICkit2Dev
    Super Member
    • Total Posts : 994
    • Reward points : 0
    • Joined: 2006/09/27 08:41:47
    • Location: 0
    • Status: offline
    RE: Problem of Configuration Word Editor dialog in PICkit2v2.60 2009/02/01 12:05:52 (permalink)
    0
    Do you have the display DPI set to a value other than 92?  This would help in determining the cause of the problem.
     
    Thanks.
     
     
    #2
    air_variable
    New Member
    • Total Posts : 17
    • Reward points : 0
    • Joined: 2007/02/22 02:50:26
    • Location: Japan
    • Status: offline
    RE: Problem of Configuration Word Editor dialog in PICkit2v2.60 2009/02/01 17:26:40 (permalink)
    0
    Thank you for reply.
     
    Indication became normal when it changed setting of DPI.
       However, this setting is not normal setting in Japanese windows.
     
    (usage:DPI setting(D) normal size(96DPI),Large size(120DPI),Custom setting...) 

     
     
     
    96DPI becomes default, and Japanese windows becomes the setting of 96% by custom setting in 92DPI.
     


    For wish, I think that it is desirable for it to be displayed in a state of windows default.
     
    To above information thanking you in advance.

     

    post edited by air_variable - 2011/12/24 03:21:22
    #3
    PICkit2Dev
    Super Member
    • Total Posts : 994
    • Reward points : 0
    • Joined: 2006/09/27 08:41:47
    • Location: 0
    • Status: offline
    RE: Problem of Configuration Word Editor dialog in PICkit2v2.60 2009/02/01 18:41:38 (permalink)
    0
    Thank you for the reply.  Now that it is known that DPI is the issue, this issue can be fixed in a software update.
    #4
    Jump to:
    © 2019 APG vNext Commercial Version 4.5