Help about MCP2510
Hi everybody,
I hope there will someone who can help me. I have developped 2 devices wich are minked with CAN protocole. 1 device had a 24FJ128GB206 + MCP2510 and the other had a 18F87J60 + MCP2510. The couple 24FJ128GB206 + MCP2510 work very well whereas 18F87J60 + MCP2510 don't work. No CAN message is drive out. The code to drive the MCP2510 is the same in the 2 cases. If someone have an idea, it would be fine.
Thanks by advance