• AVR Freaks

Getting started with PIC32MZ, Harmony and explorer 16/32

Author
tclodic
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2017/06/06 06:47:44
  • Location: 0
  • Status: offline
2017/06/08 07:12:27 (permalink)
0

Getting started with PIC32MZ, Harmony and explorer 16/32

Hello

I have a PIC32MZ2048EFH100, an explorer 16/32 dev kit, MpLab 3.61 and Harmony (last  1.x version)

I managed to blink led using timer and PWM following lab 1.a of the TLS4102 lab manual which uses Harmony 1.06.
However I don't manage to use a switch. There is nothing called "push_button" or "switch" in the device tree.
I don't manage to crate an UART communication either (following lab 1.b of the previously mentionned pdf). The pin 61 isn't available and i don't know which one to use or where I can get an info.

Could you help me please ?

Thank you in advance
#1
RISC
Super Member
  • Total Posts : 5381
  • Reward points : 0
  • Status: offline
Re: Getting started with PIC32MZ, Harmony and explorer 16/32 2017/06/09 09:02:44 (permalink)
0
Hi,
The TLS4102 lab manual is originally meant for the PIC32MZ EF starter kit hardware (not the Explorer1632).
So you'll need to adapt a lot of things to match the EXPLORER1632, especially because the PIC32MZ EF starter kit and EXPLORER1632 have very different on-board hardware...
Regards
 
#2
Jump to:
© 2020 APG vNext Commercial Version 4.5