Devices with SMSC marking

Author
gideonz74
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2017/02/08 02:37:07
  • Location: 0
  • Status: offline
2017/02/15 13:16:07 (permalink)
0

Devices with SMSC marking

As of 2012, SMSC is part of Microchip, and Microchip sells parts that were previously manufactured by SMSC, such as the ULPI PHY chips and USB HUBs.
 
Now, the curious thing is, that since I have moved my production of one product to the far east, I have received boards with SMSC chips on them (USB2513B), with a date code of "1622", while a previous production run had "1543" or something on them, with the Microchip logo (USB2513B). So, in summary: 2016 chips from SMSC and 2015 chips from Microchip. The ones from 2015 were bought through "Microchip Direct", and the 2016 chips came from a supplier in China.
 
Is this at all possible, or are we looking into counterfeited chips?
 
#1

2 Replies Related Threads

    simong123
    Lab Member No. 003
    • Total Posts : 1283
    • Reward points : 0
    • Joined: 2012/02/07 18:21:03
    • Location: Future Gadget Lab (UK Branch)
    • Status: offline
    Re: Devices with SMSC marking 2017/02/15 13:40:29 (permalink)
    3 (1)
    I would contact your local Microchip rep, giving details about when and where you sourced the chips, or raise a support ticket. I'm sure they will be very helpfull in dealing with possible counterfeit chips. You are unlikely to get a response here as this is a user forum, and the right MCHP staff are unlikely to be monitoring the Buy, Sell, Trade' forum.
    I certainly wouldn't trust them until I heard back, but it is possible they were just packaged at a different plant.
    #2
    roundrocktom
    Super Member
    • Total Posts : 1009
    • Reward points : 0
    • Joined: 2012/09/07 08:19:09
    • Location: Texas
    • Status: offline
    Re: Devices with SMSC marking 2017/03/02 12:35:45 (permalink)
    3 (1)
    Did you ever contact Microchip to check?
    microchip.com/support
     
    Post a close up photo's on both parts on something like IMGUR and post up the link.
    #3
    Jump to:
    © 2018 APG vNext Commercial Version 4.5