• AVR Freaks

Pic32mzef Develolpmet Bundle(Compiler,IDE,License)

Author
avil
Starting Member
  • Total Posts : 33
  • Reward points : 0
  • Joined: 2016/06/16 11:57:50
  • Location: 0
  • Status: offline
2016/11/06 22:01:40 (permalink)
0

Pic32mzef Develolpmet Bundle(Compiler,IDE,License)

Hi,
         we have used pic18f87j60 Controller for our firmware development,We want to upgrade it to a pic32 microcontroller.
 
We have chosen pic32mz2048EFH144 microcontroller .
 
I would like to know the suitable development board for  my testing.
 
Also would like to know the Compiler ,and other licenses to be procured for the same.
 
Specifically i found 2 suitable boards
 
1) DM320104 (Curiosity Development Board pic32mzef)
 
2) pic32MzEC starter kit
 
 
Does the Ethernet module  , and other Software packages come along with it?
#1
NKurzman
A Guy on the Net
  • Total Posts : 17246
  • Reward points : 0
  • Joined: 2008/01/16 19:33:48
  • Location: 0
  • Status: offline
Re: Pic32mzef Develolpmet Bundle(Compiler,IDE,License) 2016/11/06 22:39:29 (permalink)
0
The starter kit comes with USB and TCP/IP.
What else do you need.
You will need MPLabX and XC32.
You can start in free or eval mode.
After that you can buy it or rent it monthly.
You will likely need the Harmony frame work.

I think the explorer boards have a pin with you pic.
#2
Jim Nickerson
User 452
  • Total Posts : 5892
  • Reward points : 0
  • Joined: 2003/11/07 12:35:10
  • Location: San Diego, CA
  • Status: offline
Re: Pic32mzef Develolpmet Bundle(Compiler,IDE,License) 2016/11/07 08:35:21 (permalink)
0
The DM320104 needs the http://www.microchip.com/...px?PartNO=ac320004-3to do wired Ethernet, it comes with Wi-Fi
 
 
post edited by Jim Nickerson - 2016/11/07 08:36:27
#3
Jump to:
© 2019 APG vNext Commercial Version 4.5