• AVR Freaks

Hot!using Digital Filter Design Tool SW300001 with dspic33F and dspic33E

Author
JavierJames
New Member
  • Total Posts : 3
  • Reward points : 0
  • Joined: 2016/06/02 05:41:50
  • Location: 0
  • Status: offline
2016/06/13 06:49:03 (permalink)
0

using Digital Filter Design Tool SW300001 with dspic33F and dspic33E

Hello,

I want to use the Digital Filter Design Tool but I have a few questions.
1) Is the DFD Tool still supported? Because  I did not see it listed in this forum.
2) I read in one document that the DFD Tool is for the dspic30F/dspic33F family ( ).  But on a next site I read it is only for the dspic33F X30 compiler. ( ). Could this tool actually be used with the dsPIC33F?

3) I have not read anywhere where it states if it possible to use with other dspic, such as the dspic33E.  Can I use the DFD Tool with the dspic33E family?


#1

4 Replies Related Threads

    du00000001
    Just Some Member
    • Total Posts : 3670
    • Reward points : 0
    • Joined: 2016/05/03 13:52:42
    • Location: Germany
    • Status: offline
    Re: using Digital Filter Design Tool SW300001 with dspic33F and dspic33E 2016/06/13 09:07:44 (permalink)
    3 (1)
    From the manual (http://ww1.microchip.com/downloads/en/DeviceDoc/SW300001%20manual.pdf):
    Introduction to Filter Design for Microchip Technology dsPIC30F/dsPIC33F

    So any dsPIC is supported.
     
    And it is still sold:
    http://www.microchipdirect.com/ProductSearch.aspx?Keywords=SW300001
     
    #2
    JavierJames
    New Member
    • Total Posts : 3
    • Reward points : 0
    • Joined: 2016/06/02 05:41:50
    • Location: 0
    • Status: offline
    Re: using Digital Filter Design Tool SW300001 with dspic33F and dspic33E 2016/06/15 04:48:01 (permalink)
    0
    Dear ,
     
    Thank you for your response.
    It was helpful.
     
    Best Regards,
    Javier
    #3
    rfjhh
    Starting Member
    • Total Posts : 63
    • Reward points : 0
    • Joined: 2012/07/26 09:19:36
    • Location: 0
    • Status: offline
    Re: using Digital Filter Design Tool SW300001 with dspic33F and dspic33E 2019/08/13 08:59:09 (permalink)
    0
    How can I get the Filter Design Tool?
     
    #4
    du00000001
    Just Some Member
    • Total Posts : 3670
    • Reward points : 0
    • Joined: 2016/05/03 13:52:42
    • Location: Germany
    • Status: offline
    Re: using Digital Filter Design Tool SW300001 with dspic33F and dspic33E 2019/08/13 09:11:50 (permalink)
    0
    Sorry - looks like this one is no longer available.
    Listed as obsolete at the distributors, no longer available at microchipdirect, so sad  . . .
    you might want to use g..gl. to find another digital filter design tool.
    Preferably for free  Smile  ???
     
    There seem to be some available.
     
    And - please - don't surprise me by just needing a low-pass filter!

    PEBKAC / EBKAC / POBCAK / PICNIC (eventually see en.wikipedia.org)
    #5
    Jump to:
    © 2020 APG vNext Commercial Version 4.5