• AVR Freaks

MPFS Upload Error

Author
gary7
Starting Member
  • Total Posts : 56
  • Reward points : 0
  • Joined: 2013/03/22 13:54:08
  • Location: Winston Salem
  • Status: offline
2016/05/18 18:08:11 (permalink)
0

MPFS Upload Error

I generate a .bin file using the MPFS generator and when I try to upload it I get an error, "MPFS Image Corrupt or Wrong Version". I am using Harmony and the 'web_server_nvm_mpfs demo'.

 
I have set the Include HTTP Custom Template and Enable HTTP Update checked in the Harmony set up. It runs the embedded web pages fine. But when I generate the same pages from the included src web page files I get the error. I seem to recall a #define in the MLA version that controlled this.
 
Also have the NVM setup and Enable Erase Write Function set. It seems that it is running fine otherwise.
 
Any help?
#1

4 Replies Related Threads

    NKurzman
    A Guy on the Net
    • Total Posts : 19116
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: offline
    Re: MPFS Upload Error 2016/05/18 18:33:08 (permalink)
    0
    What Version of harmony?
    Are you using the MPFS generator form that installation?
    #2
    gary7
    Starting Member
    • Total Posts : 56
    • Reward points : 0
    • Joined: 2013/03/22 13:54:08
    • Location: Winston Salem
    • Status: offline
    Re: MPFS Upload Error 2016/05/19 06:19:59 (permalink)
    0
    Everything is most current and from the same version.
     
    Is there a setting to use the MPFS and not the embedded c-code web pages?
    #3
    Ajith Tomy
    New Member
    • Total Posts : 14
    • Reward points : 0
    • Joined: 2016/12/30 02:41:27
    • Location: India
    • Status: offline
    Re: MPFS Upload Error 2018/10/11 03:14:32 (permalink)
    0
    MPFS upload work fine in harmony 1_04_2, for harmony 2_05_1:- got an error, MPFS Image Corrupt or Wrong Version
    I use the same web pages given with harmony
    #4
    Jim Nickerson
    User 452
    • Total Posts : 6851
    • Reward points : 0
    • Joined: 2003/11/07 12:35:10
    • Location: San Diego, CA
    • Status: offline
    Re: MPFS Upload Error 2018/10/11 06:10:41 (permalink)
    0
    colour_pencils
    MPFS upload work fine in harmony 1_04_2, for harmony 2_05_1:- got an error, MPFS Image Corrupt or Wrong Version
    I use the same web pages given with harmony

    As you have the source code maybe you could search for the error message text to see what specifically it is complaining about.
    #5
    Jump to:
    © 2021 APG vNext Commercial Version 4.5