• AVR Freaks

RN42 and Windows 10

Author
jdreitzler
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2015/03/05 11:47:30
  • Location: 0
  • Status: offline
2015/10/08 12:16:47 (permalink)
0

RN42 and Windows 10

Does the RN42 work with Windows 10?
 
I have a custom Bluetooth board that works on other versions of Windows.  Recently bought a Windows 10 laptop but it will not see the RN42 device.  It will see other Bluetooth devices.
 
The custom board uses SSP.
 
J
#1

1 Reply Related Threads

    RISC
    Super Member
    • Total Posts : 5392
    • Reward points : 0
    • Status: offline
    Re: RN42 and Windows 10 2015/10/16 12:53:52 (permalink)
    0
    Hi,
    Which firmware version do you have on your RN42 device ?
    Regards
    #2
    Jump to:
    © 2020 APG vNext Commercial Version 4.5