• AVR Freaks

Hot!inacurately red squiggly underlined variables

Author
pgibbons
Starting Member
  • Total Posts : 53
  • Reward points : 0
  • Joined: 2014/08/02 18:00:45
  • Location: 0
  • Status: offline
2015/10/04 08:18:31 (permalink)
0

inacurately red squiggly underlined variables

This is another issue that's been going on for years now. Sometimes MPLAB X starts underlining stuff in red, even though it is correct and will compile perfectly fine. My only solution is to restart the program.
Overall I'm very happy with MPLAB X, just a few things that I wish got fixed at some point (from one programmer to another)...
#1

8 Replies Related Threads

    DarioG
    Allmächtig.
    • Total Posts : 54081
    • Reward points : 0
    • Joined: 2006/02/25 08:58:22
    • Location: Oesterreich
    • Status: offline
    Re: inacurately red squiggly underlined variables 2015/10/04 08:29:15 (permalink)
    0
    This is a common and known one, and has been for years... Smile

    GENOVA :D :D ! GODO
    #2
    pgibbons
    Starting Member
    • Total Posts : 53
    • Reward points : 0
    • Joined: 2014/08/02 18:00:45
    • Location: 0
    • Status: offline
    Re: inacurately red squiggly underlined variables 2015/10/04 08:42:05 (permalink)
    +1 (1)
    yeah I know :)
    Let's see if the new version fixed it.
    #3
    Aussie Susan
    Super Member
    • Total Posts : 3725
    • Reward points : 0
    • Joined: 2008/08/18 22:20:40
    • Location: Melbourne, Australia
    • Status: offline
    Re: inacurately red squiggly underlined variables 2015/10/04 18:14:20 (permalink)
    +2 (2)
    Please do not hold your breath!
    Susan
    #4
    XGenerator
    Administrator
    • Total Posts : 351
    • Reward points : 0
    • Joined: 2009/10/12 12:11:03
    • Location: 0
    • Status: offline
    Re: inacurately red squiggly underlined variables 2015/10/05 08:23:43 (permalink)
    +2 (2)
    It is true the red bangs have been a source concern for a long time. There is not one simple solution to fix everything that occurs when this happens.
    If one thinks of the IDE as a totally separate tool to the compiler it does help try to understand the paradigm. The IDE is NOT the compiler so it is necessary to feed all the compiler details into the parser correctly for each device not just each compiler.
    We are working on this and have been for a while. We are getting closer but totally understand we are not there yet. Some architectures like PIC32 and PCI24/33s behave a lot more reliably than the 8 bit. It is not necessary to try to explain in depth all the facets of this issue but re-assured we do have this as a high focus among the other tasks of supporting new silicon device that stream out.
    Thanks for your patience.
     
    #5
    Gort2015
    Klaatu Barada Nikto
    • Total Posts : 3954
    • Reward points : 0
    • Joined: 2015/04/30 10:49:57
    • Location: 0
    • Status: online
    Re: inacurately red squiggly underlined variables 2017/08/22 12:15:29 (permalink)
    +1 (1)
    Still no fix, underlined errors in C comments.
    Got rid of it once but now it is back since deleting mplabx v.4.00 which deleted all my v3.65 settings, colors, open projects, everything.
    back to v3.65

    MPLab X playing up, bug in your code? Nevermind, Star Trek:Discovery will be with us soon.
    https://www.youtube.com/watch?v=Iu1qa8N2ID0
    + ST:Continues, "What Ships are Made for", Q's back.
    #6
    Gort2015
    Klaatu Barada Nikto
    • Total Posts : 3954
    • Reward points : 0
    • Joined: 2015/04/30 10:49:57
    • Location: 0
    • Status: online
    Re: inacurately red squiggly underlined variables 2017/08/23 00:30:56 (permalink)
    +3 (3)
    Tools->Options->Editor->Spellchecker
     
    Untick C/C++/Fortran Comments.

    MPLab X playing up, bug in your code? Nevermind, Star Trek:Discovery will be with us soon.
    https://www.youtube.com/watch?v=Iu1qa8N2ID0
    + ST:Continues, "What Ships are Made for", Q's back.
    #7
    mcovington
    New Member
    • Total Posts : 18
    • Reward points : 0
    • Joined: 2019/07/12 09:19:40
    • Location: 0
    • Status: offline
    Re: inacurately red squiggly underlined variables 2019/07/14 12:25:55 (permalink)
    0
    In the latest version I am seeing things like RC0 underlined red, with pop-ups saying they are unrecognized names, even though they are in fact correct.
    #8
    ric
    Super Member
    • Total Posts : 27676
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: offline
    Re: inacurately red squiggly underlined variables 2019/07/15 18:42:17 (permalink)
    +2 (2)
    Yes, that's exactly what has been complained about for years.
     

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #9
    Jump to:
    © 2020 APG vNext Commercial Version 4.5