• AVR Freaks

Tell me how to use a visual emulator

Author
Jordanelektronika
New Member
  • Total Posts : 10
  • Reward points : 0
  • Joined: 2015/05/18 05:11:36
  • Location: 0
  • Status: offline
2015/08/16 03:42:12 (permalink)
0

Tell me how to use a visual emulator

Can someone please tell me how to use a visual emulator, I have the whole MPLAB X IDE installed, I believe, but all I see is simulator and ICD and so on in the options.However the only thing the simulator shows is text.
#1

1 Reply Related Threads

    Mike017
    Super Member
    • Total Posts : 2698
    • Reward points : 0
    • Joined: 2007/08/25 08:11:31
    • Location: Lincoln, RI, USA
    • Status: offline
    Re: Tell me how to use a visual emulator 2015/08/17 14:01:39 (permalink)
    0
    Hi,
    Can someone please tell me how to use a visual emulator, I have the whole MPLAB X IDE installed, I believe, but all I see is simulator and ICD and so on in the options.However the only thing the simulator shows is text.
    "Visual Emulator" .... if you mean something like Labcenter's Proteus graph based simulators, there is none of that in MPLABX. However, there are features available in the MPLABX SIM that are very useful i.e. mouseover, Watch Windows, Stopwatch, Analyzer, etc. Try one of the tutorials to get an idea.
     
    Good Luck,
    Mike
     
     
    #2
    Jump to:
    © 2019 APG vNext Commercial Version 4.5