• AVR Freaks

Hot!USB Driver for MPLAB PM3

Author
Durite
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2013/06/12 01:22:05
  • Location: 0
  • Status: offline
2015/07/29 06:39:15 (permalink)
0

USB Driver for MPLAB PM3

I have installed MP X IDE 3.05 IPE, but cannot seem to find the drivers for the PM3, I have also tried installing the IDE as well but still no drivers seem to be present.  All the searches I have done relating to drivers state a directory, either Drivers or Drivers64 that does not exist in the installation directory.
 
Can these be downloaded separately, if so from where?
 
Thanks.
 
Windows 7 professional 64 bit
MPLAB X 3.05
BIOS Version 02.26.03
OS Version 02.09.32
USB Version 00.04.00
 
#1

3 Replies Related Threads

    prj
    Super Member
    • Total Posts : 218
    • Reward points : 0
    • Joined: 2009/12/01 14:35:45
    • Location: 0
    • Status: offline
    Re: USB Driver for MPLAB PM3 2015/07/29 09:37:08 (permalink)
    0
    Are you saying that, using the IPE, you cannot see the PM3 in the device selection field? Or are you saying that, using the IPE, you can select the PM3/serial number combo but it cannot connect? Thanks.
    #2
    Durite
    New Member
    • Total Posts : 2
    • Reward points : 0
    • Joined: 2013/06/12 01:22:05
    • Location: 0
    • Status: offline
    Re: USB Driver for MPLAB PM3 2015/08/05 04:26:51 (permalink)
    0
    Thanks for the reply.
     
    I was having trouble getting Windows to recognise the PM3 device in the device list, it was therefor not showing in the IPE as a selectable unit.
     
    I think this came from an error while installing the IPE.  Having got the error I did an uninstall and reinstall and got no error but still no device driver.
     
    Once I'd told Windows device manager to update the driver and tell it to search the MPLAB directory under Program Files it located the drivers and installed the device correctly.
     
    It is now working.
    #3
    rcruz116
    New Member
    • Total Posts : 6
    • Reward points : 0
    • Joined: 2012/03/06 15:01:22
    • Location: 0
    • Status: offline
    Re: USB Driver for MPLAB PM3 2019/12/13 10:00:52 (permalink)
    5 (1)
    I have resolve this problem MPLAB x IDE.  
     
    From MPLAB PM3 (programmer). 
    MPLAB OS SUITE Version ... 02.12.53
    BIOS Version .........02.28.23
    OS version  ..........02.09.37
    Power Monitor Version ...... 00.01.13
    CPLD Version ...................00.06.00
    FPGA Version ...................01.11.00
    ICSP Monitor Version ........ 00.02.83
    USB Versio .........00.04.00   
    Database Vesrion ............02.22.2a
     
     
    This update is the last for the MPLAB IDE 8.92
     
    But When I install MPLAB x IDE I (version 2.0) can not communication (USB) 
     
    After read the help, I get solution (how update usb driver)
    in the "Getting Started with MPLAB X IDE", section "Before you begin", UBS Driver instalation for windows XP/7/8 Operating System. 
     
    After follow the instruction i get communication for USB. 
     
    and update my MPLAB PM3
     
     
    #4
    Jump to:
    © 2020 APG vNext Commercial Version 4.5