• AVR Freaks

Hot!PICKit3 cannot connect to EasyPIC v7

Author
internetuser2k11
Starting Member
  • Total Posts : 73
  • Reward points : 0
  • Joined: 2012/04/11 18:35:55
  • Location: 0
  • Status: offline
2015/03/27 14:20:34 (permalink)
0

PICKit3 cannot connect to EasyPIC v7

I have PICKit3 and AC164110 - RJ-11 to ICSP Adapter. I am trying to connect PICKit 3 to mikroElektronika EasyPIC v7 boards ICD2/3 RJ11 connector but I get "connection failed" message in MPLAB X IPE. ICD3 works fine when connected to EasyPIC v7.
#1

4 Replies Related Threads

    Hemjal
    New Member
    • Total Posts : 5
    • Reward points : 0
    • Joined: 2019/09/12 23:37:27
    • Location: 0
    • Status: offline
    Re: PICKit3 cannot connect to EasyPIC v7 2019/09/19 02:42:41 (permalink)
    0
    Hello,
     
    You can connect manually by connecting the pickit 3 with AC164110 connector. For that you need jumper wire to connect the pins between AC164110 and pickit 3. Remember the options, * Power the board from the pickit 3. or you have to power the easypic v7 with an usb or external power supply.
    #2
    ric
    Super Member
    • Total Posts : 27057
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: online
    Re: PICKit3 cannot connect to EasyPIC v7 2019/09/19 13:39:41 (permalink)
    0
    I suspect that after four years, the asker has moved on...
     

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #3
    MBedder
    Circuit breaker
    • Total Posts : 6876
    • Reward points : 0
    • Joined: 2008/05/30 11:24:01
    • Location: Zelenograd, Russia
    • Status: offline
    Re: PICKit3 cannot connect to EasyPIC v7 2019/09/19 13:55:22 (permalink)
    0
    ricI suspect that after four years, the asker has moved on...
    Or even died after desperately trying to connect in a non-stop manner for 4 years LoL


    #4
    katela
    Super Member
    • Total Posts : 1756
    • Reward points : 0
    • Joined: 2013/06/11 05:25:18
    • Location: South Africa
    • Status: online
    Re: PICKit3 cannot connect to EasyPIC v7 2019/09/20 08:10:43 (permalink)
    0
    Or maybe he just wanted to provide an answer to this open question to help others who might come upon it in search results.

    Free online Microcontroller Tutorials and Projects for Hobbyists and students. From beginners to advanced. Website: www.studentcompanion.co.za
    YouTube Tutorials: https://www.youtube.com/StudentCompanionSA
    #5
    Jump to:
    © 2020 APG vNext Commercial Version 4.5