• AVR Freaks

Hot!Interfacing the PIC16F628A with a TM1637 (Chinese) Multiplexed LED Display

Page: < 123 Showing page 3 of 3
Author
Joe Burch
New Member
  • Total Posts : 18
  • Reward points : 0
  • Joined: 2014/12/10 21:31:25
  • Location: 0
  • Status: offline
Re: Interfacing the PIC16F628A with a TM1637 (Chinese) Multiplexed LED Display 2019/05/09 19:50:53 (permalink)
0
Hello - a while back, I completely re-wrote the code in the PIC16F648 processor in one of those Chinese 6 digit frequency counters so that now I have two presets that will enable me to use it as a replacement frequency display for many ham radios - like the Ten-Tec series.  It's a nice, stable, very accurate unit (100 hz) with a TCXO - and it's also very inexpensive.
 
Joe - K3JLS
#41
Page: < 123 Showing page 3 of 3
Jump to:
© 2019 APG vNext Commercial Version 4.5