• AVR Freaks

USB Driver Issue MCHPUSB Driver

Author
kr121
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2014/12/09 08:42:46
  • Location: 0
  • Status: offline
2014/12/09 08:57:58 (permalink)
0

USB Driver Issue MCHPUSB Driver

Hi There, 
 
I am new to Microchip, I have inherited a project, and I am having trouble with a USB driver. 
MCHPUSB, I have a micro USB port connected up to my PIC32MX795F512L
The idea is that I can connect this to my PC via a USB cable and read the data off the SD card that is in my unit. 
I am faced with the problem that Windows 7 and Windows 8 say they do not recognize the device. 
 
I have also been told that it works on Mac.
 
I am sure this is a simple fix, for some one who knows the tools better than my self. 
 
Any help will be greatly appreciated.
 
Many Thanks
 
Kevin
 
Attached is the driver that I was given.
#1
chinzei
Super Member
  • Total Posts : 2250
  • Reward points : 0
  • Joined: 2003/11/07 12:39:02
  • Location: Tokyo, Japan
  • Status: offline
Re: USB Driver Issue MCHPUSB Driver 2014/12/10 19:52:59 (permalink)
0 (1)
Microchip has finished support of MCHPUSB drivers for recent Windows verisions.
They suggest replacement of the driver with WinUSB + MPUSBAPI 6.0.0.0, which provides compatible interface without any change on PC applications.

We discussed it on this thread.
http://www.microchip.com/forums/m832713.aspx

Tsuneo
#2
Jump to:
© 2021 APG vNext Commercial Version 4.5