• AVR Freaks

Hot!USB SPI CLICK connection with Micron Serial Nor Flash memory (SD)?

Author
sead_avdic
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2014/11/27 02:40:29
  • Location: 0
  • Status: offline
2014/11/27 06:15:06 (permalink)
0

USB SPI CLICK connection with Micron Serial Nor Flash memory (SD)?

I am beginner in this so i would appreciate any help.
I need to connect USB SPI click and Micron Serial Nor Flash memory (SD) and to read and write data into Flash.
How can I do that?.
This is what i have done by now:
1.Connection USB SPI click ---> Flash (PINs to PINs)
2.I have downloaded functions for flash memory (N25q512a) but i have problem with one library #include "rodan_mmrb.h"(language c) (picture2)
3. I have downloaded functions for MCP2210_DLL_v1.1.zip(C#), and I know how to use them, MCP2210 utility,MCC_SPI_Terminal.
I would appreciate even some basic instructions to know in which way i must go.

Attached Image(s)

#1
Rabi
Embedded engineer
  • Total Posts : 9
  • Reward points : 0
  • Joined: 2020/05/14 23:49:25
  • Location: 0
  • Status: offline
Re: USB SPI CLICK connection with Micron Serial Nor Flash memory (SD)? 2020/06/09 01:06:02 (permalink)
0
yes I also have the same problem
 
#2
Jump to:
© 2020 APG vNext Commercial Version 4.5