• AVR Freaks

Icd3 support only in commercial version?

Author
koshee
New Member
  • Total Posts : 6
  • Reward points : 0
  • Joined: 2013/08/09 06:42:05
  • Location: 0
  • Status: offline
2014/09/01 23:44:10 (permalink)
0

Icd3 support only in commercial version?

subj.
plus: are there any plans to make arriba plugin for QtCreator?
#1

2 Replies Related Threads

    guymc
    Administrator
    • Total Posts : 769
    • Reward points : 0
    • Joined: 2004/06/08 07:14:37
    • Status: offline
    Re: Icd3 support only in commercial version? 2014/09/02 10:28:28 (permalink)
    +1 (1)
    The free Community Edition supports PICkit 3 and the MPLAB X simulator, but not the ICD 3.
     
    More info is available here: www.microchip.com/arriba
     
    Cheers
    #2
    viosoft
    Moderator
    • Total Posts : 6
    • Reward points : 0
    • Joined: 2014/07/02 16:55:57
    • Location: 0
    • Status: offline
    Re: Icd3 support only in commercial version? 2014/09/02 11:51:53 (permalink)
    0
    We've discussed support for different IDE including KDevelop and Insight at MASTERs, and have verified that debugging with KDevelop works.   Since qtCreator is loosely derived from KDevelop, we suspect that it should be straight forward to support. 
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5