• AVR Freaks

Debug - breakpoint not resolvable to valid memory address?

Author
OscarTheGrouch
Super Member
  • Total Posts : 305
  • Reward points : 0
  • Joined: 2010/11/29 18:07:28
  • Location: 0
  • Status: offline
2014/05/18 15:27:02 (permalink)
0

Debug - breakpoint not resolvable to valid memory address?

Trying to debug using MPLAB 2.10, PICKit3 on a PIC32MX795 .. Harmony application.
In Switch function, can't see what is going wrong in my code because debuger skips over it.
Break points say no valid memory address .. see screen shot.
Can any one tell me what's up with this?
Thanks

Attachment(s)

Attachments are not available: Download requirements not met
#1

1 Reply Related Threads

    OscarTheGrouch
    Super Member
    • Total Posts : 305
    • Reward points : 0
    • Joined: 2010/11/29 18:07:28
    • Location: 0
    • Status: offline
    Re: Debug - breakpoint not resolvable to valid memory address? 2014/05/18 15:54:32 (permalink)
    0
    This was a test mr green: mr green
    My for loop was wrong .. condition after i++ does not work.
    #2
    Jump to:
    © 2019 APG vNext Commercial Version 4.5