• AVR Freaks

Helpful ReplyLockedXC32 v1.30 + FreeRTOS = compilation error

Author
XProject
New Member
  • Total Posts : 5
  • Reward points : 0
  • Joined: 2012/09/18 00:48:15
  • Location: 0
  • Status: offline
2013/12/10 01:02:03 (permalink)
0

XC32 v1.30 + FreeRTOS = compilation error

Hi,
In my project I'm using PIC32MX695F512L, MPLAB X IDE v1.95, FreeRTOS V7.3.0.
Everything was ok when I used  XC32 1.21 compiler version (free edition).
If I use new compiler version (v1.30, also free edition, ) then after Build All I get the following result in output window:
...
"C:\Program Files (x86)\Microchip\xc32\v1.30\bin\xc32-gcc.exe" -c -mprocessor=32MX695F512L -MMD -MF build/default/production/_ext/2096788717/port_asm.o.d -o build/default/production/_ext/2096788717/port_asm.o C:/Projects/AR207/MPLABX/FreeRTOS/port_asm.S -Wa,--defsym=__MPLAB_BUILD=1,-MD=build/default/production/_ext/2096788717/port_asm.o.asm.d,--gdwarf-2,-I.. 
C:\Users\Mario\AppData\Local\Temp\ccn1JQfi.s: Assembler messages:
C:\Users\Mario\AppData\Local\Temp\ccn1JQfi.s: Error: .size expression for xPortStartScheduler does not evaluate to a constant
make[2]: *** [build/default/production/_ext/2096788717/port_asm.o] Error 1
make[2]: *** Waiting for unfinished jobs....
make[1]: *** [.build-conf] Error 2
...
Is it some compiler bug?


Thanks in advance.
 
#1
JasonK
Moderator
  • Total Posts : 3406
  • Reward points : 0
  • Joined: 2003/11/14 09:49:40
  • Location: Microchip Technology in Arizona, USA
  • Status: offline
Re:XC32 v1.30 + FreeRTOS = compilation error 2013/12/10 10:22:16 (permalink) ☄ Helpful

Jason Kajita
 Follow me on Twitter
http://support.microchip.com for urgent questions
#2
Jump to:
© 2020 APG vNext Commercial Version 4.5