• AVR Freaks

Helpful ReplyHot!Suggestions for the next release of MPLAB® Code Configurator

Page: < 12345.. > >> Showing page 5 of 14
Author
ric
Super Member
  • Total Posts : 25483
  • Reward points : 0
  • Joined: 2003/11/07 12:41:26
  • Location: Australia, Melbourne
  • Status: offline
Re: Suggestions for the next release of MPLAB® Code Configurator 2015/03/05 20:42:26 (permalink)
3 (1)
elvinguitar
is it possible for you to include MCC support for pic16f877a? Thanks


Are you seriously doing a new design using that ancient part?
There are much cheaper, faster, easier to design around PIC16F parts now available.

I also post at: PicForum
Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
NEW USERS: Posting images, links and code - workaround for restrictions.
To get a useful answer, always state which PIC you are using!
#81
skonrad
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2015/03/11 12:11:09
  • Location: 0
  • Status: offline
Re: Suggestions for the next release of MPLAB® Code Configurator 2015/03/11 12:27:09 (permalink)
0
MCC is very useful stuff!!!
I'm interested in generation of MSSP:SPI slave with interrupt module.
Regards,
Konrad
#82
Sören van de Bilt
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2015/03/12 07:25:49
  • Location: 0
  • Status: offline
Re: Suggestions for the next release of MPLAB® Code Configurator 2015/03/12 07:27:10 (permalink)
0
I would love to see more PIC24 series, like the PIC24F16KA102 for example.
And how often is the MCC updated?
Best regards.
#83
ns.mchp
Moderator
  • Total Posts : 87
  • Reward points : 0
  • Joined: 2013/10/21 16:06:20
  • Location: 0
  • Status: offline
Re: Suggestions for the next release of MPLAB® Code Configurator 2015/03/12 10:03:52 (permalink)
0
KA102 is planned for the CQ2 release. Typically we plan to do 3 major releases and if required dot releases (bug fix releases) between them during the year. The actual number may vary. 
#84
dds
Starting Member
  • Total Posts : 40
  • Reward points : 0
  • Joined: 2012/05/26 20:32:48
  • Location: 0
  • Status: offline
Re: Suggestions for the next release of MPLAB® Code Configurator 2015/03/12 12:48:45 (permalink)
0
I would like to see a configuration module for devices with BUILT-IN-RTCC.
Also, I would like to see a module for creating and RTCC with the timers.
#85
Sören van de Bilt
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2015/03/12 07:25:49
  • Location: 0
  • Status: offline
Re: Suggestions for the next release of MPLAB® Code Configurator 2015/03/12 13:39:51 (permalink)
0
Nice, thanks!
And when is that release coming?
 
#86
ns.mchp
Moderator
  • Total Posts : 87
  • Reward points : 0
  • Joined: 2013/10/21 16:06:20
  • Location: 0
  • Status: offline
Re: Suggestions for the next release of MPLAB® Code Configurator 2015/03/12 13:41:00 (permalink)
0
The 16 bit devices which have RTCC as the device peripheral is already supported. Thank you for the feedback on supporting RTCC functionality using a timer. 
#87
ns.mchp
Moderator
  • Total Posts : 87
  • Reward points : 0
  • Joined: 2013/10/21 16:06:20
  • Location: 0
  • Status: offline
Re: Suggestions for the next release of MPLAB® Code Configurator 2015/03/13 08:51:29 (permalink)
0
Plan is to have around April - May timeframe. 
#88
skonrad
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2015/03/11 12:11:09
  • Location: 0
  • Status: offline
Re: Suggestions for the next release of MPLAB® Code Configurator 2015/03/18 03:44:20 (permalink)
0
Did you plane add SPI Slave with Interrupt for PIC18 devices?
 
Regards,
Konrad
#89
Al.THz
New Member
  • Total Posts : 18
  • Reward points : 0
  • Joined: 2012/04/04 22:18:06
  • Location: Southwest Ontario Canada
  • Status: offline
Re:Suggestions for the next release of MPLAB® Code Configurator 2015/04/24 08:18:34 (permalink)
0
NorthGuy
I wonder why from the multitude of available PICs only PIC16 got chosen. I understand there are more devices on its way, but why the initial selection is PIC16?



I completely agree, it seems to me that the very first devices that should have been added are the ones that they have and do implement in development kits/boards. It would help support the products that they are already trying to market, thus making the product more appealing. But I am no marketing wiz so what do I know.
#90
dragonet80
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2012/05/22 05:45:26
  • Location: 0
  • Status: offline
Re:Suggestions for the next release of MPLAB® Code Configurator 2015/04/30 10:25:11 (permalink)
0
To me, the very first and most important feature that MCC MUST have is to support all Microchip micros. Where are all dsPICs? I like dsPIC33EP512GM706, but there is no support for them.
#91
Pusb
Moderator
  • Total Posts : 106
  • Reward points : 0
  • Joined: 2004/02/09 09:47:27
  • Status: offline
Re:Suggestions for the next release of MPLAB® Code Configurator 2015/05/01 18:07:13 (permalink)
0
pipe-lining part support release is not a bad thing, as they become available as ready. Waiting for all all micros support to be ready means no one gets to benefit until they are all ready ?
#92
adrian.muresan
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2015/05/14 07:13:16
  • Location: 0
  • Status: offline
Re:Suggestions for the next release of MPLAB® Code Configurator 2015/05/14 07:17:57 (permalink)
0
Is there a timeline for pic18f4580 to be supported?
We are using these for an internal relay box and we'd like for non-embedded guys to be able to write apps; having Code Configurator support would help immensely.
#93
Pete_K
Starting Member
  • Total Posts : 50
  • Reward points : 0
  • Joined: 2014/04/10 04:05:22
  • Location: Germany
  • Status: offline
Re:Suggestions for the next release of MPLAB® Code Configurator 2015/05/17 07:16:37 (permalink)
0
Issue some test qualification on Graphic Composer. In some terms it`s still buggy using MPLABX 3.00 beta & Harmony 1.04.02.
For example dragging "Digital Meter" or "Static Text" into text area. It however can be compiled but system/MEB II gets screwed showing weird flickering background colors.
Then, "Frame" On/Off in "Picture" Widget is just inverted.
If you use Picture Widget, there are some weird and crappy dots/lines at the very bottom of LCD.
 
Make Graphic Composer more useful! Principal idea is fantastic though!
 
Pete
post edited by Pete_K - 2015/05/17 07:17:55
#94
MCHP_Ryan
Administrator
  • Total Posts : 22
  • Reward points : 0
  • Joined: 2015/05/05 17:10:30
  • Location: Chandler, AZ
  • Status: offline
Re:Suggestions for the next release of MPLAB® Code Configurator 2015/05/29 14:33:52 (permalink)
3 (1)
adrian.muresan
Is there a timeline for pic18f4580 to be supported?
We are using these for an internal relay box and we'd like for non-embedded guys to be able to write apps; having Code Configurator support would help immensely.


Hi Adrian,
 
We are working to add support for newer devices which we recommend using for new designs.  The PIC18F45K80 should be supported in the next release which is planned for Q3/Q4 this year.
 
Thanks,
 
Ryan
post edited by MCHP_Ryan - 2015/06/03 12:03:09
#95
ganeshkumarsw
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2015/08/20 14:16:04
  • Location: 0
  • Status: offline
Re: Suggestions for the next release of MPLAB® Code Configurator 2015/08/24 05:34:50 (permalink)
0
Hi,
   My suggestion is to have MCC supported for lots of unsupported controllers, for instance with usage of XC8 v1.35, PLIB is removed hence I had to use MCC to generate the code, but current version MCC doesn't support for the controller that I am using (PIC18F24J11), so here I need to stick with XC8 v1.34 where I have PLIB support.
 
Any plans for unsupported controllers?
post edited by ganeshkumarsw - 2015/08/24 10:18:34
#96
raja28chowdhury
Starting Member
  • Total Posts : 45
  • Reward points : 0
  • Joined: 2015/06/14 00:15:06
  • Location: 0
  • Status: offline
Re:Suggestions for the next release of MPLAB® Code Configurator 2015/08/24 11:02:57 (permalink)
0
one quick addition can be made when i select adc multiplier it is written 1x,2x ,4x please also write voltage reference instead of that
 
thanks
#97
ric
Super Member
  • Total Posts : 25483
  • Reward points : 0
  • Joined: 2003/11/07 12:41:26
  • Location: Australia, Melbourne
  • Status: offline
Re:Suggestions for the next release of MPLAB® Code Configurator 2015/08/24 15:15:49 (permalink)
0
ganeshkumarsw
   My suggestion is to have MCC supported for lots of unsupported controllers, for instance with usage of XC8 v1.35, PLIB is removed hence I had to use MCC to generate the code, but current version MCC doesn't support for the controller that I am using (PIC18F24J11), so here I need to stick with XC8 v1.34 where I have PLIB support.

PLIB is still supported in XC8 v1.35, it is just a seperate download now.
 

I also post at: PicForum
Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
NEW USERS: Posting images, links and code - workaround for restrictions.
To get a useful answer, always state which PIC you are using!
#98
rsdio
Junior Member
  • Total Posts : 116
  • Reward points : 0
  • Joined: 2008/07/03 16:18:10
  • Location: Seattle
  • Status: offline
Re:Suggestions for the next release of MPLAB® Code Configurator 2015/09/07 17:57:36 (permalink)
0
Support for the PIC18F4550 should be high on the list, assuming I'm correct that this is a very popular part.
 
p.s. I started a thread asking about 4550 support before I saw this thread for collecting all suggestions. If someone wants to remove my 4550-specific thread because it's redundant, that's fine with me. I couldn't find a way to delete my own thread.
post edited by rsdio - 2015/09/07 17:58:41
#99
sartoP
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2015/06/11 05:43:42
  • Location: 0
  • Status: offline
Re: Suggestions for the next release of MPLAB® Code Configurator 2015/09/11 01:59:12 (permalink)
0
Hello,
in our High school () we have developed for student a PIC18 based board (information on the link -> picebs2.hevs.ch).
It will be great for our students to have the PIC18F87K22 included in the Code Configurator ;-)
 
Regards
 
Page: < 12345.. > >> Showing page 5 of 14
Jump to:
© 2020 APG vNext Commercial Version 4.5