• AVR Freaks

Helpful ReplyHot!Suggestions for the next release of MPLAB® Code Configurator

Page: << < ..1112131415 Showing page 15 of 15
Author
thecucarachon
New Member
  • Total Posts : 6
  • Reward points : 0
  • Joined: 2020/10/17 16:40:32
  • Location: 0
  • Status: offline
Re:Suggestions for the next release of MPLAB® Code Configurator 2020/10/20 09:39:48 (permalink)
3.67 (3)
Liquid LCD library
OLED Library
Export MCC Project to next family type
jmmysonfire
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2020/10/23 06:32:51
  • Location: 0
  • Status: offline
Re:Suggestions for the next release of MPLAB® Code Configurator 2020/10/27 17:46:55 (permalink)
1.5 (2)
Please add support the DSPIC33FJ128GP802.
 
I realise it is an older product but it is still in production and newbies like myself would benefit greatly.
 
Thanks.
ric
Super Member
  • Total Posts : 30197
  • Reward points : 0
  • Joined: 2003/11/07 12:41:26
  • Location: Australia, Melbourne
  • Status: online
Re:Suggestions for the next release of MPLAB® Code Configurator 2020/10/28 12:18:16 (permalink)
0
jmmysonfire
Please add support the DSPIC33FJ128GP802.
 
I realise it is an older product but it is still in production and newbies like myself would benefit greatly.

They never add older parts. It is only a tool to help them sell newer parts.

I also post at: PicForum
Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
NEW USERS: Posting images, links and code - workaround for restrictions.
To get a useful answer, always state which PIC you are using!
Liem Dung Phan
Starting Member
  • Total Posts : 24
  • Reward points : 0
  • Joined: 2017/09/14 21:09:39
  • Location: 0
  • Status: offline
Re: Suggestions for the next release of MPLAB® Code Configurator 2020/12/16 18:28:26 (permalink) ☄ Helpfulby WeHongKongers 2021/02/09 02:58:53
4.5 (2)
Why don't you add Arm® Cortex®-M0+ MCUs such as SAMC,L,D to MCC?
Harmony is so slow, complex to use on entry-level MCU.
kaamil1984
Junior Member
  • Total Posts : 55
  • Reward points : 0
  • Joined: 2014/05/01 14:02:25
  • Location: Chair at the desk in my workshop ;)
  • Status: offline
Re: Suggestions for the next release of MPLAB® Code Configurator 2021/01/31 09:11:54 (permalink)
2 (1)
Hi guys,
 
Can we expect "git friendly" code generation? Can we get some feedback?
 
I have the impression that what we write here falls into a black hole and nothing is happening.
 
Does anyone at Microchip read this?
Birhan
New Member
  • Total Posts : 5
  • Reward points : 0
  • Joined: 2019/03/07 03:28:36
  • Location: 0
  • Status: offline
Re: Suggestions for the next release of MPLAB® Code Configurator 2021/02/08 15:17:55 (permalink)
0
What about asm code generation? not drivers libs etc. only device init code to asm besidesxc8 code will be perfect.
WeHongKongers
Super Member
  • Total Posts : 279
  • Reward points : 0
  • Status: offline
Re:Suggestions for the next release of MPLAB® Code Configurator 2021/02/09 02:36:15 (permalink)
0
jmmysonfire
Please add support the DSPIC33FJ128GP802.
I realise it is an older product but it is still in production and newbies like myself would benefit greatly.
Thanks.



Move up to some newer drop-in replacement to benefit MCC.  MCC includes many many macros and functions which you can call at once!
 
Open a support ticket and they will give you the best suggestion.  Don`t be shy.
oliverb
Super Member
  • Total Posts : 435
  • Reward points : 0
  • Joined: 2009/02/16 13:12:38
  • Location: 0
  • Status: offline
Re:Suggestions for the next release of MPLAB® Code Configurator 2021/03/11 02:25:57 (permalink)
0
If this hasn't already been addressed: MCC should try to maintain the order of entries in the .mcc configuration file. I'm finding that MCC randomly reorders the file sometimes leading to unnecessary changes showing up in git.
 
To solve this it could either attempt to preserve the original sequence or the module configurations could be output in a specific order, even alphabetical would do.
EdwardPage
New Member
  • Total Posts : 20
  • Reward points : 0
  • Joined: 2021/02/07 20:06:48
  • Location: 0
  • Status: offline
Re:Suggestions for the next release of MPLAB® Code Configurator 2021/03/11 12:34:15 (permalink)
0
Currently using the dsPIC33EPXXXMC202
 
Would like to see all of the peripherals supported, saves time scrolling through the datasheet.
 
CTMU - Charge time measurement unit
QEI - Quadrature encoder
 
RISC
Super Member
  • Total Posts : 6053
  • Reward points : 0
  • Status: offline
Re:Suggestions for the next release of MPLAB® Code Configurator 2021/03/11 14:59:38 (permalink)
0
Hi,
CTMU is an old peripheral included in very few PIC devices.
Since many years it has not been added to any new device so I guess it won't be supported in MCC... 
Regards
 

For support make sure to check first here : http://microchipdeveloper.com
There are hundreds of PIC, AVR, SAM...which one do YOU use ?
Page: << < ..1112131415 Showing page 15 of 15
Jump to:
© 2021 APG vNext Commercial Version 4.5