• AVR Freaks

restart computer from USB port

Author
mohamed ragab
New Member
  • Total Posts : 16
  • Reward points : 0
  • Joined: 2013/07/15 02:14:32
  • Location: 0
  • Status: offline
2013/07/28 02:21:38 (permalink)
0

restart computer from USB port

hello All, 
Kindly find below:  
i want to restart computer from USB port via pic 18f4550 program 
Best Regards,  
Mohamed Ragab 
#1

4 Replies Related Threads

    DarioG
    Allmächtig.
    • Total Posts : 54081
    • Reward points : 0
    • Joined: 2006/02/25 08:58:22
    • Location: Oesterreich
    • Status: offline
    Re:restart computer from USB port 2013/07/28 02:38:17 (permalink)
    0
    We've been into this some time ago Smile
    It's not difficult at all, but you need to have some User Program running on the PC, that listens for commands from the USB port.
     
    Am not sure if any "special" USB devices - possibly UPS class - have drivers/handlers on most OSes that can perform the reset automatically...

    GENOVA :D :D ! GODO
    #2
    mohamed ragab
    New Member
    • Total Posts : 16
    • Reward points : 0
    • Joined: 2013/07/15 02:14:32
    • Location: 0
    • Status: offline
    Re:restart computer from USB port 2013/07/28 02:53:05 (permalink)
    0
    hello Dario Greggio,
    i want some examples or links to do this
    #3
    chinzei
    Super Member
    • Total Posts : 2250
    • Reward points : 0
    • Joined: 2003/11/07 12:39:02
    • Location: Tokyo, Japan
    • Status: offline
    Re:restart computer from USB port 2013/07/28 10:51:37 (permalink)
    +2 (1)
    Windows accepts these Usages on Generic desktop page, sent from HID System Control device.
    - System Power down: 0x81
    - System Sleep     : 0x82
    - System Wake up   : 0x83

    Restart (reboot) is not directly supported, but it may be emulated with "System Wake up" after "System Power down"

    In this topic, we've discussed on PIC implementation of HID System Control device.
    http://www.microchip.com/forums/m405397.aspx

    Tsuneo
    #4
    DarioG
    Allmächtig.
    • Total Posts : 54081
    • Reward points : 0
    • Joined: 2006/02/25 08:58:22
    • Location: Oesterreich
    • Status: offline
    Re:restart computer from USB port 2013/07/28 15:19:12 (permalink)
    0
    Perfect Tsuneo Smile

    GENOVA :D :D ! GODO
    #5
    Jump to:
    © 2021 APG vNext Commercial Version 4.5