PIC24F I2C to Raspberry Pi
Hi All,
I'm new to PIC's and PIC programming but I'm working on a little project to try get a PIC24F32KA301 to communicate with a Raspberry Pi using I2C. In this setup the Raspberry Pi is the master and the PIC is the slave. I have created a little python program on the Raspberry Pi and tested that it works by successfully communicating with an Arduino, what I want to do now is replace the Arduino with a PIC.
Just for completeness I've included the python program below:
import smbus
import time
bus = smbus.SMBus(1)
address = 0x22
def writeNumber(value):
bus.write_byte(address, value)
return -1
def readNumber():
number = bus.read_byte(address)
return number
while True:
var = input("Enter 1 - 9: ")
if not var:
continue
writeNumber(var)
print "RPI: Hi Arduino, I sent you ", var
time.sleep(1)
number = readNumber()
print "Arduino: Hey RPI, I received a digit ", number
print
I'm pretty sure I've connected the PIC and Raspberry Pi correctly, e.g. GND <---> Vss (pin 19), SCL <---> SCL1 (pin 12), SDA <---> SDA1 (pin 13). The Raspberry Pi is powered over USB (so I think that's 5V, but it might be 3V) and the PIC is powered separately using a 3V battery. The Arduino didn't have any pull up resistors so I assumed it would be ok to not have any on the PIC (maybe this is wrong?). I'm using C with the XC16 compiler and the i2c.h library to program the PIC but I'm not really sure what I'm doing, I've tried my best to piece things together from I2C examples and little bits I've read on various forums etc. My code is below:
#define USE_AND_OR // not sure what this is!
#include <p24Fxxxx.h>
#include <i2c.h>
unsigned char I2C_RECV[1]
void main(void) {
unsigned int temp, i;
for(i=0; i<1; i++)
I2C_RECV[i]=0;
TRISA = 0b0000000000000000;
PORTA = 0b0000000000000001;
/* INITIALISE I2C MODULE */
CloseI2C1(); // close i2c if it was operating earlier
while(1) {
OpenI2C1((I2C_ON | I2C_7BIT_ADD | I2C_CLK_REL | I2C_STR_EN), 0);
I2C1ADD = 0x22; // initialze slave address to 1E
// receive data from master
while(DataRdyI2C1() == 0); // wait until data is transmitted from master
temp = SlaveReadI2C1(); // read address to empty buffer
SlavegetsI2C1(I2C_RECV, 1); // receive data
if(I2C_RECV[0] == 9) {
PORTA = 0b0000000000000011;
}
CloseI2C1();
}
}
The code is quite simple (but probably very wrong!). Basically I initialise the I2C module and turn on an LED, then I enter a loop, open the I2C connection using address 0x22 and wait for the master to send some data. When data is received I check it's value, if it's 9 I turn on another LED.
On the Raspberry Pi I can confirm that the PIC is accessible by running
i2cdetect -y 1. I can see the PIC at address 0x22, which gives me some confidence that I'm at least heading in the right direction! However, when I run the python program I receive an IO error, the error number is 5. I've looked around to find out what that means, but it's a very vague error, basically anything could have gone wrong!
I'm not sure if it's my circuit that's incorrect (i.e. do I need pull up resistors, if so how do I calculate what resistance they need to be?) or my PIC program. If anyone has any advice I'd be very very grateful.
Thanks.